This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC3200 的SPI DMA

Other Parts Discussed in Thread: CC3200

hello,对于SPI的DMA模式无法使用的BUG:


********************************************
CC3200 SPI Demo Application!
Birate: 10000000
DMA size:1024
********************************************

Start the slave and press any key to transmit data....

我发输入,卡在这里。

代码:

int main()
{
uint32_t tx_crc = 0;
uint32_t tx_crc_old = 0;
uint32_t a = 364;
uint32_t b = 53457;
uint32_t c = 976;
uint32_t d = 66;
uint32_t error_counter = 0;
uint32_t transfer_counter = 0;


init();

// initialize buffers with some known value
memset(tx_buffer,0x33,sizeof(tx_buffer));
memset(rx_buffer,0x44,sizeof(rx_buffer));

// wait for keystroke: this gives the user time to start the slave
Report("Start the slave and press any key to transmit data....\n\r");
MAP_UARTCharGet(UARTA0_BASE);

spi_setup(SPI_MODE_MASTER,interrupt_handler);

tx_crc = fill_buffer(tx_buffer,DMA_SIZE);

..........................

  • http://www.deyisupport.com/cfs-file.ashx/__key/communityserver-discussions-components-files/105/7024.spi_5F00_demo_5F00_DMA.zip

    
    
    //*****************************************************************************
    //
    // Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com/ 
    // 
    // 
    //  Redistribution and use in source and binary forms, with or without 
    //  modification, are permitted provided that the following conditions 
    //  are met:
    //
    //    Redistributions of source code must retain the above copyright 
    //    notice, this list of conditions and the following disclaimer.
    //
    //    Redistributions in binary form must reproduce the above copyright
    //    notice, this list of conditions and the following disclaimer in the 
    //    documentation and/or other materials provided with the   
    //    distribution.
    //
    //    Neither the name of Texas Instruments Incorporated nor the names of
    //    its contributors may be used to endorse or promote products derived
    //    from this software without specific prior written permission.
    //
    //  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    //  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    //  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    //  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    //  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    //  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    //  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    //  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    //  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    //  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    //  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // Application Name     - SPI Demo
    // Application Overview - The demo application focuses on showing the required 
    //                        initialization sequence to enable the CC3200 SPI 
    //                        module in full duplex 4-wire master and slave mode(s).
    // Application Details  -
    // http://processors.wiki.ti.com/index.php/CC32xx_SPI_Demo
    // or
    // docs\examples\CC32xx_SPI_Demo.pdf
    //
    //*****************************************************************************
    
    
    //*****************************************************************************
    //
    //! \addtogroup SPI_Demo
    //! @{
    //
    //*****************************************************************************
    
    // Standard includes
    #include <string.h>
    
    // Driverlib includes
    #include "hw_types.h"
    #include "hw_memmap.h"
    #include "hw_common_reg.h"
    #include "hw_ints.h"
    #include "hw_mcspi.h"
    #include "hw_udma.h"
    #include "spi.h"
    #include "rom.h"
    #include "rom_map.h"
    #include "utils.h"
    #include "prcm.h"
    #include "uart.h"
    #include "udma.h"
    #include "interrupt.h"
    
    // Common interface includes
    #include "uart_if.h"
    #include "udma_if.h"
    #include "pinmux.h"
    
    
    #define APPLICATION_VERSION     "1.1.0"
    //*****************************************************************************
    //
    // Application Master/Slave mode selector macro
    //
    // MASTER_MODE = 1 : Application in master mode
    // MASTER_MODE = 0 : Application in slave mode
    //
    //*****************************************************************************
    #define MASTER_MODE      1
    
    #define SPI_IF_BIT_RATE  1000000
    #define TR_BUFF_SIZE     100
    
    #define MASTER_MSG       "This is CC3200 SPI Master Application\n\r"
    #define SLAVE_MSG        "This is CC3200 SPI Slave Application\n\r"
    
    //*****************************************************************************
    //                 GLOBAL VARIABLES -- Start
    //*****************************************************************************
    static unsigned char g_ucTxBuff[TR_BUFF_SIZE];
    static unsigned char g_ucRxBuff[TR_BUFF_SIZE];
    //static unsigned char g_ucDummyBuff[10];
    static unsigned char ucTxBuffNdx;
    static unsigned char ucRxBuffNdx;
    
    unsigned char g_ucDMAEnabled = 0;
    
    volatile char g_cDummy;
    
    #if defined(ccs)
    extern void (* const g_pfnVectors[])(void);
    #endif
    #if defined(ewarm)
    extern uVectorEntry __vector_table;
    #endif
    //*****************************************************************************
    //                 GLOBAL VARIABLES -- End
    //*****************************************************************************
    
    
    
    //*****************************************************************************
    //
    //! SPI Slave Interrupt handler
    //!
    //! This function is invoked when SPI slave has its receive register full or
    //! transmit register empty.
    //!
    //! \return None.
    //
    //*****************************************************************************
    static void SpiIntHandler()
    {
        unsigned long ulRecvData;
        unsigned long ulStatus;
    
        //ulStatus = MAP_SPIIntStatus(GSPI_BASE,true);
        
        //MAP_SPIIntClear(GSPI_BASE,SPI_INT_DMARX|SPI_INT_DMATX);
        SPIIntClear(GSPI_BASE,SPI_INT_EOW);
        SPICSDisable(GSPI_BASE);
        g_cDummy = 0x01;
        //MAP_SPIIntClear(GSPI_BASE,SPI_INT_RX_FULL|SPI_INT_TX_EMPTY);
    
        if(ulStatus & SPI_INT_TX_EMPTY)
        {
            //MAP_SPIDataPut(GSPI_BASE,g_ucTxBuff[ucTxBuffNdx%TR_BUFF_SIZE]);
            ucTxBuffNdx++;
        }
    
        if(ulStatus & SPI_INT_RX_FULL)
        {
            //MAP_SPIDataGetNonBlocking(GSPI_BASE,&ulRecvData);
            //g_ucTxBuff[ucRxBuffNdx%TR_BUFF_SIZE] = ulRecvData;
            //Report("%c",ulRecvData);
            ucRxBuffNdx++;
        }
        
        if(ulStatus & SPI_INT_DMARX)
        {
          ucTxBuffNdx++;
          //MAP_SPIDataGet(GSPI_BASE,&ulDummy);
        }
        
        if(ulStatus & SPI_INT_DMATX)
        {
          ucTxBuffNdx++;
        }
        
    }
    void Master_Send(unsigned char *ucBuff,int len)
    {
      unsigned long ulDummy=0;
     
      SPIWordCountSet(GSPI_BASE,len);
      
      SetupTransfer(UDMA_CH31_GSPI_TX,UDMA_MODE_BASIC,len,
                    UDMA_SIZE_8,UDMA_ARB_1,
                    (void *)ucBuff,UDMA_SRC_INC_8,(void *)(GSPI_BASE + MCSPI_O_TX0),
                    UDMA_DST_INC_NONE);
    
      SetupTransfer(UDMA_CH30_GSPI_RX,UDMA_MODE_BASIC,len,
                    UDMA_SIZE_8,UDMA_ARB_1,
                    (void *)(GSPI_BASE + MCSPI_O_RX0),UDMA_SRC_INC_NONE,
                    &ulDummy,UDMA_SRC_INC_NONE);
      
      MAP_SPIIntClear(GSPI_BASE,SPI_INT_EOW);
      
      //SPICSEnable(GSPI_BASE);
      MAP_SPIEnable(GSPI_BASE);
      
      while( !(MAP_SPIIntStatus(GSPI_BASE,false) & SPI_INT_EOW) );
      
      //SPICSDisable(GSPI_BASE);
      MAP_SPIDisable(GSPI_BASE);
    }
    
    void Master_Receive(unsigned char *ucBuff,int len)
    {
      unsigned long ulDummy=0;
      
      SPIWordCountSet(GSPI_BASE,len);
      
      SetupTransfer(UDMA_CH30_GSPI_RX,UDMA_MODE_BASIC,len,
                    UDMA_SIZE_8,UDMA_ARB_1,
                    (void *)(GSPI_BASE + MCSPI_O_RX0),UDMA_SRC_INC_NONE,
                    (void *)ucBuff,UDMA_DST_INC_8);
      
      SetupTransfer(UDMA_CH31_GSPI_TX,UDMA_MODE_BASIC,len,
                    UDMA_SIZE_8,UDMA_ARB_1,
                    &ulDummy,UDMA_SRC_INC_NONE,(void *)(GSPI_BASE + MCSPI_O_TX0),
                    UDMA_DST_INC_NONE);
    
      MAP_SPIIntClear(GSPI_BASE,SPI_INT_EOW);
      
      MAP_SPIEnable(GSPI_BASE);
      //SPICSEnable(GSPI_BASE);
      
      while( !(MAP_SPIIntStatus(GSPI_BASE,false) & SPI_INT_EOW) );
    
      //SPICSDisable(GSPI_BASE);
      MAP_SPIDisable(GSPI_BASE);
    }
    
    
    //*****************************************************************************
    //
    //! SPI Slave mode main loop
    //!
    //! This function configures SPI modelue as slave and enables the channel for
    //! communication
    //!
    //! \return None.
    //
    //*****************************************************************************
    void Spi_Init()
    {
        unsigned long ulBase;
    
        //NWP master interface
        ulBase = GSPI_BASE;
    
        //Enable MCSPIA2
        PRCMPeripheralClkEnable(PRCM_GSPI,PRCM_RUN_MODE_CLK);
    
        //Disable Chip Select
        SPICSDisable(ulBase);
    
        //Disable SPI Channel
        SPIDisable(ulBase);
    
        // Reset SPI
        SPIReset(ulBase);
    
        //
      // Configure SPI interface
      //
      SPIConfigSetExpClk(ulBase,PRCMPeripheralClockGet(PRCM_GSPI),
                         SPI_IF_BIT_RATE,SPI_MODE_MASTER,SPI_SUB_MODE_0,
                         (SPI_SW_CTRL_CS |
                         SPI_4PIN_MODE |
                         SPI_TURBO_OFF |
                         SPI_CS_ACTIVEHIGH |
                         SPI_WL_8));
    
      //
      // Initialize UDMA
      //
      UDMAInit();
      
    if(PRCMPeripheralStatusGet(PRCM_UDMA))
    {
      g_ucDMAEnabled = (HWREG(UDMA_BASE + UDMA_O_CTLBASE) != 0x0) ? 1 : 0;
    }
    else
    {
    	g_ucDMAEnabled = 0;
    }
    
    if(g_ucDMAEnabled)
    {
        // Set DMA channel
        MAP_uDMAChannelAssign(UDMA_CH30_GSPI_RX);
        MAP_uDMAChannelAttributeDisable(UDMA_CH30_GSPI_RX,UDMA_ATTR_ALTSELECT);
        MAP_uDMAChannelAssign(UDMA_CH31_GSPI_TX);
        MAP_uDMAChannelAttributeDisable(UDMA_CH31_GSPI_TX,UDMA_ATTR_ALTSELECT);
    
        SPIFIFOLevelSet(ulBase,1,1);
        SPIFIFOEnable(ulBase,SPI_RX_FIFO|SPI_TX_FIFO);
        SPIDmaEnable(ulBase,SPI_RX_DMA|SPI_TX_DMA);
    
        IntRegister(INT_GSPI,SpiIntHandler);
        
        SPICSEnable(GSPI_BASE);
        //IntPrioritySet(INT_GSPI, INT_PRIORITY_LVL_1);
        //IntEnable(INT_GSPI);
        
        //SPIIntEnable(ulBase,SPI_INT_DMARX|SPI_INT_DMATX);
        //SPIIntEnable(ulBase,SPI_INT_EOW);
    }
        g_cDummy = 0;
    
        //MAP_SPIEnable(ulBase);
    }
    
    //*****************************************************************************
    //
    //! Board Initialization & Configuration
    //!
    //! \param  None
    //!
    //! \return None
    //
    //*****************************************************************************
    static void
    BoardInit(void)
    {
    /* In case of TI-RTOS vector table is initialize by OS itself */
    #ifndef USE_TIRTOS
      //
      // Set vector table base
      //
    #if defined(ccs)
        MAP_IntVTableBaseSet((unsigned long)&g_pfnVectors[0]);
    #endif
    #if defined(ewarm)
        MAP_IntVTableBaseSet((unsigned long)&__vector_table);
    #endif
    #endif
        //
        // Enable Processor
        //
        MAP_IntMasterEnable();
        MAP_IntEnable(FAULT_SYSTICK);
    
        PRCMCC3200MCUInit();
    }
    
    //*****************************************************************************
    //
    //! Main function for spi demo application
    //!
    //! \param none
    //!
    //! \return None.
    //
    //*****************************************************************************
    void main()
    {
      unsigned long i=0;
      unsigned long j=0;
      unsigned long k=0;
        //
        // Initialize Board configurations
        //
        BoardInit();
    
        //
        // Muxing UART and SPI lines.
        //
        PinMuxConfig();
    
        //
        // Enable the SPI module clock
        //
        MAP_PRCMPeripheralClkEnable(PRCM_GSPI,PRCM_RUN_MODE_CLK);
    
        //
        // Initialising the Terminal.
        //
        InitTerm();
    
        //
        // Clearing the Terminal.
        //
        ClearTerm();
    
        //
        // Display the Banner
        //
        Message("\n\n\n\r");
        Message("\t\t   ********************************************\n\r");
        Message("\t\t        CC3200 SPI Demo Application  \n\r");
        Message("\t\t   ********************************************\n\r");
        Message("\n\n\n\r");
    
        //
        // Reset the peripheral
        //
        MAP_PRCMPeripheralReset(PRCM_GSPI);
        
        Spi_Init();
        
    
        while(1)
        {
           //Master_Send(g_ucTxBuff,10);
           //while(g_cDummy != 0x01);
             //g_cDummy = 0x00;
           Master_Receive(g_ucRxBuff,10);
           //Master_Receive();
           for(i=0;i<50000;i++)
           {}
             //for(j=0;j<40000;j++);
        }
        
        while(1);
        
    
    }
    
  • 更多主题相关例子访问 https://github.com/severin-kacianka/cc3200_dma_spi_example

  • 我也是用这两个demo,就是无法使用的,伙伴你怎么改的?

  • while(transfer_status != COMPLETE)一直卡着,中断服务函数没有进去