This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uart2配置dma



uart配置dma接收和发送应该都是一样的,可是为什么uart1可以正常运行,而uart2不行。

代码如下:

void
InitUART2Transfer(void)
{
unsigned int uIdx;

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART2);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART2);

HWREG(GPIO_PORTD_BASE+GPIO_O_LOCK)=GPIO_LOCK_KEY;
HWREG(GPIO_PORTD_BASE+GPIO_O_CR)=0xff;

ROM_UARTConfigSetExpClk(UART2_BASE, ROM_SysCtlClockGet(), 115200,
UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE);


ROM_UARTFIFOLevelSet(UART2_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);

ROM_UARTEnable(UART2_BASE);
ROM_UARTDMAEnable(UART2_BASE, UART_DMA_RX | UART_DMA_TX);

HWREG(UART2_BASE + UART_O_CTL) |= UART_CTL_LBE;


ROM_IntEnable(INT_UART2);

uDMAChannelSelectSecondary(UDMA_DEF_USBEP1RX_SEC_UART2RX);

ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_USBEP1RX,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);

ROM_uDMAChannelControlSet(UDMA_CHANNEL_USBEP1RX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);

ROM_uDMAChannelControlSet(UDMA_CHANNEL_USBEP1RX | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);

ROM_uDMAChannelTransferSet(UDMA_CHANNEL_USBEP1RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART2_BASE + UART_O_DR),
g_ui8RxBufA, sizeof(g_ui8RxBufA));

ROM_uDMAChannelTransferSet(UDMA_CHANNEL_USBEP1RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART2_BASE + UART_O_DR),
g_ui8RxBufB, sizeof(g_ui8RxBufB));

uDMAChannelSelectSecondary(UDMA_DEF_USBEP1TX_SEC_UART2TX);

ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_USBEP1TX,
UDMA_ATTR_ALTSELECT |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);

ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_USBEP1TX, UDMA_ATTR_USEBURST);

ROM_uDMAChannelControlSet(UDMA_CHANNEL_USBEP1TX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 | UDMA_DST_INC_NONE |
UDMA_ARB_4);

ROM_uDMAChannelTransferSet(UDMA_CHANNEL_USBEP1TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, tx_buf,
(void *)(UART2_BASE + UART_O_DR),
sizeof(tx_buf));

ROM_uDMAChannelEnable(UDMA_CHANNEL_USBEP1RX);
ROM_uDMAChannelEnable(UDMA_CHANNEL_USBEP1TX);
}

望大神指点一下...