This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在此向各位大侠请教一些问题,
1)在CC1310中,有类似zigbee中的短地址概念吗?其地址分配过程和zigbee类似吗?
2)concentrator和多个node之间是如何交互通信的?比如多个node节点给concentrator发消息,怎么解决冲突的问题的?网络中node的加入和断开状态,可以知道吗?
3)官网上看到一个支持CC1310的 TI-15.4 Stack: IEEE802.15.4e/g Standard Based Star Networking Software Development Kit (SDK),但是不支持433MHz,有支持433MHz的类似协议栈吗?
谢谢了!
1.CC1310星型网络中也存在地址管理,node address. 具体你可以参考TI例程 RF Wireless Sensor Network Concentrator 和 RF Wireless Sensor Network Node
2. Concentrator 一直处于接收状态,如果多个Node同时发送数据,会导致相互干扰,需要在节点端加LBT功能,参考TI listen before talk 例程。 网络中NODE加入和断开是Concentrator来管理的,所以它是知道。
3. 应该是支持433MHz, 协议是应用层,跟频率关系不大。主要是因为TI先出了US版本评估板,暂没有433M评估板。
好的,谢谢耐心解答!
2)在WSN例程中没看出来,哪里有管理网络状态改变的部分
3)collector_cc13xx配置文件config.h,只有一下这两种定义,如果我想用433MHz,应该修改哪边?
/*! PHY IDs - 915MHz US Frequency band operating mode # 1 */ #define APIMAC_STD_US_915_PHY_1 1 /*! 863MHz ETSI Frequency band operating mode #1 */ #define APIMAC_STD_ETSI_863_PHY_3 3
谢谢!
jad json 说:好的,谢谢耐心解答!
2)在WSN例程中没看出来,哪里有管理网络状态改变的部分
例程中只有增加节点添加,未对其节点做管理。需要用户自己添加功能。
3)collector_cc13xx配置文件config.h,只有一下这两种定义,如果我想用433MHz,应该修改哪边?
/*! PHY IDs - 915MHz US Frequency band operating mode # 1 */ #define APIMAC_STD_US_915_PHY_1 1 /*! 863MHz ETSI Frequency band operating mode #1 */ #define APIMAC_STD_ETSI_863_PHY_3 3射频配置完全不一样,需要smart sniffer生产配置。
谢谢!
1)例程中只有增加节点添加,未对其节点做管理。需要用户自己添加功能。
如果我想在此基础上,现实一个类似zigbee z-stack中,协调器建立网络,终端加入网络,并且获得终端的网络状态,这样一个组网建网功能,可以实现吗?可否给点建议?
2)射频配置完全不一样,需要smart sniffer生产配置。
smart sniffer?是用smartRF studio吧?你是说用smartRF studio就可以修改frequency对15.4 stack进行配置,实现433MHz的频率通信?
多谢了!