This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294 PWM时钟分频的问题。



使用函数  PWMClockSet() 不能给 PWM 分频,可能是哪边没有配置好啊 。急等。

大神们,有没有例程啊。跪求。

  • 你这个函数就不对吧。正确的应该是SysCtlPWMClockSet,给你个完整的PWM的例程看看

    //PWM实验程序解析
    //头文件
    #include <stdint.h>
    #include <stdbool.h>
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/rom.h"
    #include "driverlib/gpio.h"
    #include "driverlib/pwm.h"
    #include "driverlib/fpu.h"
    #include "driverlib/pin_map.h"
    
    int main (void)
    {
      //使能FPU
      FPUEnable();
      FPULazyStackingEnable();
    
      //设置系统时钟为50MHz
      SysCtlClockSet(SYSCTL_SYSDIV_4 |SYSCTL_USE_PLL 
    |SYSCTL_OSC_MAIN |SYSCTL_XTAL_16MHZ);
    
      //使能PWM模块
      ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM); 
      //使能PWM2和PWM3输出所在GPIO
      ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH); 
      //配置PH0/PH1为PWM功能
      ROM_GPIOPinTypePWM(GPIO_PORTH_BASE, GPIO_PIN_0); 
      ROM_GPIOPinTypePWM(GPIO_PORTH_BASE, GPIO_PIN_1); 
    
      // PWM时钟配置:不分频
      ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_1); 
      //配置PWM发生器1:加减计数 
      ROM_PWMGenConfigure(PWM_BASE,     
                        PWM_GEN_0,PWM_GEN_MODE_UP_DOWN 
    | PWM_GEN_MODE_NO_SYNC);
       //设置PWM发生器1的周期 
      ROM_PWMGenPeriodSet(PWM_BASE, PWM_GEN_0, 6000); 
      //设置PWM2/PWM3输出的脉冲宽度
      ROM_PWMPulseWidthSet(PWM_BASE, PWM_OUT_0, 4200); 
      ROM_PWMPulseWidthSet(PWM_BASE, PWM_OUT_1, 1800);
      //使能PWM2和PWM3的输出 
      ROM_PWMOutputState(PWM_BASE, (PWM_OUT_0_BIT | 
                           PWM_OUT_1_BIT), true);
      //使能PWM发生器1
      ROM_PWMGenEnable(PWM0_BASE, PWM_GEN_0); 
    
    while(1);
       {
       }
    }
    
  • 您好 谢谢您的回答。

    我用的芯片是TM4C1924   用 ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_1); 这个函数没有用  

    不能给PWM 分频。

    官网外设库手册貌似必须用 PWMClockSet()才对。---

    大神求助。。研究研究啊  帮帮我 要交货。

  • 您好 谢谢您的回答。

    我用的芯片是TM4C1924   用 ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_1); 这个函数没有用  

    不能给PWM 分频。

    官网外设库手册貌似必须用 PWMClockSet()才对。---

    大神求助。。研究研究啊  帮帮我 要交货。

  • 果然是这个函数,这个函数居然ROM中的和库中的不一样。你函数是如何写的呢?你是如何知道不能给PWM分配的呢?寄存器查看了没有。

  • peng xue 说:

    您好 谢谢您的回答。

    我用的芯片是TM4C1924   用 ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_1); 这个函数没有用  

    不能给PWM 分�。

    官网外设库手册貌似必须用 PWMClockSet()才对。---

    大神求助。。研究研究啊  帮帮我 要交货。

    //*****************************************************************************
    //
    //! Sets the PWM clock configuration.
    //!
    //! \param ui32Config is the configuration for the PWM clock; it must be one of
    //! \b SYSCTL_PWMDIV_1, \b SYSCTL_PWMDIV_2, \b SYSCTL_PWMDIV_4,
    //! \b SYSCTL_PWMDIV_8, \b SYSCTL_PWMDIV_16, \b SYSCTL_PWMDIV_32, or
    //! \b SYSCTL_PWMDIV_64.
    //!
    //! This function configures the rate of the clock provided to the PWM module
    //! as a ratio of the processor clock. This clock is used by the PWM module to
    //! generate PWM signals; its rate forms the basis for all PWM signals.
    //!
    //! \note This function should only be used with TM4C123 devices. For
    //! other TM4C devices, the PWMClockSet() function should be used.
    //!
    //! \note The clocking of the PWM is dependent on the system clock rate as
    //! configured by SysCtlClockSet().
    //!
    //! \return None.
    //
    //*****************************************************************************
    void
    SysCtlPWMClockSet(uint32_t ui32Config)
    {
    //
    // Check the arguments.
    //
    ASSERT((ui32Config == SYSCTL_PWMDIV_1) ||
    (ui32Config == SYSCTL_PWMDIV_2) ||
    (ui32Config == SYSCTL_PWMDIV_4) ||
    (ui32Config == SYSCTL_PWMDIV_8) ||
    (ui32Config == SYSCTL_PWMDIV_16) ||
    (ui32Config == SYSCTL_PWMDIV_32) ||
    (ui32Config == SYSCTL_PWMDIV_64));

    //
    // Check that there is a PWM block on this part.
    //
    ASSERT(HWREG(SYSCTL_DC1) & (SYSCTL_DC1_PWM0 | SYSCTL_DC1_PWM1));

    //
    // Set the PWM clock configuration into the run-mode clock configuration
    // register.
    //
    HWREG(SYSCTL_RCC) = ((HWREG(SYSCTL_RCC) &
    ~(SYSCTL_RCC_USEPWMDIV | SYSCTL_RCC_PWMDIV_M)) |
    ui32Config);
    }

    //*****************************************************************************
    ///
    //! Sets the PWM clock configuration.
    //!
    //! \param ui32Base is the base address of the PWM module.
    //! \param ui32Config is the configuration for the PWM clock; it must be one of
    //! \b PWM_SYSCLK_DIV_1, \b PWM_SYSCLK_DIV_2, \b PWM_SYSCLK_DIV_4,
    //! \b PWM_SYSCLK_DIV_8, \b PWM_SYSCLK_DIV_16, \b PWM_SYSCLK_DIV_32, or
    //! \b PWM_SYSCLK_DIV_64.
    //!
    //! This function sets the PWM clock divider as the PWM clock source. It also
    //! configures the clock frequency to the PWM module as a division of the
    //! system clock. This clock is used by the PWM module to generate PWM
    //! signals; its rate forms the basis for all PWM signals.
    //!
    //! \note This function should not be used with TM4C123 devices. For
    //! TM4C123 devices, the SysCtlPWMClockGet() function should be used.
    //!
    //! \note The clocking of the PWM is dependent upon the system clock rate as
    //! configured by SysCtlClockFreqSet().
    //!
    //! \return None.
    //
    //*****************************************************************************
    void
    PWMClockSet(uint32_t ui32Base, uint32_t ui32Config)
    {
    //
    // Check the arguments.
    //
    ASSERT((ui32Base == PWM0_BASE) || (ui32Base == PWM1_BASE));
    ASSERT((ui32Config == PWM_SYSCLK_DIV_2) ||
    (ui32Config == PWM_SYSCLK_DIV_4) ||
    (ui32Config == PWM_SYSCLK_DIV_8) ||
    (ui32Config == PWM_SYSCLK_DIV_16) ||
    (ui32Config == PWM_SYSCLK_DIV_32) ||
    (ui32Config == PWM_SYSCLK_DIV_64));

    //
    // Set the PWM clock configuration into the PWM clock configuration
    // register.
    //
    HWREG(ui32Base + PWM_O_CC) = ((HWREG(ui32Base + PWM_O_CC) &
    ~(PWM_CC_USEPWM | PWM_CC_PWMDIV_M)) |
    ui32Config);
    }

  • Maka 说:

    您好 谢谢您的回答。

    我用的芯片是TM4C1924   用 ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_1); 这个函数没有用  

    �能给PWM 分�。

    官网外设库手册貌似必须用 PWMClockSet()才对。---

    大神求助。。研究研究啊  帮帮我 要交货。

    //*****************************************************************************
    //
    //! Sets the PWM clock configuration.
    //!
    //! \param ui32Config is the configuration for the PWM clock; it must be one of
    //! \b SYSCTL_PWMDIV_1, \b SYSCTL_PWMDIV_2, \b SYSCTL_PWMDIV_4,
    //! \b SYSCTL_PWMDIV_8, \b SYSCTL_PWMDIV_16, \b SYSCTL_PWMDIV_32, or
    //! \b SYSCTL_PWMDIV_64.
    //!
    //! This function configures the rate of the clock provided to the PWM module
    //! as a ratio of the processor clock. This clock is used by the PWM module to
    //! generate PWM signals; its rate forms the basis for all PWM signals.
    //!
    //! \note This function should only be used with TM4C123 devices. For
    //! other TM4C devices, the PWMClockSet() function should be used.
    //!
    //! \note The clocking of the PWM is dependent on the system clock rate as
    //! configured by SysCtlClockSet().
    //!
    //! \return None.
    //
    //*****************************************************************************
    void
    SysCtlPWMClockSet(uint32_t ui32Config)
    {
    //
    // Check the arguments.
    //
    ASSERT((ui32Config == SYSCTL_PWMDIV_1) ||
    (ui32Config == SYSCTL_PWMDIV_2) ||
    (ui32Config == SYSCTL_PWMDIV_4) ||
    (ui32Config == SYSCTL_PWMDIV_8) ||
    (ui32Config == SYSCTL_PWMDIV_16) ||
    (ui32Config == SYSCTL_PWMDIV_32) ||
    (ui32Config == SYSCTL_PWMDIV_64));

    //
    // Check that there is a PWM block on this part.
    //
    ASSERT(HWREG(SYSCTL_DC1) & (SYSCTL_DC1_PWM0 | SYSCTL_DC1_PWM1));

    //
    // Set the PWM clock configuration into the run-mode clock configuration
    // register.
    //
    HWREG(SYSCTL_RCC) = ((HWREG(SYSCTL_RCC) &
    ~(SYSCTL_RCC_USEPWMDIV | SYSCTL_RCC_PWMDIV_M)) |
    ui32Config);
    }

    //*****************************************************************************
    ///
    //! Sets the PWM clock configuration.
    //!
    //! \param ui32Base is the base address of the PWM module.
    //! \param ui32Config is the configuration for the PWM clock; it must be one of
    //! \b PWM_SYSCLK_DIV_1, \b PWM_SYSCLK_DIV_2, \b PWM_SYSCLK_DIV_4,
    //! \b PWM_SYSCLK_DIV_8, \b PWM_SYSCLK_DIV_16, \b PWM_SYSCLK_DIV_32, or
    //! \b PWM_SYSCLK_DIV_64.
    //!
    //! This function sets the PWM clock divider as the PWM clock source. It also
    //! configures the clock frequency to the PWM module as a division of the
    //! system clock. This clock is used by the PWM module to generate PWM
    //! signals; its rate forms the basis for all PWM signals.
    //!
    //! \note This function should not be used with TM4C123 devices. For
    //! TM4C123 devices, the SysCtlPWMClockGet() function should be used.
    //!
    //! \note The clocking of the PWM is dependent upon the system clock rate as
    //! configured by SysCtlClockFreqSet().
    //!
    //! \return None.
    //
    //*****************************************************************************
    void
    PWMClockSet(uint32_t ui32Base, uint32_t ui32Config)
    {
    //
    // Check the arguments.
    //
    ASSERT((ui32Base == PWM0_BASE) || (ui32Base == PWM1_BASE));
    ASSERT((ui32Config == PWM_SYSCLK_DIV_2) ||
    (ui32Config == PWM_SYSCLK_DIV_4) ||
    (ui32Config == PWM_SYSCLK_DIV_8) ||
    (ui32Config == PWM_SYSCLK_DIV_16) ||
    (ui32Config == PWM_SYSCLK_DIV_32) ||
    (ui32Config == PWM_SYSCLK_DIV_64));

    //
    // Set the PWM clock configuration into the PWM clock configuration
    // register.
    //
    HWREG(ui32Base + PWM_O_CC) = ((HWREG(ui32Base + PWM_O_CC) &
    ~(PWM_CC_USEPWM | PWM_CC_PWMDIV_M)) |
    ui32Config);
    }

    [/quote]

    TM4C123X 和TM4C129X在配置PWM 时钟函数有不一样。

    1294就用void PWMClockSet(uint32_t ui32Base, uint32_t ui32Config) 是对的。

  • peng xue 说:

    使用函数  PWMClockSet() 不能给 PWM 分频,可能是哪边没有配置好啊 。急等。

    大神们,有没有例程啊。跪求。

    你的配置代码发上来看看 包括系统时钟配置函数。

  • 发现了,TM4C123和TM4C129x的就是不一样。奇怪的是ROM中的函数不应该都是一样的么?

  • ROM对应肯定也不一样,可以仔细对一下ROM函数。

  • peng xue 说:

    您好 谢谢您的回答。

    我用的芯片是TM4C1924   用 ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_1); 这个函数没有用  

    不能给PWM 分频。

    官网外设库手册貌似必须用 PWMClockSet()才对。---

    大神求助。。研究研究啊  帮帮我 要交货。

    TM4C1294用PWMClockSet(uint32_t ui32Base, uint32_t ui32Config) 是正确的,但是还是建议把代码上传上来分析。

  • 到现在居然才发现这个问题,TM4C123x和TM4C129x用的是一个.lib函数库,但是却有两个ROM的函数库,官方为什么不统一呢。一直用的TM4C123x居然没发现这个问题。

  • 谢谢哈,项目问题暂时通过调节 周期和占空比解决。  

  • 帖子里 回复的内容 怎么都回复给自己了???

  • TI的回复,是通过邮件订阅通知的。不像普通论坛那样,给你回复了才通知。