This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1231H6PMI 进不去中断 求解



我要用TIMER使LED灯亮
但进不去中断

int sys_status;

void
IRQ_Timer0AIntHandler(void)
{
MAP_IntMasterDisable();
MAP_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);

switch (sys_status)
{
case 0:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_4, GPIO_PIN_4);
sys_status = 1;
break;
case 1:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_4, 0);
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_5, GPIO_PIN_5);
sys_status = 2;
break;
case 2:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_5, 0);
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_6, GPIO_PIN_6);
sys_status = 3;
break;
case 3:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_6, 0);
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_7, GPIO_PIN_7);
sys_status = 4;
break;
case 4:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_7, 0);
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, GPIO_PIN_0);
sys_status = 5;
break;
case 5:
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, 0);
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1);
sys_status = 6;
break;
case 6:
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0);
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2);
sys_status = 7;
break;
case 7:
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0);
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, GPIO_PIN_3);
sys_status = 8;
break;
case 8:
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0);
sys_status = 0;
break;
default :
sys_status = 0;
break;
}
MAP_IntMasterEnable();
}

int
main(void)
{
MAP_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);

MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART3);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART4);

MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

MAP_GPIOPinConfigure(GPIO_PA0_U0RX);
MAP_GPIOPinConfigure(GPIO_PA1_U0TX);
MAP_GPIOPinConfigure(GPIO_PC4_U4RX);
MAP_GPIOPinConfigure(GPIO_PC5_U4TX);
MAP_GPIOPinConfigure(GPIO_PC6_U3RX);
MAP_GPIOPinConfigure(GPIO_PC7_U3TX);

HWREG(GPIO_PORTF_BASE + 0x520) = 0x4C4F434B;
HWREG(GPIO_PORTF_BASE + 0x524) = 0x00FF;
HWREG(GPIO_PORTF_BASE + 0x420) = 0x0000;
HWREG(GPIO_PORTF_BASE + 0x51C) = 0x001F;

MAP_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
MAP_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_4 | GPIO_PIN_5);
MAP_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);

MAP_GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7);
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_4);

MAP_UARTConfigSetExpClk(UART0_BASE, MAP_SysCtlClockGet(), 9600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));//115200


MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);

MAP_TimerDisable(TIMER0_BASE, TIMER_A);
MAP_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC | TIMER_CFG_A_PERIODIC);
MAP_TimerLoadSet(TIMER0_BASE, TIMER_A, MAP_SysCtlClockGet());
MAP_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
MAP_IntEnable(INT_TIMER0A);
MAP_TimerEnable(TIMER0_BASE, TIMER_A);

sys_status = 0;

while(1)
{
}
}

  • 向量表中的中断服务函数没有安装吧。

  • 不好意思,請問下向量表是指甚麼?

    是加入这行吗?

    void IRQ_Timer0AIntHandler(void);

    加了但没有作用

    不懂如何安裝中斷服務函數

  • #pragma DATA_SECTION(g_pfnVectors, ".intvecs")
    void (* const g_pfnVectors[])(void) =
    {
        (void (*)(void))((uint32_t)&__STACK_TOP),
                                                // The initial stack pointer
        ResetISR,                               // The reset handler
        NmiSR,                                  // The NMI handler
        FaultISR,                               // The hard fault handler
        IntDefaultHandler,                      // The MPU fault handler
        IntDefaultHandler,                      // The bus fault handler
        IntDefaultHandler,                      // The usage fault handler
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // SVCall handler
        IntDefaultHandler,                      // Debug monitor handler
        0,                                      // Reserved
        IntDefaultHandler,                      // The PendSV handler
        IntDefaultHandler,                      // The SysTick handler
        IntDefaultHandler,                      // GPIO Port A
        IntDefaultHandler,                      // GPIO Port B
        IntDefaultHandler,                      // GPIO Port C
        IntDefaultHandler,                      // GPIO Port D
        IntDefaultHandler,                      // GPIO Port E
        IntDefaultHandler,                      // UART0 Rx and Tx
        IntDefaultHandler,                      // UART1 Rx and Tx
        IntDefaultHandler,                      // SSI0 Rx and Tx
        IntDefaultHandler,                      // I2C0 Master and Slave
        IntDefaultHandler,                      // PWM Fault
        IntDefaultHandler,                      // PWM Generator 0
        IntDefaultHandler,                      // PWM Generator 1
        IntDefaultHandler,                      // PWM Generator 2
        IntDefaultHandler,                      // Quadrature Encoder 0
        IntDefaultHandler,                      // ADC Sequence 0
        IntDefaultHandler,                      // ADC Sequence 1
        IntDefaultHandler,                      // ADC Sequence 2
        IntDefaultHandler,                      // ADC Sequence 3
        IntDefaultHandler,                      // Watchdog timer
        IntDefaultHandler,                      // Timer 0 subtimer A
        IntDefaultHandler,                      // Timer 0 subtimer B
        IntDefaultHandler,                      // Timer 1 subtimer A
        IntDefaultHandler,                      // Timer 1 subtimer B
        IntDefaultHandler,                      // Timer 2 subtimer A
        IntDefaultHandler,                      // Timer 2 subtimer B
        IntDefaultHandler,                      // Analog Comparator 0
        IntDefaultHandler,                      // Analog Comparator 1
        IntDefaultHandler,                      // Analog Comparator 2
        IntDefaultHandler,                      // System Control (PLL, OSC, BO)
        IntDefaultHandler,                      // FLASH Control
        IntDefaultHandler,                      // GPIO Port F
        IntDefaultHandler,                      // GPIO Port G
        IntDefaultHandler,                      // GPIO Port H
        IntDefaultHandler,                      // UART2 Rx and Tx
        IntDefaultHandler,                      // SSI1 Rx and Tx
        IntDefaultHandler,                      // Timer 3 subtimer A
        IntDefaultHandler,                      // Timer 3 subtimer B
        IntDefaultHandler,                      // I2C1 Master and Slave
        IntDefaultHandler,                      // Quadrature Encoder 1
        IntDefaultHandler,                      // CAN0
        IntDefaultHandler,                      // CAN1
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // Hibernate
        IntDefaultHandler,                      // USB0
        IntDefaultHandler,                      // PWM Generator 3
        IntDefaultHandler,                      // uDMA Software Transfer
        IntDefaultHandler,                      // uDMA Error
        IntDefaultHandler,                      // ADC1 Sequence 0
        IntDefaultHandler,                      // ADC1 Sequence 1
        IntDefaultHandler,                      // ADC1 Sequence 2
        IntDefaultHandler,                      // ADC1 Sequence 3
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // GPIO Port J
        IntDefaultHandler,                      // GPIO Port K
        IntDefaultHandler,                      // GPIO Port L
        IntDefaultHandler,                      // SSI2 Rx and Tx
        IntDefaultHandler,                      // SSI3 Rx and Tx
        IntDefaultHandler,                      // UART3 Rx and Tx
        IntDefaultHandler,                      // UART4 Rx and Tx
        IntDefaultHandler,                      // UART5 Rx and Tx
        IntDefaultHandler,                      // UART6 Rx and Tx
        IntDefaultHandler,                      // UART7 Rx and Tx
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // I2C2 Master and Slave
        IntDefaultHandler,                      // I2C3 Master and Slave
        IntDefaultHandler,                      // Timer 4 subtimer A
        IntDefaultHandler,                      // Timer 4 subtimer B
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // Timer 5 subtimer A
        IntDefaultHandler,                      // Timer 5 subtimer B
        IntDefaultHandler,                      // Wide Timer 0 subtimer A
        IntDefaultHandler,                      // Wide Timer 0 subtimer B
        IntDefaultHandler,                      // Wide Timer 1 subtimer A
        IntDefaultHandler,                      // Wide Timer 1 subtimer B
        IntDefaultHandler,                      // Wide Timer 2 subtimer A
        IntDefaultHandler,                      // Wide Timer 2 subtimer B
        IntDefaultHandler,                      // Wide Timer 3 subtimer A
        IntDefaultHandler,                      // Wide Timer 3 subtimer B
        IntDefaultHandler,                      // Wide Timer 4 subtimer A
        IntDefaultHandler,                      // Wide Timer 4 subtimer B
        IntDefaultHandler,                      // Wide Timer 5 subtimer A
        IntDefaultHandler,                      // Wide Timer 5 subtimer B
        IntDefaultHandler,                      // FPU
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // I2C4 Master and Slave
        IntDefaultHandler,                      // I2C5 Master and Slave
        IntDefaultHandler,                      // GPIO Port M
        IntDefaultHandler,                      // GPIO Port N
        IntDefaultHandler,                      // Quadrature Encoder 2
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // GPIO Port P (Summary or P0)
        IntDefaultHandler,                      // GPIO Port P1
        IntDefaultHandler,                      // GPIO Port P2
        IntDefaultHandler,                      // GPIO Port P3
        IntDefaultHandler,                      // GPIO Port P4
        IntDefaultHandler,                      // GPIO Port P5
        IntDefaultHandler,                      // GPIO Port P6
        IntDefaultHandler,                      // GPIO Port P7
        IntDefaultHandler,                      // GPIO Port Q (Summary or Q0)
        IntDefaultHandler,                      // GPIO Port Q1
        IntDefaultHandler,                      // GPIO Port Q2
        IntDefaultHandler,                      // GPIO Port Q3
        IntDefaultHandler,                      // GPIO Port Q4
        IntDefaultHandler,                      // GPIO Port Q5
        IntDefaultHandler,                      // GPIO Port Q6
        IntDefaultHandler,                      // GPIO Port Q7
        IntDefaultHandler,                      // GPIO Port R
        IntDefaultHandler,                      // GPIO Port S
        IntDefaultHandler,                      // PWM 1 Generator 0
        IntDefaultHandler,                      // PWM 1 Generator 1
        IntDefaultHandler,                      // PWM 1 Generator 2
        IntDefaultHandler,                      // PWM 1 Generator 3
        IntDefaultHandler                       // PWM 1 Fault
    };

    要在这里把你的中断服务函数加进去的。

  • 有的,我有加入了,但还是没有亮,也没有ERROR

    __root const uVectorEntry __vector_table[] @ ".intvec" =
    {
        { .ui32Ptr = (uint32_t)pui32Stack + sizeof(pui32Stack) },
                                                // The initial stack pointer
        ResetISR,                               // The reset handler
        NmiSR,                                  // The NMI handler
        FaultISR,                               // The hard fault handler
        IntDefaultHandler,                      // The MPU fault handler
        IntDefaultHandler,                      // The bus fault handler
        IntDefaultHandler,                      // The usage fault handler
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // SVCall handler
        IntDefaultHandler,                      // Debug monitor handler
        0,                                      // Reserved
        IntDefaultHandler,                      // The PendSV handler
        IntDefaultHandler,                      // The SysTick handler
        IntDefaultHandler,                               // GPIO Port A
        IntDefaultHandler,                               // GPIO Port B
        IntDefaultHandler,                               // GPIO Port C
        IntDefaultHandler,                      // GPIO Port D
        IntDefaultHandler,                      // GPIO Port E
    //    IRQ_UI_UARTIntHandler,                      // UART0 Rx and Tx
        IntDefaultHandler,                      // UART1 Rx and Tx
        IntDefaultHandler,                      // SSI0 Rx and Tx
        IntDefaultHandler,                      // I2C0 Master and Slave
        IntDefaultHandler,                      // PWM Fault
        IntDefaultHandler,                      // PWM Generator 0
        IntDefaultHandler,                      // PWM Generator 1
        IntDefaultHandler,                      // PWM Generator 2
        IntDefaultHandler,                      // Quadrature Encoder 0
        IntDefaultHandler,                      // ADC Sequence 0
        IntDefaultHandler,                      // ADC Sequence 1
        IntDefaultHandler,                      // ADC Sequence 2
        IntDefaultHandler,                      // ADC Sequence 3
        IntDefaultHandler,                      // Watchdog timer
        IRQ_Timer0AIntHandler,                      // Timer 0 subtimer A
        IntDefaultHandler,                      // Timer 0 subtimer B
        IntDefaultHandler,                      // Timer 1 subtimer A
        IntDefaultHandler,                      // Timer 1 subtimer B
        IntDefaultHandler,                      // Timer 2 subtimer A
        IntDefaultHandler,                      // Timer 2 subtimer B
        IntDefaultHandler,                      // Analog Comparator 0
        IntDefaultHandler,                      // Analog Comparator 1
        IntDefaultHandler,                      // Analog Comparator 2
        IntDefaultHandler,                      // System Control (PLL, OSC, BO)
        IntDefaultHandler,                      // FLASH Control
        IntDefaultHandler,                      // GPIO Port F
        IntDefaultHandler,                      // GPIO Port G
        IntDefaultHandler,                      // GPIO Port H
        IntDefaultHandler,                      // UART2 Rx and Tx
        IntDefaultHandler,                      // SSI1 Rx and Tx
        IntDefaultHandler,                      // Timer 3 subtimer A
        IntDefaultHandler,                      // Timer 3 subtimer B
        IntDefaultHandler,                      // I2C1 Master and Slave
        IntDefaultHandler,                      // Quadrature Encoder 1
        IntDefaultHandler,                      // CAN0
        IntDefaultHandler,                      // CAN1
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // Hibernate
        IntDefaultHandler,                      // USB0
        IntDefaultHandler,                      // PWM Generator 3
        IntDefaultHandler,                      // uDMA Software Transfer
        IntDefaultHandler,                      // uDMA Error
        IntDefaultHandler,                      // ADC1 Sequence 0
        IntDefaultHandler,                      // ADC1 Sequence 1
        IntDefaultHandler,                      // ADC1 Sequence 2
        IntDefaultHandler,                      // ADC1 Sequence 3
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // GPIO Port J
        IntDefaultHandler,                      // GPIO Port K
        IntDefaultHandler,                      // GPIO Port L
        IntDefaultHandler,                      // SSI2 Rx and Tx
        IntDefaultHandler,                      // SSI3 Rx and Tx
    //    IRQ_BLE_UARTIntHandler,                      // UART3 Rx and Tx
    //    IRQ_AIT_UARTIntHandler,                      // UART4 Rx and Tx
        IntDefaultHandler,                      // UART5 Rx and Tx
        IntDefaultHandler,                      // UART6 Rx and Tx
        IntDefaultHandler,                      // UART7 Rx and Tx
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // I2C2 Master and Slave
        IntDefaultHandler,                      // I2C3 Master and Slave
        IntDefaultHandler,                      // Timer 4 subtimer A
        IntDefaultHandler,                      // Timer 4 subtimer B
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // Timer 5 subtimer A
        IntDefaultHandler,                      // Timer 5 subtimer B
        IntDefaultHandler,                      // Wide Timer 0 subtimer A
        IntDefaultHandler,                      // Wide Timer 0 subtimer B
    //    IRQ_WTimer1AIntHandler,                      // Wide Timer 1 subtimer A
    //    IRQ_WTimer1BIntHandler,                      // Wide Timer 1 subtimer B
        IntDefaultHandler,                      // Wide Timer 2 subtimer A
        IntDefaultHandler,                      // Wide Timer 2 subtimer B
        IntDefaultHandler,                      // Wide Timer 3 subtimer A
        IntDefaultHandler,                      // Wide Timer 3 subtimer B
        IntDefaultHandler,                      // Wide Timer 4 subtimer A
        IntDefaultHandler,                      // Wide Timer 4 subtimer B
        IntDefaultHandler,                      // Wide Timer 5 subtimer A
        IntDefaultHandler,                      // Wide Timer 5 subtimer B
        IntDefaultHandler,                      // FPU
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // I2C4 Master and Slave
        IntDefaultHandler,                      // I2C5 Master and Slave
        IntDefaultHandler,                      // GPIO Port M
        IntDefaultHandler,                      // GPIO Port N
        IntDefaultHandler,                      // Quadrature Encoder 2
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // GPIO Port P (Summary or P0)
        IntDefaultHandler,                      // GPIO Port P1
        IntDefaultHandler,                      // GPIO Port P2
        IntDefaultHandler,                      // GPIO Port P3
        IntDefaultHandler,                      // GPIO Port P4
        IntDefaultHandler,                      // GPIO Port P5
        IntDefaultHandler,                      // GPIO Port P6
        IntDefaultHandler,                      // GPIO Port P7
        IntDefaultHandler,                      // GPIO Port Q (Summary or Q0)
        IntDefaultHandler,                      // GPIO Port Q1
        IntDefaultHandler,                      // GPIO Port Q2
        IntDefaultHandler,                      // GPIO Port Q3
        IntDefaultHandler,                      // GPIO Port Q4
        IntDefaultHandler,                      // GPIO Port Q5
        IntDefaultHandler,                      // GPIO Port Q6
        IntDefaultHandler,                      // GPIO Port Q7
        IntDefaultHandler,                      // GPIO Port R
        IntDefaultHandler,                      // GPIO Port S
        IntDefaultHandler,                      // PWM 1 Generator 0
        IntDefaultHandler,                      // PWM 1 Generator 1
        IntDefaultHandler,                      // PWM 1 Generator 2
        IntDefaultHandler,                      // PWM 1 Generator 3
        IntDefaultHandler                       // PWM 1 Fault
    };
  • 问题解决了,谢谢解答!