This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

*Enable函数



就是配置UART0是没有用UARTEnable函数,而在配置ADC、SPI等的时候有对应的这个ADCSequenceEnable、SSIEnable。额,这是为什么???

  • 你加上这个,肯定是没错的。但为什么没加也可以用呢,有可能是你用的库中,比如初始化函数结束后,直接就在这个函数中使能了,但由于库是封装的,你看不到而已。

  • 在调用这个函数中使能UART 

    void
    UARTConfigSetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk,
    uint32_t ui32Baud, uint32_t ui32Config)
    {
    uint32_t ui32Div;

    //
    // Check the arguments.
    //
    ASSERT(_UARTBaseValid(ui32Base));
    ASSERT(ui32Baud != 0);
    ASSERT(ui32UARTClk >= (ui32Baud * UART_CLK_DIVIDER));

    //
    // Stop the UART.
    //
    UARTDisable(ui32Base);

    //
    // Is the required baud rate greater than the maximum rate supported
    // without the use of high speed mode?
    //
    if((ui32Baud * 16) > ui32UARTClk)
    {
    //
    // Enable high speed mode.
    //
    HWREG(ui32Base + UART_O_CTL) |= UART_CTL_HSE;

    //
    // Half the supplied baud rate to compensate for enabling high speed
    // mode. This allows the following code to be common to both cases.
    //
    ui32Baud /= 2;
    }
    else
    {
    //
    // Disable high speed mode.
    //
    HWREG(ui32Base + UART_O_CTL) &= ~(UART_CTL_HSE);
    }

    //
    // Compute the fractional baud rate divider.
    //
    ui32Div = (((ui32UARTClk * 8) / ui32Baud) + 1) / 2;

    //
    // Set the baud rate.
    //
    HWREG(ui32Base + UART_O_IBRD) = ui32Div / 64;
    HWREG(ui32Base + UART_O_FBRD) = ui32Div % 64;

    //
    // Set parity, data length, and number of stop bits.
    //
    HWREG(ui32Base + UART_O_LCRH) = ui32Config;

    //
    // Clear the flags register.
    //
    HWREG(ui32Base + UART_O_FR) = 0;

    //
    // Start the UART.
    //
    UARTEnable(ui32Base);
    }