This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP FET 连接 MSP 432 问题



从网上买了MSP FET 和 MSP-FET-432ADPTR 连接 MSP ‑ ‑ EXP432P401R launchpad(红色版本), IDE是IAR 7.70.1

驱动安装没有问题(MSP Application UART1(COM13) 和 MSP Debug Interface(COM6)),现在启动debug,

报错:could not find device (or device not supported), 试了CCS 6.2也是有问题

我参考了红板的文档,把J101的跳帽全部拿掉(除3.3v, 5v 和 GND),红板用USB供电。

转接板用的10Pin的接到红板的J8, 转接板的S1在左侧位置,

这里有个疑问:转接板的14Pin接头怎么跟FET的接头都是母的,不能直接连接

我就用几根针把它们连起来

不知道问题在哪, 谢谢