This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SM470R1B1M-HT



1、可以使用片内的1M的flash空间进行数据的存储,来进行掉电数据保护吗?

2、问题1答案是可以得话,下载的程序存到哪里了呢?是不是可以通过IAR设置程序的地址?

3、问题1答案是可以得话,存储数据的地址可以自己确定吗?,可编程地址如下:

       

    请问,RAM、FLASH、HET RAM的地址分别是多少?

4、如果可以存储数据的话,存储的时候,看到这句话:

      

      请问,这个芯片写入的时候是可以2个2个字节写入对吧?那写之前要进行擦除吗?是不是按页(16K字节)擦除?对于已经有数据的地址再写数据时,要擦除吗?

5、在其总的手册中有以下一句话: ,请问,这个50000是指读写次数吗?那么这个次数是怎么算的呢?①是每bit可以进行50000次读写,②还是读写1次就算1次?比如,对flash中的8个字,64bit进行每2个字节的间断性写操作,过程中是对每bit进行操作,按第1中解释,那么其实算使用掉了1次读写机会;按第2种解释,写了8/2=4次,使用掉了4次读写机会。