This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART485口,为什么芯片发送的数据一直是00?



#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "inc/hw_types.h"
#include "driverlib/fpu.h"
#include "driverlib/debug.h"
#include "driverlib/pwm.h"
#include "inc/hw_gpio.h"

#define UARTConfigSet(a, b, c) UARTConfigSetExpClk(a, 16000000, b, c)
#define NUM_UART_DATA 4
#define GPIO_PA5_U3TX 0x00001401
#define GPIO_PA4_U3RX 0x00001001
uint8_t ui8DataTx[NUM_UART_DATA];
/*char SerialRxData[200];

int SerialDataCount = 0;

void
UARTSend(const uint8_t *pui8Buffer, unsigned long ui32Count)
{
while(ui32Count--)
{
UARTCharPut(UART5_BASE, *pui8Buffer++);
}

}*/
///


int main(void)
{
void UARTSend();
void uartPuts();
// char c;
uint32_t ui32SysClock;
ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);

/*
IntMasterDisable();
IntEnable(SYSCTL_OSC_INT);
*/
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);//ʹÄÜGPIOA¿Ú
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART3);
GPIOPinConfigure(GPIO_PA4_U3RX);
GPIOPinConfigure(GPIO_PA5_U3TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_4 | GPIO_PIN_5);
//UARTClockSourceSet(UART3_BASE,UART_CLOCK_PIOSC);

UARTConfigSet(UART3_BASE, 9600, (UART_CONFIG_WLEN_8 |
UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));

//µãÁÁLED
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH);//ʹÄÜGPIOH¿Ú
GPIODirModeSet(GPIO_PORTH_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,GPIO_DIR_MODE_OUT);
GPIOPadConfigSet(GPIO_PORTH_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,GPIO_STRENGTH_8MA_SC,GPIO_PIN_TYPE_STD);

GPIOPinWrite(GPIO_PORTH_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,0x00);///½ÓÊÕµ½Êý¾Ý£¬ÁÁµÆ
SysCtlDelay(1000 * (ui32SysClock/ 3000));///ÑÓʱ³ÌÐò
GPIOPinWrite(GPIO_PORTH_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,0xff);///½ÓÊÕµ½Êý¾Ý£¬ÁÁµÆ
SysCtlDelay(1000 * (ui32SysClock/ 3000));///ÑÓʱ³ÌÐò

ui8DataTx[0] = 'u';
ui8DataTx[1] = 'a';
ui8DataTx[2] = 'r';
ui8DataTx[3] = 't';

while(1)
{
//uartPuts("HELLO EEWORLD:\r\n"); // ÇëÊäÈëÒ»¸öÃüÁ°´»Ø³µÖ´ÐÐ
UARTSend(UART3_BASE, (uint8_t *)"0101", NUM_UART_DATA);
GPIOPinWrite(GPIO_PORTH_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,0x00);///½ÓÊÕµ½Êý¾Ý£¬ÁÁµÆ
SysCtlDelay(1000 * (ui32SysClock/ 3000));///ÑÓʱ³ÌÐò
GPIOPinWrite(GPIO_PORTH_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,0xff);///½ÓÊÕµ½Êý¾Ý£¬ÁÁµÆ
SysCtlDelay(1000 * (ui32SysClock/ 3000));///ÑÓʱ³ÌÐò

/* c=UARTCharGet(UART3_BASE);

if(c=='1')
{
GPIOPinWrite(GPIO_PORTH_BASE,GPIO_PIN_3,0x07);///½ÓÊÕµ½Êý¾Ý£¬ÁÁµÆ
SysCtlDelay(1000 * (ui32SysClock/ 3000));///ÑÓʱ³ÌÐò
}
if(c=='0')
{
GPIOPinWrite(GPIO_PORTH_BASE,GPIO_PIN_3,0xff);///½ÓÊÕµ½Êý¾Ý£¬ÁÁµÆ
SysCtlDelay(1000 * (ui32SysClock/ 3000));///ÑÓʱ³ÌÐò
}
SerialRxData[SerialDataCount]=UARTCharGet(UART3_BASE);///²»½ÓÊÕµ½Êý¾Ý£¬µÈ´ý
if(SerialRxData[SerialDataCount])
{
GPIOPinWrite(GPIO_PORTH_BASE,GPIO_PIN_3,0x07);///½ÓÊÕµ½Êý¾Ý£¬ÁÁµÆ
SysCtlDelay(1000 * (ui32SysClock/ 3000));///ÑÓʱ³ÌÐò
}*/

}

}
void
UARTSend(uint32_t ui32UARTBase, const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
//
MAP_UARTCharPut(ui32UARTBase, *pui8Buffer++);
}
}
// ͨ¹ýUART·¢ËÍÒ»¸ö×Ö·û
void uartPutc(const char c)
{
UARTCharPut(UART3_BASE, c);
}

// ͨ¹ýUART·¢ËÍ×Ö·û´®
void uartPuts(const char *s)
{
while (*s != '\0')
{
//UARTCharPut(UART3_BASE, *(s++));
uartPutc(*(s++));
}

}