This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急急急,关于TM4C123GXLADC功能实现???



各位前辈你们好;

         TM4C123GXL的40个引脚的供电是不是也有USBdebug或Device完成实现,+3.3V和+5V是什么意思,我想外接一个传感器,利用ADC来采集数据需要将R25和R29接起来吗?传感器的电源和GND需要和班子的5V引脚和GND连接吗???????

            

 

                                                                                                                                                            谢谢

  • 1.5V是usb提供的,这个不一定可以到5V。3.3V是芯片的供电电压,是usb的5V经过一个LDO提供的。

    2.R25和R29和这个没关系,这两个短接是直接接IO的.直接GND和电源连接起来就好了。