我是一名新手,最近运行了usb_dev_bulk例程,在c:\program files\Texas Instruments\stellaris\usb_example找不到usb_bulk_example.exe测试工具,根本就没有找到c盘下的文件,驱动没有问题,搜索电脑也没有usb_bulk_example.exe,是不是哪里出了问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
USB Bulk Example (usb_bulk_example)
-----------------------------------
This Windows command line application is written using C for Windows
and should be built using Microsoft Visual Studio 2008. Project
file usb_bulk_example.vcproj is provided to build the application.
USB communication with the Tiva boards running the usb_dev_bulk sample
application is performed using the LMUSBDLL interface which is a thin wrapper
over the Microsoft WinUSB API. The relevant WinUSB subsystem files and the
LMUSBDLL.dll are installed when you first connect the board to a Windows host
via USB and install the drivers. Device drivers for the usb_dev_bulk device
can be found in the windows_drivers subdirectory under
"C:\TI\TivaWare for X Series", where "X" indicates the Tiva series for which
the software was installed.
The LMUSBDLL interface is provided purely to allow the sample applications
to be compiled and run in the absence of the Windows Device Driver Kit
(DDK). The WinUSB API header and library files are not included in the
Windows SDK shipped with Visual Studio 2008 so any code which uses this
interface requires access to the DDK to build. LMUSBDLL contains all
the application code requiring WinUSB so applications may link to it
without the need for the Windows DDK.
看说明,上面我给出的目录下的例程,用VS2008编译下,就是一个命令行工具了。