Other Parts Discussed in Thread: EK-TM4C123GXL
TI工程师您好!我用的是官方的例程,tivaware下ek-tm4c123gxl的USB_DEV_serial例程,程序可以运行,Windows下也安装了CDC的驱动并虚拟出来个串口,但是我用串口助手发送数据却没有任何数据返回,程序可以进入USBUARTIntHandler中断,但状态是发送,在PC端却接收不到任何数据,为什么?我用UARTprintf发送数据也收不到任何数据,我应该怎么调试?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: EK-TM4C123GXL
TI工程师您好!我用的是官方的例程,tivaware下ek-tm4c123gxl的USB_DEV_serial例程,程序可以运行,Windows下也安装了CDC的驱动并虚拟出来个串口,但是我用串口助手发送数据却没有任何数据返回,程序可以进入USBUARTIntHandler中断,但状态是发送,在PC端却接收不到任何数据,为什么?我用UARTprintf发送数据也收不到任何数据,我应该怎么调试?
我通过仿真,确定串口发送的数据,USB端都正确的收到并读取,然后数据直接通过ROM_UARTChartPutNonBlovking放入USB的发送FIFO中,但PC端却没收到数据,不知道为什么?我的USB只接了4根线,电源,地,DP,DM。
测试的怎么样?我想知道是硬件问题还是软件问题,还是测试方法问题。
USB_dev_bulk例程怎么测试?我写于了这个例程,但不知道怎么测试,它不像CDC那么好测试。CDC用串口调试助手就可以了,这也是我选择CDC的原因。
USB Generic Bulk Device
This example provides a generic USB device offering simple bulk data
transfer to and from the host. The device uses a vendor-specific class ID
and supports a single bulk IN endpoint and a single bulk OUT endpoint.
Data received from the host is assumed to be ASCII text and it is
echoed back with the case of all alphabetic characters swapped.
A Windows INF file for the device is provided on the installation CD and
in the C:/ti/TivaWare-for-C-Series/windows_drivers directory of TivaWare C
series releases. This INF contains information required to install the
WinUSB subsystem on Windowi16XP and Vista PCs. WinUSB is a Windows
subsystem allowing user mode applications to access the USB device without
the need for a vendor-specific kernel mode driver.
A sample Windows command-line application, usb_bulk_example, illustrating
how to connect to and communicate with the bulk device is also provided.
The application binary is installed as part of the ''Windows-side examples
for USB kits'' package (SW-USB-win) on the installation CD or via download
from http://www.ti.com/tivaware . Project files are included to allow
the examples to be built using Microsoft VisualStudio 2008. Source code
for this application can be found in directory
TivaWare-for-C-Series/tools/usb_bulk_example.
根据官方的说法,用VS2008编译生成一个软件,然后就可以交互运行了。