This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于cortex-m4 UART的技术问题请教



UART有8个串口,UART0调试正常(有范例)但配置在UART1/2/3/4/5/6/7都不能正常通讯,不知道是怎么回事。配置了GPIO pin脚的功能还是无法通信

如题,相同代码按照uart0配置可以通信,换成uart1不行,tivac 123M4H6PM

int main (void)

{
char cThisChar;
//SysCtlClockSet(SYSCTL_SYSDIV_4|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
SysCtlClockSet(SYSCTL_SYSDIV_1|SYSCTL_USE_OSC|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);

SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

GPIOPinConfigure(GPIO_PB0_U1RX);
GPIOPinConfigure(GPIO_PB1_U1TX);

GPIOPinTypeUART(GPIO_PORTB_BASE,GPIO_PIN_0|GPIO_PIN_1);

UARTConfigSetExpClk(UART1_BASE,SysCtlClockGet(),115200,(UART_CONFIG_WLEN_8|UART_CONFIG_STOP_ONE|UART_CONFIG_PAR_NONE));


UARTCharPut(UART1_BASE,'!');
do
{
cThisChar=UARTCharGet(UART1_BASE);
UARTCharPut(UART1_BASE,cThisChar);

}while ((cThisChar!='\n')&&(cThisChar!='\r'));
return(0);

}


  • 我配置串口1,没有问题

    //                        sensor.
    //
    // Copyright (c) 2010-2017 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    //   Redistribution and use in source and binary forms, with or without
    //   modification, are permitted provided that the following conditions
    //   are met:
    //
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    //
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the
    //   distribution.
    //
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // 
    // This is part of revision 2.1.4.178 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_memmap.h"
    #include "driverlib/adc.h"
    #include "driverlib/gpio.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //
    //! \addtogroup adc_examples_list
    //! <h1>ADC Temperature Sensor (temperature_sensor)</h1>
    //!
    //! This example shows how to setup ADC0 to read the internal temperature
    //! sensor.
    //!
    //! NOTE: The internal temperature sensor is not calibrated.  This example
    //! just takes the raw temperature sensor sample and converts it using the
    //! equation found in the LM3S9B96 datasheet.
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - ADC0 peripheral
    //!
    //! The following UART signals are configured only for displaying console
    //! messages for this example.  These are not required for operation of the
    //! ADC.
    //! - UART0 peripheral
    //! - GPIO Port A peripheral (for UART0 pins)
    //! - UART0RX - PA0
    //! - UART0TX - PA1
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - None.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // This function sets up UART0 to be used for a console to display information
    // as the example is running.
    //
    //*****************************************************************************
    void
    InitConsole(void)
    {
        //
        // Enable GPIO port A which is used for UART0 pins.
        // TODO: change this to whichever GPIO port you are using.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    
        //
        // Configure the pin muxing for UART0 functions on port A0 and A1.
        // This step is not necessary if your part does not support pin muxing.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinConfigure(GPIO_PB0_U1RX);
        GPIOPinConfigure(GPIO_PB1_U1TX);
    
        //
        // Enable UART0 so that we can configure the clock.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
    
        //
        // Use the internal 16MHz oscillator as the UART clock source.
        //
        UARTClockSourceSet(UART1_BASE, UART_CLOCK_PIOSC);
    
        //
        // Select the alternate (UART) function for these pins.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    
        //
        // Initialize the UART for console I/O.
        //
        UARTStdioConfig(1, 115200, 16000000);
    }
    
    int main(void)
    {
        uint32_t ui32ADC0Value[4];
        volatile uint32_t ui32TempAvg;
        volatile uint32_t ui32TempValueC;
        volatile uint32_t ui32TempValueF;
    
        SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
        InitConsole();
    
        //
        // Display the setup on the console.
        //
        UARTprintf("ADC ->\n");
        UARTprintf("  Type: Internal Temperature Sensor\n");
        UARTprintf("  Samples: One\n");
        UARTprintf("  Update Rate: 250ms\n");
        UARTprintf("  Input Pin: Internal temperature sensor\n\n");
        //5分频,使用PLL,外部晶振16M,system时钟源选择 main osc。系统时钟40MHZ
        SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
        //使能ADC0
        ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_PROCESSOR, 0);
        //We want to use ADC0, sample sequencer 1,
        //we want the processor to trigger the sequence and we want to use the highest priority
        ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_TS);
        ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_TS);
        ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_TS);
        //Configure steps 0 - 2 on sequencer 1 to sample the temperature sensor (ADC_CTL_TS).
        ADCSequenceStepConfigure(ADC0_BASE,1,3,ADC_CTL_TS|ADC_CTL_IE|ADC_CTL_END);
        //Sample the temperature sensor (ADC_CTL_TS) and configure the interrupt flag (ADC_CTL_IE)
        //Tell the ADC logic that this is the last conversion on sequencer1 (ADC_CTL_END).
        ADCSequenceEnable(ADC0_BASE, 1);
        //enable ADC sequencer 1
        while(1)
        {
           ADCIntClear(ADC0_BASE, 1);
           ADCProcessorTrigger(ADC0_BASE, 1);
           //trigger the ADC conversion with software
           while(!ADCIntStatus(ADC0_BASE, 1, false))
           {
           }
           //wait for the conversion to complete
           ADCSequenceDataGet(ADC0_BASE, 1, ui32ADC0Value);
           ui32TempAvg = (ui32ADC0Value[0] + ui32ADC0Value[1] + ui32ADC0Value[2] + ui32ADC0Value[3] + 2)/4;
           //Since 2/4 = 1/2 = 0.5, 1.5 will be rounded to 2.0 with
           //the addition of 0.5. In the case of 1.0, when 0.5 is added to yield 1.5, this will be rounded
           //back down to 1.0 due to the rules of integer math.即四舍五入
           ui32TempValueC = (1475 - ((2475 * ui32TempAvg)) / 4096)/10;
           //TEMP = 147.5 – ((75 * (VREFP – VREFN) * ADCVALUE) / 4096)
           //VREFP – VREFN=3.3V
           ui32TempValueF = ((ui32TempValueC * 9) + 160) / 5;
           UARTprintf("Temperature = %d*C or %d*F\r\n", ui32TempValueC,
                      ui32TempValueF);
           //F = ( C * 9)/5 +32
        }
    }
    

    直接用的第三方的库,没用你的例程,但是肯定是可以的,继续检查细节吧。

  • 你硬件配置的时候接了跳帽或者连线吗,我检查了好久感觉代码没什么问题

  • 直接把PB0/PB1/GND三者连接到usb转ttl的三个脚上面,打开串口调试工具就接收到数据了。