This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我采用的是tm4c1294ncpdt芯片,想用ti-rtos中的timer模块来定时1s实现led的闪烁,period我设置的是1000000,单位是微妙,但是结果虽然LED闪烁,但我调用timer_getperiod得到的是120000000,下面是我的源码和结果,请帮忙分析一下。
#include <xdc/std.h> #include <xdc/runtime/System.h> //#include <ti/sysbios/family/arm/m3/Hwi.h> /* BIOS Header files */ #include <ti/sysbios/BIOS.h> #include <ti/sysbios/knl/Task.h> #include <ti/sysbios/hal/Timer.h> #include <xdc/runtime/Error.h> /* TI-RTOS Header files */ #include <ti/drivers/GPIO.h> /* Example/Board Header files */ #include "Board.h" UInt FLAG=0; Timer_Params timerParams; Timer_Handle timer0; Void myIsr(UArg arg0) { FLAG=!FLAG; if(FLAG==0) {GPIO_write(Board_LED0, Board_LED_ON);} else {GPIO_write(Board_LED0, Board_LED_OFF);} System_printf("Current period = %d\n", Timer_getPeriod(timer0)); System_printf("%d\n",FLAG); System_flush(); } int main(void) { Board_initGeneral(); Board_initGPIO(); Error_Block eb; Error_init(&eb); Timer_Params_init(&timerParams); timerParams.period = 1000000; timerParams.periodType = Timer_PeriodType_MICROSECS; timerParams.arg = 1; timer0 = Timer_create(Timer_ANY, myIsr, &timerParams, &eb); if (timer0 == NULL) { System_abort("Timer create failed"); } System_flush(); /* Start BIOS */ BIOS_start(); return (0); }
下面是运行结果