This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在AM335x 芯片中,用GPIO来实现一个时序的通信的过程。



我在AM335x中使用 gpio1_12,gpio1_13 分别作为数据写输出的 片选 ,和数据输出引脚,用gpio1_14,gpio1_15 作为数据的读使能,数据输入的引脚,

我用示波器已经测试了 gpio1_12 和 gpio1_13 的 输出信号是有的,信号到 输入引脚 gpio1_14和gpio1_15时还是有,但是 gpio1_14 和gpio1_15 这两个引脚读取不到信号的状态。如果有人遇到类似的问题,可不可以告知你的方法,或者给我提供一些更好的方案。谢谢各位,下面就是我要发送的数据信号,1的持续时间5ms 0的持续时间也是5ms