This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何通过串口下载程序到TM4C1230d5pm中



1、目前我所知道的是,先用LM Flash Program下载boot_serial到0x00处,接着下载boot_demo1到0x2800处,然后我就可以通过串口下载更新程序了吗?

2、而每次下载更新程序的时候,是不是都要先下载boot_demo1(这样才能进入bootloader中),然后才能下载自己的应用程序?

3、keil5可以通过ULINK2下载boot_serial到芯片中吗?如果可以我该怎么做?

  • 1.对的。下载完boot_serial后,你就可以用串口连接上板子,就可以进行下载了。

    2.不需要重新下载boot_demo1的,只要0x00-0x2800这部分的空间不擦除,就可以的。

    3.理论上是可以的。但是没试过,可是看看STM32类似的教程设置,分散加载代码。