This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于双向DC--DC电路给18650锂电池充电的问题

我们在做一个如下的题目:

题目中的第二点遇到了困难,具体情况是:当U2设置为24V,占空比为84.3%时,空载电压正常,此时五节18650电池串联的电压总共为18.5V,在正常充电范围内,接上五节电池后,输出电压U1被拉低到19.1V,而且输出电流I1很小,只有0.28A,通过提升占空比,最多可以到达1A,但远远不能满足题目的要求。怎样解决这一问题呢,希望各位工程师们指点。下面是双向DC-DC电路原理图

请各位看看是双向DC-DC电路的问题,还是其他问题导致电压被拉低,输出电流过小。这个问题很急啊,有人知道吗