Other Parts Discussed in Thread: MSP430F4793
请问有没有MSP430F4793 内部温度传感器的 使用例程,十分感谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F4793
请问有没有MSP430F4793 内部温度传感器的 使用例程,十分感谢!!
#include <msp430.h>
unsigned int ADCresult;
unsigned long DegC = 0;
unsigned long DegF = 0;
int main(void)
{
volatile unsigned int i; // Use volatile to prevent removal
// by compiler optimization
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
FLL_CTL0 |= XCAP11PF; // Configure load caps
for (i = 0; i < 10000; i++); // Delay for 32 kHz crystal to
// stabilize
SD16CTL = SD16REFON+SD16SSEL0; // 1.2V ref, SMCLK
SD16CCTL2 |= SD16SNGL+SD16IE ; // Single conv, enable interrupt
SD16INCTL2 |= SD16INCH_6; // Select Channel A6
for (i = 0; i < 0x3600; i++); // Delay for 1.2V ref startup
while (1)
{
SD16CCTL2 |= SD16SC; // Set bit to start conversion
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts
DegC = ((unsigned long)ADCresult * 909)/65536 - 727;
// Calculate degrees Celcius
DegF = ((unsigned long)ADCresult * 1636)/65536 - 1276;
// Calculate degrees Farenheit
__no_operation(); //SET BREAKPOINT HERE
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=SD16A_VECTOR
__interrupt void SD16AISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(SD16A_VECTOR))) SD16AISR (void)
#else
#error Compiler not supported!
#endif
{
switch (SD16IV)
{
case 2: // SD16MEM Overflow
break;
case 4: // SD16MEM0 IFG
break;
case 6: // SD16MEM1 IFG
break;
case 8: // SD16MEM2 IFG
ADCresult = SD16MEM2; // Save CH2 results (clears IFG)
break;
}
__bic_SR_register_on_exit(LPM0_bits); // Exit LPM0
}