Other Parts Discussed in Thread: TM4C123GH6PM
板子是TM4C123GH6PM,总是会遇到莫名其妙进入FaultISR的问题,且不知道怎么解决,今天又遇上了。代码贴在下面,用了很多延时也没用。请问大家有什么解决办法嘛?
/*
* main.c
*/
#include "mytype.h"
#include "stdbool.h"
#include "stdint.h"
#include "inc/hw_types.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/gpio.h"
#include "driverlib/adc.h"
#include "driverlib/pin_map.h"
#include "inc/hw_memmap.h"
#include "driverlib/interrupt.h"
#include "driverlib/timer.h"
#include "driverlib/fpu.h"
#include "inc/hw_ints.h"
#include "mytype.h"
#include "stdio.h"
long sysclock = 0;
uint32_t buffer;
byte refresh_lcd_flag;
#define DELAY SysCtlDelay(30)
#define TIMER_FREQUENCY 100
#define SYSTICK_FREQUENCY 1
void initSystem();
void LCDDisplay(char * notation,double num,unsigned char x,unsigned char y);
int main(void) {
FPUEnable();
FPULazyStackingEnable();
initSystem();
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);
DELAY;
while(1){
if(refresh_lcd_flag){
refresh_lcd_flag = 0;
// LCDDisplay("num1",buffer,0,0);
}
}
}
void initSystem(){
sysclock = SysCtlClockGet();
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
DELAY;
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
DELAY;
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
DELAY;
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
DELAY;
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE,GPIO_INT_PIN_0);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE,GPIO_INT_PIN_1);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE,GPIO_INT_PIN_5);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_INT_PIN_2);
GPIOPinTypeADC(GPIO_PORTB_BASE,GPIO_PIN_4);
ADCSequenceConfigure(ADC0_BASE,0,ADC_TRIGGER_PROCESSOR,0);
ADCSequenceStepConfigure(ADC0_BASE,0,0,ADC_CTL_CH0 | ADC_CTL_END | ADC_CTL_IE);
ADCSequenceEnable(ADC0_BASE, 0);
ADCIntClear(ADC0_BASE, 0);
ADCIntEnable(ADC0_BASE,0);
IntEnable(INT_ADC0SS0);
DELAY;
i2cInit();
i2cCls();
DELAY;
SysTickEnable();
SysTickPeriodSet(SysCtlClockGet() / SYSTICK_FREQUENCY);
SysTickIntEnable();
IntMasterEnable();
}
void adcSeq0IntHandler(void){
ADCIntClear(ADC0_BASE,0);
TimerIntClear(TIMER0_BASE,TIMER_TIMA_TIMEOUT);
while(!ADCIntStatus(ADC0_BASE, 0, false));//等待采集结束
ADCSequenceDataGet(ADC0_BASE,0,&buffer);
}
void LCDDisplay(char * notation,double num,unsigned char x,unsigned char y){
char buf[50];
if(num>0){
sprintf(
buf,
"%s: %d.%02d",
notation,
(int)num,
(int)((num-(int)num)*100)
);
// i2cP6x8Str(x,y,buf);
}else{
sprintf(
buf,
"%s: -%d.%02d",
notation,
(int)-num,
(int)-((num-(int)num)*100)
);
// i2cP6x8Str(x,y,buf);
}
}
void sysTickIntHandler(void){
refresh_lcd_flag = 1;
}