This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129为什么同一个定时器的CCP0和CCP1不能同时使用?

SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER3);//PM2
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
GPIOPinConfigure(GPIO_PM2_T3CCP0);
GPIOPinTypeTimer(GPIO_PORTM_BASE, GPIO_PIN_2);
GPIOPadConfigSet(GPIO_PORTM_BASE, GPIO_PIN_2, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU); // 为管脚配置弱上拉模式
TimerConfigure(TIMER3_BASE, TIMER_CFG_SPLIT_PAIR | TIMER_CFG_A_CAP_COUNT_UP);//边沿加计数模式
TimerControlEvent(TIMER3_BASE, TIMER_A, TIMER_EVENT_NEG_EDGE);
TimerMatchSet(TIMER3_BASE, TIMER_A, 0x1FFF);
TimerEnable(TIMER3_BASE, TIMER_A);
/****************************************************/
GPIOPinConfigure(GPIO_PM3_T3CCP1); //PM3
GPIOPinTypeTimer(GPIO_PORTM_BASE, GPIO_PIN_3);
GPIOPadConfigSet(GPIO_PORTM_BASE, GPIO_PIN_3, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU); // 为管脚配置弱上拉模式
TimerConfigure(TIMER3_BASE, TIMER_CFG_SPLIT_PAIR | TIMER_CFG_B_CAP_COUNT_UP);//边沿加计数模式
TimerControlEvent(TIMER3_BASE, TIMER_B, TIMER_EVENT_NEG_EDGE);
TimerMatchSet(TIMER3_BASE, TIMER_B, 0x1FFF);
TimerEnable(TIMER3_BASE, TIMER_B);
/****************************************************/

这样初始化只能用CCP1,也就是PM3,此时TimerValueGet(TIMER3_BASE, TIMER_A);的值都是0xFFFF。

如果把PM3那段不要初始化CCP0就正常了。

是不是TIMER  的A B模块不能同时使用?