This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
自己写了一下SHT30温湿度传感器的读取值函数,但是读不上来数呀。大侠,帮忙看看哪的问题。代码如下,先谢谢了
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/rom.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/gpio.h"
#include "driverlib/i2c.h"
#include "sht30_init.h"
#define i2cAddWrite 0x88
#define i2cAddRead 0x89
#define CMD_MEAS_PERI_4_HI 0x2334
#define CMD_FETCH_COMM 0xE000
typedef struct { uint8_t dostate;
uint8_t count;
uint8_t putData[6]; }i2c_parameter i2c0;
void sht30_init(void)
{
uint8_t i;
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
// SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3 );
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
I2CMasterEnable(I2C0_BASE);
for(i=0;i<50;i++)
{ SysCtlDelay(SysCtlClockGet()/3000);
}
}
int read_Periodidata(void)
{
uint8_t j,rop;
//写连续读指令0x2334
I2CMasterSlaveAddrSet(I2C0_BASE, i2cAddWrite, false);
I2CMasterDataPut(I2C0_BASE, 0x23);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusBusy(I2C0_BASE));
I2CMasterDataPut(I2C0_BASE, 0x34);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
while(I2CMasterBusBusy(I2C0_BASE));
//开始读取温湿度
I2CMasterSlaveAddrSet(I2C0_BASE, i2cAddWrite, false);
I2CMasterDataPut(I2C0_BASE, 0xe0);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusBusy(I2C0_BASE));
I2CMasterDataPut(I2C0_BASE, 0x00);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
while(I2CMasterBusBusy(I2C0_BASE));
I2CMasterSlaveAddrSet(I2C0_BASE, i2cAddRead, true);
I2CMasterControl(I2C0_BASE,I2C_MASTER_CMD_BURST_RECEIVE_START);
for(j = 0; j < 5; j++)
{
while(I2CMasterBusBusy(I2C0_BASE));
i2c0.putData[j] = I2CMasterDataGet(I2C0_BASE);
if(j==(5-1))
I2CMasterControl(I2C0_BASE,I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
else
I2CMasterControl(I2C0_BASE,I2C_MASTER_CMD_BURST_RECEIVE_CONT);
}
while(I2CMasterBusBusy(I2C0_BASE));
rop = I2CMasterErr(I2C0_BASE);
return rop;
}
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);端口B在主函数开始已经使能。上传一下SHT30数据手册,现在没有思路了
I2CMasterSlaveAddrSet(I2C0_BASE, i2cAddWrite, false);
I2CMasterDataPut(I2C0_BASE, i2cAddWrite);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusBusy(I2C0_BASE));到while这就一直等待了,不知道为啥