I encountered the following problems when I output M432P401R P4.2. I can't make LFXTCLK_ON 1. I refer to the example of MSP432P401R for the output of 48MHz, but it is still unable to output the external crystal vibration of P4.2.I need your help. I look forward to your reply.thank you