你好,
我现在使用的是cc2650芯片,往开发板里烧入了程序后,上电池后不能自动运行,是否是外部晶振出问题了?
请问下怎么样只是用内部晶振?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
内部的32.768K时钟是可以作为时钟源,提供给其他模块使用;并且这个32.768K的时钟还可以作为CPU唤醒使用。
有一片详细的文档解释和介绍如何使用,希望对你有帮助。
http://www.ti.com/lit/an/swra499b/swra499b.pdf
This application report explains how you can configure the SimpleLink™ Bluetooth low energy CC2640 wireless MCU and multi-standard CC2650 wireless MCU to run the Bluetooth low energy (BLE) software stack without the need for a 32 kHz crystal. This application report explains how to configure this mode of operation, what considerations have to be taken to use the internal RC low frequency oscillator (RCOSC_LF) for the Bluetooth low energy peripheral and broadcast (beacon) role devices instead of the 32 kHz crystal, and what impact it has on current consumption. This document assumes the reader is familiar with the concepts described in CC2640 and CC2650 SimpleLink™ Bluetooth® low energy Software Stack Developer's Guide and the CC13xx, CC26xx SimpleLink™ Wireless MCU Technical Reference Manual. Removing the 32 kHz crystal from a design lowers the bill of material (BOM) cost, reduces the required board space and simplifies procurement.