This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129NCPDT 在Bootloader中UART3串口不能中断

TI M4 UART3串口RX中断 同样的配置在application中是可以进入中断的,但是在bootloader里,进不了中断。 中断入口函数也配置了,是否还有其他地方需要设置?我发现默认启动文件.S文件里面的中断向量表里面没有uart3入口,所以自己添加了,但是offset地址>0x110时,bootloader就运行不了。但是uart3的offset地址是0x12C。是不是bootloader中大小限制呢?

  • 启动文件中有uart3的中断入口地址了呀。

    //*****************************************************************************
    //
    // startup_ccs.c - Startup code for use with TI's Code Composer Studio.
    //
    // Copyright (c) 2013-2017 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    // 
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    // 
    // This is part of revision 2.1.4.178 of the DK-TM4C129X Firmware Package.
    //
    //*****************************************************************************
    
    #include <stdint.h>
    #include "inc/hw_nvic.h"
    #include "inc/hw_types.h"
    
    //*****************************************************************************
    //
    // Forward declaration of the default fault handlers.
    //
    //*****************************************************************************
    void ResetISR(void);
    static void NmiSR(void);
    static void FaultISR(void);
    static void IntDefaultHandler(void);
    
    //*****************************************************************************
    //
    // External declaration for the reset handler that is to be called when the
    // processor is started
    //
    //*****************************************************************************
    extern void _c_int00(void);
    
    //*****************************************************************************
    //
    // Linker variable that marks the top of the stack.
    //
    //*****************************************************************************
    extern uint32_t __STACK_TOP;
    
    //*****************************************************************************
    //
    // External declarations for the interrupt handlers used by the application.
    //
    //*****************************************************************************
    extern void lwIPEthernetIntHandler(void);
    extern void SysTickHandler(void);
    
    //*****************************************************************************
    //
    // The vector table.  Note that the proper constructs must be placed on this to
    // ensure that it ends up at physical address 0x0000.0000 or at the start of
    // the program if located at a start address other than 0.
    //
    //*****************************************************************************
    #pragma DATA_SECTION(g_pfnVectors, ".intvecs")
    void (* const g_pfnVectors[])(void) =
    {
        (void (*)(void))((uint32_t)&__STACK_TOP),
                                                // The initial stack pointer
        ResetISR,                               // The reset handler
        NmiSR,                                  // The NMI handler
        FaultISR,                               // The hard fault handler
        IntDefaultHandler,                      // The MPU fault handler
        IntDefaultHandler,                      // The bus fault handler
        IntDefaultHandler,                      // The usage fault handler
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // SVCall handler
        IntDefaultHandler,                      // Debug monitor handler
        0,                                      // Reserved
        IntDefaultHandler,                      // The PendSV handler
        SysTickHandler,                         // The SysTick handler
        IntDefaultHandler,                      // GPIO Port A
        IntDefaultHandler,                      // GPIO Port B
        IntDefaultHandler,                      // GPIO Port C
        IntDefaultHandler,                      // GPIO Port D
        IntDefaultHandler,                      // GPIO Port E
        IntDefaultHandler,                      // UART0 Rx and Tx
        IntDefaultHandler,                      // UART1 Rx and Tx
        IntDefaultHandler,                      // SSI0 Rx and Tx
        IntDefaultHandler,                      // I2C0 Master and Slave
        IntDefaultHandler,                      // PWM Fault
        IntDefaultHandler,                      // PWM Generator 0
        IntDefaultHandler,                      // PWM Generator 1
        IntDefaultHandler,                      // PWM Generator 2
        IntDefaultHandler,                      // Quadrature Encoder 0
        IntDefaultHandler,                      // ADC Sequence 0
        IntDefaultHandler,                      // ADC Sequence 1
        IntDefaultHandler,                      // ADC Sequence 2
        IntDefaultHandler,                      // ADC Sequence 3
        IntDefaultHandler,                      // Watchdog timer
        IntDefaultHandler,                      // Timer 0 subtimer A
        IntDefaultHandler,                      // Timer 0 subtimer B
        IntDefaultHandler,                      // Timer 1 subtimer A
        IntDefaultHandler,                      // Timer 1 subtimer B
        IntDefaultHandler,                      // Timer 2 subtimer A
        IntDefaultHandler,                      // Timer 2 subtimer B
        IntDefaultHandler,                      // Analog Comparator 0
        IntDefaultHandler,                      // Analog Comparator 1
        IntDefaultHandler,                      // Analog Comparator 2
        IntDefaultHandler,                      // System Control (PLL, OSC, BO)
        IntDefaultHandler,                      // FLASH Control
        IntDefaultHandler,                      // GPIO Port F
        IntDefaultHandler,                      // GPIO Port G
        IntDefaultHandler,                      // GPIO Port H
        IntDefaultHandler,                      // UART2 Rx and Tx
        IntDefaultHandler,                      // SSI1 Rx and Tx
        IntDefaultHandler,                      // Timer 3 subtimer A
        IntDefaultHandler,                      // Timer 3 subtimer B
        IntDefaultHandler,                      // I2C1 Master and Slave
        IntDefaultHandler,                      // CAN0
        IntDefaultHandler,                      // CAN1
        lwIPEthernetIntHandler,                 // Ethernet
        IntDefaultHandler,                      // Hibernate
        IntDefaultHandler,                      // USB0
        IntDefaultHandler,                      // PWM Generator 3
        IntDefaultHandler,                      // uDMA Software Transfer
        IntDefaultHandler,                      // uDMA Error
        IntDefaultHandler,                      // ADC1 Sequence 0
        IntDefaultHandler,                      // ADC1 Sequence 1
        IntDefaultHandler,                      // ADC1 Sequence 2
        IntDefaultHandler,                      // ADC1 Sequence 3
        IntDefaultHandler,                      // External Bus Interface 0
        IntDefaultHandler,                      // GPIO Port J
        IntDefaultHandler,                      // GPIO Port K
        IntDefaultHandler,                      // GPIO Port L
        IntDefaultHandler,                      // SSI2 Rx and Tx
        IntDefaultHandler,                      // SSI3 Rx and Tx
        IntDefaultHandler,                      // UART3 Rx and Tx
        IntDefaultHandler,                      // UART4 Rx and Tx
        IntDefaultHandler,                      // UART5 Rx and Tx
        IntDefaultHandler,                      // UART6 Rx and Tx
        IntDefaultHandler,                      // UART7 Rx and Tx
        IntDefaultHandler,                      // I2C2 Master and Slave
        IntDefaultHandler,                      // I2C3 Master and Slave
        IntDefaultHandler,                      // Timer 4 subtimer A
        IntDefaultHandler,                      // Timer 4 subtimer B
        IntDefaultHandler,                      // Timer 5 subtimer A
        IntDefaultHandler,                      // Timer 5 subtimer B
        IntDefaultHandler,                      // FPU
        0,                                      // Reserved
        0,                                      // Reserved
        IntDefaultHandler,                      // I2C4 Master and Slave
        IntDefaultHandler,                      // I2C5 Master and Slave
        IntDefaultHandler,                      // GPIO Port M
        IntDefaultHandler,                      // GPIO Port N
        0,                                      // Reserved
        IntDefaultHandler,                      // Tamper
        IntDefaultHandler,                      // GPIO Port P (Summary or P0)
        IntDefaultHandler,                      // GPIO Port P1
        IntDefaultHandler,                      // GPIO Port P2
        IntDefaultHandler,                      // GPIO Port P3
        IntDefaultHandler,                      // GPIO Port P4
        IntDefaultHandler,                      // GPIO Port P5
        IntDefaultHandler,                      // GPIO Port P6
        IntDefaultHandler,                      // GPIO Port P7
        IntDefaultHandler,                      // GPIO Port Q (Summary or Q0)
        IntDefaultHandler,                      // GPIO Port Q1
        IntDefaultHandler,                      // GPIO Port Q2
        IntDefaultHandler,                      // GPIO Port Q3
        IntDefaultHandler,                      // GPIO Port Q4
        IntDefaultHandler,                      // GPIO Port Q5
        IntDefaultHandler,                      // GPIO Port Q6
        IntDefaultHandler,                      // GPIO Port Q7
        IntDefaultHandler,                      // GPIO Port R
        IntDefaultHandler,                      // GPIO Port S
        IntDefaultHandler,                      // SHA/MD5 0
        IntDefaultHandler,                      // AES 0
        IntDefaultHandler,                      // DES3DES 0
        IntDefaultHandler,                      // LCD Controller 0
        IntDefaultHandler,                      // Timer 6 subtimer A
        IntDefaultHandler,                      // Timer 6 subtimer B
        IntDefaultHandler,                      // Timer 7 subtimer A
        IntDefaultHandler,                      // Timer 7 subtimer B
        IntDefaultHandler,                      // I2C6 Master and Slave
        IntDefaultHandler,                      // I2C7 Master and Slave
        IntDefaultHandler,                      // HIM Scan Matrix Keyboard 0
        IntDefaultHandler,                      // One Wire 0
        IntDefaultHandler,                      // HIM PS/2 0
        IntDefaultHandler,                      // HIM LED Sequencer 0
        IntDefaultHandler,                      // HIM Consumer IR 0
        IntDefaultHandler,                      // I2C8 Master and Slave
        IntDefaultHandler,                      // I2C9 Master and Slave
        IntDefaultHandler                       // GPIO Port T
    };
    
    //*****************************************************************************
    //
    // This is the code that gets called when the processor first starts execution
    // following a reset event.  Only the absolutely necessary set is performed,
    // after which the application supplied entry() routine is called.  Any fancy
    // actions (such as making decisions based on the reset cause register, and
    // resetting the bits in that register) are left solely in the hands of the
    // application.
    //
    //*****************************************************************************
    void
    ResetISR(void)
    {
        //
        // Jump to the CCS C initialization routine.  This will enable the
        // floating-point unit as well, so that does not need to be done here.
        //
        __asm("    .global _c_int00\n"
              "    b.w     _c_int00");
    }
    
    //*****************************************************************************
    //
    // This is the code that gets called when the processor receives a NMI.  This
    // simply enters an infinite loop, preserving the system state for examination
    // by a debugger.
    //
    //*****************************************************************************
    static void
    NmiSR(void)
    {
        //
        // Enter an infinite loop.
        //
        while(1)
        {
        }
    }
    
    //*****************************************************************************
    //
    // This is the code that gets called when the processor receives a fault
    // interrupt.  This simply enters an infinite loop, preserving the system state
    // for examination by a debugger.
    //
    //*****************************************************************************
    static void
    FaultISR(void)
    {
        //
        // Enter an infinite loop.
        //
        while(1)
        {
        }
    }
    
    //*****************************************************************************
    //
    // This is the code that gets called when the processor receives an unexpected
    // interrupt.  This simply enters an infinite loop, preserving the system state
    // for examination by a debugger.
    //
    //*****************************************************************************
    static void
    IntDefaultHandler(void)
    {
        //
        // Go into an infinite loop.
        //
        while(1)
        {
        }
    }
    


  • 你好,苦行僧

          在不带bootloader的例程中有串口3的中断入口;但是在bootloader例程中没有串口3的中断入口。我自己在后面补充了中断入口,但是不能工作。

     

     

  • 你补充的是哪个启动文件呢?如果想用串口3的话,用自带的bootloader函数好像是不支持的,测试的是哪个例程呢?