This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28069同时采样问题

我采样的是一个模拟信号的A+和A-,(A+) 减去(A-)后的结果是实际模拟量的值,我采用同时采样模式。我希望初始化时用软件启动一次转换,之后通过ADCINT1触发连续执行ADC,可是程序只进一次ADC中断,后面就再也不进了,麻烦帮我看看问题在哪里。谢谢

初始化部分:

EALLOW;
AdcRegs.ADCCTL2.bit.ADCNONOVERLAP = 1; // Enable non-overlap mode
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; // INT pulse generation, 0=start of conversion, 1=end of conversion
AdcRegs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; // Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 1; //setup EOC1 to trigger ADCINT1 to fire
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN0 = 1;
AdcRegs.ADCSOC0CTL.bit.CHSEL = 0; //set SOC0 channel select to ADCINA0 and ADCINB0
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 0; //set SOC0 start trigger on software
AdcRegs.ADCSOC0CTL.bit.ACQPS = 6;   //set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)

AdcRegs.ADCINTSOCSEL1.bit.SOC0 = 1; //ADCINT1 will trigger SOC0

AdcRegs.ADCSOCFRC1.bit.SOC0 = 1;
EDIS;

中断部分:

interrupt void adc_isr(void)
{
Voltage1[ConversionCount] = AdcResult.ADCRESULT0;
Voltage2[ConversionCount] = AdcResult.ADCRESULT1;

// If 20 conversions have been logged, start over
if(ConversionCount == 1)
{
ConversionCount = 0;
//GpioDataRegs.GPATOGGLE.bit.GPIO7 = 1;
}
else ConversionCount++;
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Clear ADCINT1 flag reinitialize for next SOC

PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE

return;
}

以上代码运行时,只进一次中断,但当我把AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 2; 时,每次都可进ADC中断,我不明白这是什么原因?本来想AdcRegs.ADCSOC0CTL.bit.TRIGSEL设置为ADCINT1触发,因为我认为要和AdcRegs.ADCINTSOCSEL1.bit.SOC0 = 1; //ADCINT1 will trigger SOC0保持一致,可是设置里面没有ADCINT1触发这一项,所以我就试着选了TINT1n触发,没想到这样就可以进中断了。请问这是什么原因? 谢谢!

另外,AdcRegs.INTSEL1N2.bit.INT1SEL = 1; INT1SEL 这个位设置为0或者1,程序都能正常进中断,这是为什么?我个人理解设置为1才会产生ADCINT1中断,可是我设置为0照样可以进中断。请解释,谢谢啊!