请问各位大神,我在rebuild Simple_Peer_To_Peer工程时,出现链接错误,芯片使用cc1110
Error[e16]: Segment PDATA_Z (size: 0 align: 0) is too long for segment definition. At least 0 more bytes needed. The problem occurred while processing the
segment placement command "-Z(XDATA)PDATA_Z,PDATA_I=_PDATA0_START-_PDATA0_END", where at the moment of placement the available memory
ranges were "-none-"
Reserved ranges relevant to this placement:
XDATA:f000-f3fe XSTACK
BIT:0-7 BREG
BIT:80-87 SFR_AN
BIT:90-97 SFR_AN
BIT:a8-af SFR_AN
BIT:d8-df SFR_AN
Error while running Linker