This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430afe253如何配置时钟系统

新手,在使afe253不知道怎配置时钟系统,外部不加晶振,如何配置主系统时钟,子系统时钟?求大神讲解讲解

  •  ACLK = n/a, MCLK = SMCLK = default DCO

    如果你不配置,默认就是DCO

  • http://www.ti.com.cn/cn/lit/ug/slau144j/slau144j.pdf

    其实所有的配置都在这个手册上,可以通过提供的系统组织图看出来怎么个配置方式。

    另外你找到这个芯片主页后,下面可以找到例子程序包。

    程序表如下,基本上都是采用内部振荡器

    File Name                      Description
    ----------------------------------------------------------------------------------------
    msp430afe_clks.c               Basic Clock, Output Buffered SMCLK, ACLK and MCLK/10
    msp430afe_flashwrite_01.c      Flash In-System Programming, Copy SegC to SegD
    msp430afe_lpm3_vlo.c           Basic Clock, LPM3 Using WDT ISR, VLO ACLK
    msp430afe_nmi.c                Basic Clock, Configure RST/NMI as NMI
    msp430afe_P1_01.c              Software Poll P1.4, Set P1.0 if P1.4 = 1
    msp430afe_P1_02.c              Software Port Interrupt Service on P1.4 from LPM4
    msp430afe_sd24_01.c            SD24, Continuous Conversion on a Group of 3 Channels
    msp430afe_sd24_02.c            SD24, Single Conversion on a Group of 3 Channels
    msp430afe_sd24_03.c            SD24, Continuous Conversion on a Single Channel
    msp430afe_sd24_04.c            SD24, Single Conversion on Single Channel Polling IFG
    msp430afe_sd24_05.c            SD24, Single Conversion on a Single Channel Using ISR
    msp430afe_sd24_06.c            SD24, Using the Integrated Temperature Sensor
    msp430afe_sd24_10.c            SD24, Continuous Conversion on a Group of Channels
    msp430afe_sd24_11.c            SD24, Single Conversion on a Group of Channels
    msp430afe_svs_01.c             SVS, POR @ 2.5V Vcc
    msp430afe_svs_03.c             SVM, Toggle port 5.1 on Vcc < 2.8V
    msp430afe_ta_01.c              Timer_A, Toggle P1.0, CCR0 Cont. Mode ISR, DCO SMCLK
    msp430afe_ta_02.c              Timer_A, Toggle P1.0, CCR0 Up Mode ISR, DCO SMCLK
    msp430afe_ta_03.c              Timer_A, Toggle P1.0, Overflow ISR, DCO SMCLK
    msp430afe_ta_04.c              Timer_A, Toggle P1.0, Overflow ISR, VLO ACLK
    msp430afe_ta_06.c              Timer_A, Toggle P1.0, CCR1 Cont. Mode ISR, DCO SMCLK
    msp430afe_ta_07.c              Timer_A, Toggle P1.0-2, Cont. Mode ISR, DCO SMCLK
    msp430afe_ta_13.c              Timer_A, Toggle P1.1/TA0, Up/Down Mode, DCO SMCLK
    msp430afe_ta_14.c              Timer_A, Toggle P1.1/TA0, Up/Down Mode, VLO ACLK
    msp430afe_ta_19.c              Timer_A, PWM TA1, Up/Down Mode, DCO SMCLK
    msp430afe_uart_115k.c          USART0, 115200 UART Echo ISR, DCO SMCLK
    msp430afe_vlo.c                Software Toggle P1.0, MCLK = VLO/8
    msp430afe_wdt_01.c             WDT, Toggle P1.0, Interval Overflow ISR, DCO SMCLK
    msp430afe_wdt_04.c             WDT+ Failsafe Clock, DCO SMCLK
    msp430afe_wdt_05.c             Reset on Invalid Address fetch, Toggle P1.0