This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMA串口发送数据不成功



想用DMA把内存中数据通过串口发送出去,一直不成功
void uDMAInit()
{
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);//ʹÄÜʱÖÓ
ROM_uDMAEnable();//ʹÄÜÍâÉè
ROM_uDMAControlBaseSet(pui8ControlTable);

ROM_IntEnable(INT_UDMA);

ROM_UARTFIFOLevelSet(UART0_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);

//
// Put the attributes in a known state for the uDMA UART1TX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART0TX,
UDMA_ATTR_ALTSELECT |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);

//
// Set the USEBURST attribute for the uDMA UART TX channel. This will
// force the controller to always use a burst when transferring data from
// the TX buffer to the UART. This is somewhat more effecient bus usage
// than the default which allows single or burst transfers.
//
ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_UART0TX, UDMA_ATTR_USEBURST);

//
// Configure the control parameters for the UART TX. The uDMA UART TX
// channel is used to transfer a block of data from a buffer to the UART.
// The data size is 8 bits. The source address increment is 8-bit bytes
// since the data is coming from a buffer. The destination increment is
// none since the data is to be written to the UART data register. The
// arbitration size is set to 4, which matches the UART TX FIFO trigger
// threshold.
//
ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 |
UDMA_DST_INC_NONE |
UDMA_ARB_4);

//
// Set up the transfer parameters for the uDMA UART TX channel. This will
// configure the transfer source and destination and the transfer size.
// Basic mode is used because the peripheral is making the uDMA transfer
// request. The source is the TX buffer and the destination is the UART
// data register.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ui8TxBuf,
(void *)(UART0_BASE + UART_O_DR),
sizeof(g_ui8TxBuf));


//
// Now both the uDMA UART TX and RX channels are primed to start a
// transfer. As soon as the channels are enabled, the peripheral will
// issue a transfer request and the data transfers will begin.
//
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART0TX);

//
// Enable the UART DMA TX/RX interrupts.
//
ROM_UARTIntEnable(UART0_BASE, UART_INT_DMATX );


ROM_IntEnable(INT_UART0);
}

void usart_init_all(void)
{

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);//+
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);//??UART0

GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);

GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);//??UART????PA0 PA1

UARTConfigSetExpClk(UART0_BASE, SysClock, 115200,(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));

UARTFIFOEnable(UART0_BASE);//»¹²»È·¶¨FIFOÓëDMAÊÇ·ñÓгåÍ»

UARTDMAEnable(UART0_BASE,UART_DMA_TX);//ÊÇÄÚ´æµ½´®¿Ú£¬´®¿ÚÔÙ·¢³öÈ¥£¬DMA´«Êäµ½RX»¹ÊÇTX
ROM_UARTIntEnable(UART0_BASE,UART_INT_DMATX);
IntEnable(INT_UART0); //enable the UART interrupt


//UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT); //only enable RX and TX interrupts
}

void UART0IntHandler()
{
uint32_t ui32Status,ui32Mode;

ui32Status = UARTIntStatus(UART0_BASE,true);
UARTIntClear(UART0_BASE,ui32Status);

if(!ROM_uDMAChannelIsEnabled(UDMA_CHANNEL_UART0TX))
{
//
// Start another DMA transfer to UART1 TX.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ui8TxBuf,
(void *)(UART0_BASE + UART_O_DR),
sizeof(g_ui8TxBuf));

//
// The uDMA TX channel must be re-enabled.
//
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART0TX);
}



}

  • //*****************************************************************************
    //
    // udma_demo.c - uDMA example.
    //
    // Copyright (c) 2011-2017 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    // 
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    // 
    // This is part of revision 2.1.4.178 of the DK-TM4C123G Firmware Package.
    //
    //*****************************************************************************
    
    #include <stdint.h>
    #include <stdbool.h>
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "inc/hw_uart.h"
    #include "driverlib/fpu.h"
    #include "driverlib/gpio.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/systick.h"
    #include "driverlib/uart.h"
    #include "driverlib/udma.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/rom.h"
    #include "grlib/grlib.h"
    #include "utils/cpu_usage.h"
    #include "utils/ustdlib.h"
    #include "drivers/cfal96x64x16.h"
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>uDMA (udma_demo)</h1>
    //!
    //! This example application demonstrates the use of the uDMA controller to
    //! transfer data between memory buffers, and to transfer data to and from a
    //! UART.  The test runs for 10 seconds before exiting.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // The number of SysTick ticks per second used for the SysTick interrupt.
    //
    //*****************************************************************************
    #define SYSTICKS_PER_SECOND     100
    
    //*****************************************************************************
    //
    // The size of the memory transfer source and destination buffers (in words).
    //
    //*****************************************************************************
    #define MEM_BUFFER_SIZE         1024
    
    //*****************************************************************************
    //
    // The size of the UART transmit and receive buffers.  They do not need to be
    // the same size.
    //
    //*****************************************************************************
    #define UART_TXBUF_SIZE         256
    #define UART_RXBUF_SIZE         256
    
    //*****************************************************************************
    //
    // Graphics context used to show text on the CSTN display.
    //
    //*****************************************************************************
    static tContext g_sContext;
    
    //*****************************************************************************
    //
    // The source and destination buffers used for memory transfers.
    //
    //*****************************************************************************
    static uint32_t g_ui32SrcBuf[MEM_BUFFER_SIZE];
    static uint32_t g_ui32DstBuf[MEM_BUFFER_SIZE];
    
    //*****************************************************************************
    //
    // The transmit and receive buffers used for the UART transfers.  There is one
    // transmit buffer and a pair of recieve ping-pong buffers.
    //
    //*****************************************************************************
    static uint8_t g_ui8TxBuf[UART_TXBUF_SIZE];
    static uint8_t g_ui8RxBufA[UART_RXBUF_SIZE];
    static uint8_t g_ui8RxBufB[UART_RXBUF_SIZE];
    
    //*****************************************************************************
    //
    // The count of uDMA errors.  This value is incremented by the uDMA error
    // handler.
    //
    //*****************************************************************************
    static uint32_t g_ui32uDMAErrCount = 0;
    
    //*****************************************************************************
    //
    // The count of times the uDMA interrupt occurred but the uDMA transfer was not
    // complete.  This should remain 0.
    //
    //*****************************************************************************
    static uint32_t g_ui32BadISR = 0;
    
    //*****************************************************************************
    //
    // The count of UART buffers filled, one for each ping-pong buffer.
    //
    //*****************************************************************************
    static uint32_t g_ui32RxBufACount = 0;
    static uint32_t g_ui32RxBufBCount = 0;
    
    //*****************************************************************************
    //
    // The count of memory uDMA transfer blocks.  This value is incremented by the
    // uDMA interrupt handler whenever a memory block transfer is completed.
    //
    //*****************************************************************************
    static uint32_t g_ui32MemXferCount = 0;
    
    //*****************************************************************************
    //
    // The CPU usage in percent, in 16.16 fixed point format.
    //
    //*****************************************************************************
    static uint32_t g_ui32CPUUsage;
    
    //*****************************************************************************
    //
    // The number of seconds elapsed since the start of the program.  This value is
    // maintained by the SysTick interrupt handler.
    //
    //*****************************************************************************
    static uint32_t g_ui32Seconds = 0;
    
    //*****************************************************************************
    //
    // The number of ticks elapsed since the start of the program.  This value is
    // maintained by the SysTick interrupt handler.
    //
    //*****************************************************************************
    static uint32_t g_ui32TickCount = 0;
    
    //*****************************************************************************
    //
    // The control table used by the uDMA controller.  This table must be aligned
    // to a 1024 byte boundary.
    //
    //*****************************************************************************
    #if defined(ewarm)
    #pragma data_alignment=1024
    uint8_t ui8ControlTable[1024];
    #elif defined(ccs)
    #pragma DATA_ALIGN(ui8ControlTable, 1024)
    uint8_t ui8ControlTable[1024];
    #else
    uint8_t ui8ControlTable[1024] __attribute__ ((aligned(1024)));
    #endif
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif
    
    //*****************************************************************************
    //
    // The interrupt handler for the SysTick timer.  This handler will increment a
    // seconds counter whenever the appropriate number of ticks has occurred.  It
    // will also call the CPU usage tick function to find the CPU usage percent.
    //
    //*****************************************************************************
    void
    SysTickHandler(void)
    {
        //
        // Increment the tick counter.
        //
        g_ui32TickCount++;
    
        //
        // If the number of ticks per second has occurred, then increment the
        // seconds counter.
        //
        if(!(g_ui32TickCount % SYSTICKS_PER_SECOND))
        {
            g_ui32Seconds++;
        }
    
        //
        // Call the CPU usage tick function.  This function will compute the amount
        // of cycles used by the CPU since the last call and return the result in
        // percent in fixed point 16.16 format.
        //
        g_ui32CPUUsage = CPUUsageTick();
    }
    
    //*****************************************************************************
    //
    // The interrupt handler for uDMA errors.  This interrupt will occur if the
    // uDMA encounters a bus error while trying to perform a transfer.  This
    // handler just increments a counter if an error occurs.
    //
    //*****************************************************************************
    void
    uDMAErrorHandler(void)
    {
        uint32_t ui32Status;
    
        //
        // Check for uDMA error bit
        //
        ui32Status = ROM_uDMAErrorStatusGet();
    
        //
        // If there is a uDMA error, then clear the error and increment
        // the error counter.
        //
        if(ui32Status)
        {
            ROM_uDMAErrorStatusClear();
            g_ui32uDMAErrCount++;
        }
    }
    
    //*****************************************************************************
    //
    // The interrupt handler for uDMA interrupts from the memory channel.  This
    // interrupt will increment a counter, and then restart another memory
    // transfer.
    //
    //*****************************************************************************
    void
    uDMAIntHandler(void)
    {
        uint32_t ui32Mode;
    
        //
        // Check for the primary control structure to indicate complete.
        //
        ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_SW);
        if(ui32Mode == UDMA_MODE_STOP)
        {
            //
            // Increment the count of completed transfers.
            //
            g_ui32MemXferCount++;
    
            //
            // Configure it for another transfer.
            //
            ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SW, UDMA_MODE_AUTO,
                                       g_ui32SrcBuf, g_ui32DstBuf,
                                       MEM_BUFFER_SIZE);
    
            //
            // Initiate another transfer.
            //
            ROM_uDMAChannelEnable(UDMA_CHANNEL_SW);
            ROM_uDMAChannelRequest(UDMA_CHANNEL_SW);
        }
    
        //
        // If the channel is not stopped, then something is wrong.
        //
        else
        {
            g_ui32BadISR++;
        }
    }
    
    //*****************************************************************************
    //
    // The interrupt handler for UART0.  This interrupt will occur when a DMA
    // transfer is complete using the UART0 uDMA channel.  It will also be
    // triggered if the peripheral signals an error.  This interrupt handler will
    // switch between receive ping-pong buffers A and B.  It will also restart a TX
    // uDMA transfer if the prior transfer is complete.  This will keep the UART
    // running continuously (looping TX data back to RX).
    //
    //*****************************************************************************
    void
    UART0IntHandler(void)
    {
        uint32_t ui32Status;
        uint32_t ui32Mode;
    
        //
        // Read the interrupt status of the UART.
        //
        ui32Status = ROM_UARTIntStatus(UART0_BASE, 1);
    
        //
        // Clear any pending status, even though there should be none since no UART
        // interrupts were enabled.  If UART error interrupts were enabled, then
        // those interrupts could occur here and should be handled.  Since uDMA is
        // used for both the RX and TX, then neither of those interrupts should be
        // enabled.
        //
        ROM_UARTIntClear(UART0_BASE, ui32Status);
    
        //
        // Check the DMA control table to see if the ping-pong "A" transfer is
        // complete.  The "A" transfer uses receive buffer "A", and the primary
        // control structure.
        //
        ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT);
    
        //
        // If the primary control structure indicates stop, that means the "A"
        // receive buffer is done.  The uDMA controller should still be receiving
        // data into the "B" buffer.
        //
        if(ui32Mode == UDMA_MODE_STOP)
        {
            //
            // Increment a counter to indicate data was received into buffer A.  In
            // a real application this would be used to signal the main thread that
            // data was received so the main thread can process the data.
            //
            g_ui32RxBufACount++;
    
            //
            // Set up the next transfer for the "A" buffer, using the primary
            // control structure.  When the ongoing receive into the "B" buffer is
            // done, the uDMA controller will switch back to this one.  This
            // example re-uses buffer A, but a more sophisticated application could
            // use a rotating set of buffers to increase the amount of time that
            // the main thread has to process the data in the buffer before it is
            // reused.
            //
            ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
                                       UDMA_MODE_PINGPONG,
                                       (void *)(UART0_BASE + UART_O_DR),
                                       g_ui8RxBufA, sizeof(g_ui8RxBufA));
        }
    
        //
        // Check the DMA control table to see if the ping-pong "B" transfer is
        // complete.  The "B" transfer uses receive buffer "B", and the alternate
        // control structure.
        //
        ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT);
    
        //
        // If the alternate control structure indicates stop, that means the "B"
        // receive buffer is done.  The uDMA controller should still be receiving
        // data into the "A" buffer.
        //
        if(ui32Mode == UDMA_MODE_STOP)
        {
            //
            // Increment a counter to indicate data was received into buffer A.  In
            // a real application this would be used to signal the main thread that
            // data was received so the main thread can process the data.
            //
            g_ui32RxBufBCount++;
    
            //
            // Set up the next transfer for the "B" buffer, using the alternate
            // control structure.  When the ongoing receive into the "A" buffer is
            // done, the uDMA controller will switch back to this one.  This
            // example re-uses buffer B, but a more sophisticated application could
            // use a rotating set of buffers to increase the amount of time that
            // the main thread has to process the data in the buffer before it is
            // reused.
            //
            ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
                                       UDMA_MODE_PINGPONG,
                                       (void *)(UART0_BASE + UART_O_DR),
                                       g_ui8RxBufB, sizeof(g_ui8RxBufB));
        }
    
        //
        // If the UART0 DMA TX channel is disabled, that means the TX DMA transfer
        // is done.
        //
        if(!ROM_uDMAChannelIsEnabled(UDMA_CHANNEL_UART0TX))
        {
            //
            // Start another DMA transfer to UART0 TX.
            //
            ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
                                       UDMA_MODE_BASIC, g_ui8TxBuf,
                                       (void *)(UART0_BASE + UART_O_DR),
                                       sizeof(g_ui8TxBuf));
    
            //
            // The uDMA TX channel must be re-enabled.
            //
            ROM_uDMAChannelEnable(UDMA_CHANNEL_UART0TX);
        }
    }
    
    //*****************************************************************************
    //
    // Initializes the UART0 peripheral and sets up the TX and RX uDMA channels.
    // The UART is configured for loopback mode so that any data sent on TX will be
    // received on RX.  The uDMA channels are configured so that the TX channel
    // will copy data from a buffer to the UART TX output.  And the uDMA RX channel
    // will receive any incoming data into a pair of buffers in ping-pong mode.
    //
    //*****************************************************************************
    void
    InitUART0Transfer(void)
    {
        uint_fast16_t ui16Idx;
    
        //
        // Fill the TX buffer with a simple data pattern.
        //
        for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
        {
            g_ui8TxBuf[ui16Idx] = ui16Idx;
        }
    
        //
        // Enable the UART peripheral, and configure it to operate even if the CPU
        // is in sleep.
        //
        ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
        ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART0);
    
        //
        // Configure the UART communication parameters.
        //
        ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 115200,
                                UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
                                UART_CONFIG_PAR_NONE);
    
        //
        // Set both the TX and RX trigger thresholds to 4.  This will be used by
        // the uDMA controller to signal when more data should be transferred.  The
        // uDMA TX and RX channels will be configured so that it can transfer 4
        // bytes in a burst when the UART is ready to transfer more data.
        //
        ROM_UARTFIFOLevelSet(UART0_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);
    
        //
        // Enable the UART for operation, and enable the uDMA interface for both TX
        // and RX channels.
        //
        ROM_UARTEnable(UART0_BASE);
        ROM_UARTDMAEnable(UART0_BASE, UART_DMA_RX | UART_DMA_TX);
    
        //
        // This register write will set the UART to operate in loopback mode.  Any
        // data sent on the TX output will be received on the RX input.
        //
        HWREG(UART0_BASE + UART_O_CTL) |= UART_CTL_LBE;
    
        //
        // Enable the UART peripheral interrupts.  Note that no UART interrupts
        // were enabled, but the uDMA controller will cause an interrupt on the
        // UART interrupt signal when a uDMA transfer is complete.
        //
        ROM_IntEnable(INT_UART0);
    
        //
        // Put the attributes in a known state for the uDMA UART0RX channel.  These
        // should already be disabled by default.
        //
        ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART0RX,
                                        UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
                                        UDMA_ATTR_HIGH_PRIORITY |
                                        UDMA_ATTR_REQMASK);
    
        //
        // Configure the control parameters for the primary control structure for
        // the UART RX channel.  The primary contol structure is used for the "A"
        // part of the ping-pong receive.  The transfer data size is 8 bits, the
        // source address does not increment since it will be reading from a
        // register.  The destination address increment is byte 8-bit bytes.  The
        // arbitration size is set to 4 to match the RX FIFO trigger threshold.
        // The uDMA controller will use a 4 byte burst transfer if possible.  This
        // will be somewhat more effecient that single byte transfers.
        //
        ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
                                  UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                                  UDMA_ARB_4);
    
        //
        // Configure the control parameters for the alternate control structure for
        // the UART RX channel.  The alternate contol structure is used for the "B"
        // part of the ping-pong receive.  The configuration is identical to the
        // primary/A control structure.
        //
        ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
                                  UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                                  UDMA_ARB_4);
    
        //
        // Set up the transfer parameters for the UART RX primary control
        // structure.  The mode is set to ping-pong, the transfer source is the
        // UART data register, and the destination is the receive "A" buffer.  The
        // transfer size is set to match the size of the buffer.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
                                   UDMA_MODE_PINGPONG,
                                   (void *)(UART0_BASE + UART_O_DR),
                                   g_ui8RxBufA, sizeof(g_ui8RxBufA));
    
        //
        // Set up the transfer parameters for the UART RX alternate control
        // structure.  The mode is set to ping-pong, the transfer source is the
        // UART data register, and the destination is the receive "B" buffer.  The
        // transfer size is set to match the size of the buffer.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
                                   UDMA_MODE_PINGPONG,
                                   (void *)(UART0_BASE + UART_O_DR),
                                   g_ui8RxBufB, sizeof(g_ui8RxBufB));
    
        //
        // Put the attributes in a known state for the uDMA UART0TX channel.  These
        // should already be disabled by default.
        //
        ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART0TX,
                                        UDMA_ATTR_ALTSELECT |
                                        UDMA_ATTR_HIGH_PRIORITY |
                                        UDMA_ATTR_REQMASK);
    
        //
        // Set the USEBURST attribute for the uDMA UART TX channel.  This will
        // force the controller to always use a burst when transferring data from
        // the TX buffer to the UART.  This is somewhat more effecient bus usage
        // than the default which allows single or burst transfers.
        //
        ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_UART0TX, UDMA_ATTR_USEBURST);
    
        //
        // Configure the control parameters for the UART TX.  The uDMA UART TX
        // channel is used to transfer a block of data from a buffer to the UART.
        // The data size is 8 bits.  The source address increment is 8-bit bytes
        // since the data is coming from a buffer.  The destination increment is
        // none since the data is to be written to the UART data register.  The
        // arbitration size is set to 4, which matches the UART TX FIFO trigger
        // threshold.
        //
        ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
                                  UDMA_SIZE_8 | UDMA_SRC_INC_8 | UDMA_DST_INC_NONE |
                                  UDMA_ARB_4);
    
        //
        // Set up the transfer parameters for the uDMA UART TX channel.  This will
        // configure the transfer source and destination and the transfer size.
        // Basic mode is used because the peripheral is making the uDMA transfer
        // request.  The source is the TX buffer and the destination is the UART
        // data register.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
                                   UDMA_MODE_BASIC, g_ui8TxBuf,
                                   (void *)(UART0_BASE + UART_O_DR),
                                   sizeof(g_ui8TxBuf));
    
        //
        // Now both the uDMA UART TX and RX channels are primed to start a
        // transfer.  As soon as the channels are enabled, the peripheral will
        // issue a transfer request and the data transfers will begin.
        //
        ROM_uDMAChannelEnable(UDMA_CHANNEL_UART0RX);
        ROM_uDMAChannelEnable(UDMA_CHANNEL_UART0TX);
    }
    
    //*****************************************************************************
    //
    // Initializes the uDMA software channel to perform a memory to memory uDMA
    // transfer.
    //
    //*****************************************************************************
    void
    InitSWTransfer(void)
    {
        uint_fast16_t ui16Idx;
    
        //
        // Fill the source memory buffer with a simple incrementing pattern.
        //
        for(ui16Idx = 0; ui16Idx < MEM_BUFFER_SIZE; ui16Idx++)
        {
            g_ui32SrcBuf[ui16Idx] = ui16Idx;
        }
    
        //
        // Enable interrupts from the uDMA software channel.
        //
        ROM_IntEnable(INT_UDMA);
    
        //
        // Put the attributes in a known state for the uDMA software channel.
        // These should already be disabled by default.
        //
        ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_SW,
                                        UDMA_ATTR_USEBURST | UDMA_ATTR_ALTSELECT |
                                        (UDMA_ATTR_HIGH_PRIORITY |
                                        UDMA_ATTR_REQMASK));
    
        //
        // Configure the control parameters for the SW channel.  The SW channel
        // will be used to transfer between two memory buffers, 32 bits at a time.
        // Therefore the data size is 32 bits, and the address increment is 32 bits
        // for both source and destination.  The arbitration size will be set to 8,
        // which causes the uDMA controller to rearbitrate after 8 items are
        // transferred.  This keeps this channel from hogging the uDMA controller
        // once the transfer is started, and allows other channels cycles if they
        // are higher priority.
        //
        ROM_uDMAChannelControlSet(UDMA_CHANNEL_SW | UDMA_PRI_SELECT,
                                  UDMA_SIZE_32 | UDMA_SRC_INC_32 | UDMA_DST_INC_32 |
                                  UDMA_ARB_8);
    
        //
        // Set up the transfer parameters for the software channel.  This will
        // configure the transfer buffers and the transfer size.  Auto mode must be
        // used for software transfers.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SW | UDMA_PRI_SELECT,
                                   UDMA_MODE_AUTO, g_ui32SrcBuf, g_ui32DstBuf,
                                   MEM_BUFFER_SIZE);
    
        //
        // Now the software channel is primed to start a transfer.  The channel
        // must be enabled.  For software based transfers, a request must be
        // issued.  After this, the uDMA memory transfer begins.
        //
        ROM_uDMAChannelEnable(UDMA_CHANNEL_SW);
        ROM_uDMAChannelRequest(UDMA_CHANNEL_SW);
    }
    
    //*****************************************************************************
    //
    // This example demonstrates how to use the uDMA controller to transfer data
    // between memory buffers and to and from a peripheral, in this case a UART.
    // The uDMA controller is configured to repeatedly transfer a block of data
    // from one memory buffer to another.  It is also set up to repeatedly copy a
    // block of data from a buffer to the UART output.  The UART data is looped
    // back so the same data is received, and the uDMA controlled is configured to
    // continuously receive the UART data using ping-pong buffers.
    //
    // The processor is put to sleep when it is not doing anything, and this allows
    // collection of CPU usage data to see how much CPU is being used while the
    // data transfers are ongoing.
    //
    //*****************************************************************************
    int
    main(void)
    {
        static uint32_t ui32PrevSeconds;
        static uint32_t ui32PrevXferCount;
        static uint32_t ui32PrevUARTCount = 0;
        static char pcStrBuf[40];
        tRectangle sRect;
        uint32_t ui32CenterX;
        uint32_t ui32XfersCompleted;
        uint32_t ui32BytesTransferred;
    
        //
        // Enable lazy stacking for interrupt handlers.  This allows floating-point
        // instructions to be used within interrupt handlers, but at the expense of
        // extra stack usage.
        //
        ROM_FPULazyStackingEnable();
    
        //
        // Set the clocking to run from the PLL at 50 MHz.
        //
        ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
                           SYSCTL_XTAL_16MHZ);
    
        //
        // Enable peripherals to operate when CPU is in sleep.
        //
        ROM_SysCtlPeripheralClockGating(true);
    
        //
        // Initialize the display driver.
        //
        CFAL96x64x16Init();
    
        //
        // Initialize the graphics context and find the middle X coordinate.
        //
        GrContextInit(&g_sContext, &g_sCFAL96x64x16);
    
        //
        // Get the center X coordinate of the screen, since it is used a lot.
        //
        ui32CenterX = GrContextDpyWidthGet(&g_sContext) / 2;
    
        //
        // Fill the top part of the screen with blue to create the banner.
        //
        sRect.i16XMin = 0;
        sRect.i16YMin = 0;
        sRect.i16XMax = GrContextDpyWidthGet(&g_sContext) - 1;
        sRect.i16YMax = 9;
        GrContextForegroundSet(&g_sContext, ClrDarkBlue);
        GrRectFill(&g_sContext, &sRect);
    
        //
        // Change foreground for white text.
        //
        GrContextForegroundSet(&g_sContext, ClrWhite);
    
        //
        // Put the application name in the middle of the banner.
        //
        GrContextFontSet(&g_sContext, g_psFontFixed6x8);
        GrStringDrawCentered(&g_sContext, "udma-demo", -1, ui32CenterX, 4, 0);
    
        //
        // Show the clock frequency on the display.
        //
        GrContextFontSet(&g_sContext, g_psFontFixed6x8);
        usnprintf(pcStrBuf, sizeof(pcStrBuf), "%u MHz",
                  ROM_SysCtlClockGet() / 1000000);
        GrStringDrawCentered(&g_sContext, pcStrBuf, -1, ui32CenterX, 14, 0);
    
        //
        // Show static text and field labels on the display.
        //
        GrStringDraw(&g_sContext, "Mem", -1, 0, 22, 0);
        GrStringDraw(&g_sContext, "UART", -1, 0, 32, 0);
    
        //
        // Configure SysTick to occur 100 times per second, to use as a time
        // reference.  Enable SysTick to generate interrupts.
        //
        ROM_SysTickPeriodSet(ROM_SysCtlClockGet() / SYSTICKS_PER_SECOND);
        ROM_SysTickIntEnable();
        ROM_SysTickEnable();
    
        //
        // Initialize the CPU usage measurement routine.
        //
        CPUUsageInit(ROM_SysCtlClockGet(), SYSTICKS_PER_SECOND, 2);
    
        //
        // Enable the uDMA controller at the system level.  Enable it to continue
        // to run while the processor is in sleep.
        //
        ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
        ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
    
        //
        // Enable the uDMA controller error interrupt.  This interrupt will occur
        // if there is a bus error during a transfer.
        //
        ROM_IntEnable(INT_UDMAERR);
    
        //
        // Enable the uDMA controller.
        //
        ROM_uDMAEnable();
    
        //
        // Point at the control table to use for channel control structures.
        //
        ROM_uDMAControlBaseSet(ui8ControlTable);
    
        //
        // Initialize the uDMA memory to memory transfers.
        //
        InitSWTransfer();
    
        //
        // Initialize the uDMA UART transfers.
        //
        InitUART0Transfer();
    
        //
        // Remember the current SysTick seconds count.
        //
        ui32PrevSeconds = g_ui32Seconds;
    
        //
        // Remember the current count of memory buffer transfers.
        //
        ui32PrevXferCount = g_ui32MemXferCount;
    
        //
        // Loop until the button is pressed.  The processor is put to sleep
        // in this loop so that CPU utilization can be measured.
        //
        while(1)
        {
            //
            // Check to see if one second has elapsed.  If so, the make some
            // updates.
            //
            if(g_ui32Seconds != ui32PrevSeconds)
            {
                //
                // Print a message to the display showing the CPU usage percent.
                // The fractional part of the percent value is ignored.
                //
                usnprintf(pcStrBuf, sizeof(pcStrBuf), "CPU %2u%%",
                          g_ui32CPUUsage >> 16);
                GrStringDrawCentered(&g_sContext, pcStrBuf, -1, ui32CenterX, 44,
                                     1);
    
                //
                // Tell the user how many seconds we have to go before ending.
                //
                usnprintf(pcStrBuf, sizeof(pcStrBuf), " %d seconds ",
                          10 - g_ui32Seconds);
                GrStringDrawCentered(&g_sContext, pcStrBuf, -1, ui32CenterX, 54,
                                     1);
    
                //
                // Remember the new seconds count.
                //
                ui32PrevSeconds = g_ui32Seconds;
    
                //
                // Calculate how many memory transfers have occurred since the last
                // second.
                //
                ui32XfersCompleted = g_ui32MemXferCount - ui32PrevXferCount;
    
                //
                // Remember the new transfer count.
                //
                ui32PrevXferCount = g_ui32MemXferCount;
    
                //
                // Compute how many bytes were transferred in the memory transfer
                // since the last second.
                //
                ui32BytesTransferred = ui32XfersCompleted * MEM_BUFFER_SIZE * 4;
    
                //
                // Print a message to the display showing the memory transfer rate.
                //
                usnprintf(pcStrBuf, sizeof(pcStrBuf), "%8u B/s ",
                          ui32BytesTransferred);
                GrStringDraw(&g_sContext, pcStrBuf, -1, 24, 22, 1);
    
                //
                // Calculate how many UART transfers have occurred since the last
                // second.
                //
                ui32XfersCompleted = (g_ui32RxBufACount + g_ui32RxBufBCount -
                                    ui32PrevUARTCount);
    
                //
                // Remember the new UART transfer count.
                //
                ui32PrevUARTCount = g_ui32RxBufACount + g_ui32RxBufBCount;
    
                //
                // Compute how many bytes were transferred by the UART.  The number
                // of bytes received is multiplied by 2 so that the TX bytes
                // transferred are also accounted for.
                //
                ui32BytesTransferred = ui32XfersCompleted * UART_RXBUF_SIZE * 2;
    
                //
                // Print a message to the display showing the UART transfer rate.
                //
                usnprintf(pcStrBuf, sizeof(pcStrBuf), "%7u B/s ",
                          ui32BytesTransferred);
                GrStringDraw(&g_sContext, pcStrBuf, -1, 30, 32, 1);
            }
    
            //
            // Put the processor to sleep if there is nothing to do.  This allows
            // the CPU usage routine to measure the number of free CPU cycles.
            // If the processor is sleeping a lot, it can be hard to connect to
            // the target with the debugger.
            //
            ROM_SysCtlSleep();
    
            //
            // See if we have run int32_t enough and exit the loop if so.
            //
            if(g_ui32Seconds >= 10)
            {
                break;
            }
        }
    
        //
        // Indicate on the display that the example is stopped.
        //
        GrContextForegroundSet(&g_sContext, ClrRed);
        GrStringDrawCentered(&g_sContext, "    Stopped    ", -1,
                             ui32CenterX, 54, 1);
    
        //
        // Loop forever with the CPU not sleeping, so the debugger can connect.
        //
        while(1)
        {
        }
    }
    

    这是官方的串口DMA的例程,直接移植过去就好了。