This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

选型 DSP



各位TI工程师:
您好!
如下是需求,如有其他型号请推荐。
 
关于STM32F407替换,想选用TI的DSP,需求如下,帮忙筛一下
 
1、  处理速度>400DMIPS
2、  有低功耗模式,全速运行功耗最好<50mA,不能超过100Ma
3、  支持McBSP或类似的通信接口,可以模拟成I2S与codec相连
4、  支持SPI从接口
5、  支持DMA
6、  内置RAM >512K,FLASH > 1M
7、  尺寸越小越好,最好在10×10 mm以内