Other Parts Discussed in Thread: TM4C129EKCPDT
我有一个TM4C129的开发版DK-TM4C 129x,我的工程已经在这个开发板上完成了绝大部分的工作,现在我们自己做的板子已经回来,选用的是TM4C129EKCPDT,用自己的XDS100V2连接我们的目标板,Test Connection 可以通过测试,但是直接在CCS6中点F11进行编译连接下载时(代码不变,可能和封装和pin脚分配有关),编译没有问题,首次接入时有弹出进度条,但是很快就结束了,弹框报错如下:
Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
用板载ICDI仿真器(接法和XDS100V2)通过LM Flash Programmer读取TM4C129EKCPDT ,的MAC地址 提示 Unable to initialize target - 0
用LM Flash Programmer Unlock ,按操作完成了,也没有任何反应。
麻烦帮我分析一下什么原因,该怎么解决。
其中有用IDCI调试后换到XDS100V2 调试,和首次链接现象一样。若首次连接后,就不会弹出进度条,直接报错 Error 1170