Other Parts Discussed in Thread: MSP430G2955, MSP430FR4133
单片机下电,如果电压由正常的工作电压3.3V降到0V的过程时长在500ms左右(使用主频16M),这样会不会在电压到下降的这个过程中导致单片机程序跑飞,如果单片机程序中有擦写Flash的函数(函数有编译),如果频繁下电的测试操作,那跑飞有可能执行到擦写Flash的函数是吧?近期下电测试就有遇到这些问题。论坛里,有人遇到这样的问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430G2955, MSP430FR4133
单片机下电,如果电压由正常的工作电压3.3V降到0V的过程时长在500ms左右(使用主频16M),这样会不会在电压到下降的这个过程中导致单片机程序跑飞,如果单片机程序中有擦写Flash的函数(函数有编译),如果频繁下电的测试操作,那跑飞有可能执行到擦写Flash的函数是吧?近期下电测试就有遇到这些问题。论坛里,有人遇到这样的问题吗?
看了MSP430G2955的寄存器,这单片机没有欠压复位的功能,没有相关的寄存器可以操作
你好
我有一个办法你可以测试一下:你可以使用ADC去检测电压电压(不需要外部电路)ADC的采集通道可直接采用内部参考电压(一般为1.5V,具体请查看技术手册)进行采样,且ADC的参考电压是可以配置为电源电压。(这种电源电压检测的方法有官方例程的)。然后当检测到电压低时可以进入低功耗模式关闭CPU。
ADC可以设置成定时器或RTC触发然后用窗口比较器比较整个过程不需要CPU干预的,CPU可以做其它的事情。你可以先不用做这么复杂,先用CPU进行判断测试一下这个方法。
给你一个参考代码,但这个是在MSP430FR4133上测试的,到G2你要再稍微修改一下
#include <msp430.h>
#define High_Threshold 568
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
P1REN = 0xff;
P2REN = 0xff;
P3REN = 0xff;
P4REN = 0xf9;
P5REN = 0xff;
P6REN = 0xff;
P7REN = 0xff;
P8REN = 0x0f;
P1OUT =0;
P2OUT =0;
P3OUT =0;
P4OUT =0;
P5OUT =0;
P6OUT =0;
P7OUT =0;
P8OUT =0;
P8DIR=BIT0;//P8.0 SMCLK
P8SEL0 |= BIT0;
// SYSCFG2 |= ADCPCTL1;
P4SEL0 |= BIT1 | BIT2; // set XT1 pin as second function
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
do
{
CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
__bis_SR_register(SCG0); // disable FLL
CSCTL3 |= SELREF__XT1CLK; // Set XT1CLK as FLL reference source
__delay_cycles(3);
__bic_SR_register(SCG0); // enable FLL
while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK; // Set ACLK = XT1CLK = 32768Hz
// Configure ADC10
ADCCTL0 &= ~ADCENC; // Disable ADC
ADCCTL0 = ADCSHT_2 | ADCON; // ADCON, S&H=16 ADC clks
// ADCCTL1 = ADCSHP|ADCSSEL_1|ADCSHS_1|ADCCONSEQ_2; // sample_timer,ACLK,rtc,repeat_single
ADCCTL1 = ADCSHP|ADCSHS_1|ADCCONSEQ_2; // sample_timer,MODCLK,rtc,repeat_single
ADCHI = High_Threshold; // Window Comparator Hi-threshold
ADCMCTL0 = ADCINCH_13 | ADCSREF_0;
ADCIE = ADCHIIE;
ADCCTL2 = ADCRES|ADCSR;
// Configure reference module located in the PMM
PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
PMMCTL2 |= INTREFEN; // Enable internal reference
while(!(PMMCTL2 & REFGENRDY)); // Poll till internal reference settles
__delay_cycles(400); // Delay for reference settling
RTCMOD = 0x7; // Initialize RTC
RTCCTL = RTCSS_3 | RTCSR | RTCPS__1000 ;//VLOCLK,
ADCCTL0 |= ADCENC; // Sampling and conversion start
while(1)
{
// __delay_cycles(90000);
__bis_SR_register(LPM3_bits | GIE); // Enter LPM0, ADC_ISR will force exit
}
}
// ADC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADCIV, ADCIV_ADCIFG))
{
case ADCIV_NONE:
break;
case ADCIV_ADCOVIFG:
break;
case ADCIV_ADCTOVIFG:
break;
case ADCIV_ADCHIIFG:
__delay_cycles(2);//alarming
__bic_SR_register_on_exit(LPM3_bits);// Exit from LPM
break;
case ADCIV_ADCLOIFG:
break;
case ADCIV_ADCINIFG:
break;
case ADCIV_ADCIFG:
// adcResult = ADCMEM0; // Read ADC memory
// __bic_SR_register_on_exit(LPM0_bits);// Exit from LPM
break;
default:
break;
}
}