This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

STM32F4的主频选择和系统中其他模块的什么指标有关?



请问,STM32F4系列作为系统MCU主频168Mhz,为了满足168MHz的主频,那系统中其他通信模块、GPS模块等的选择应该注意哪些指标?是指其他模块的频率不高于168MHz?还是什么意思?

  • 这个应该是去ST的论坛里问那。不过友情支持一下,GPS一般都用模块,通过UART和MCU通讯,168M的主频支持GPS的UART问题不大。一般外设主频不高于系统主频。

  • 不知道你是不是来砸场子的,还是走错路了。

    我也顺便给你回答个:不管你是用32的单片机还是我们430的单片机,或者是别家的单片机,主频指的单片机的CPU可工作的运行最快速度,这个是不仅由CPU性能决定,同时有时钟系统决定。

    至于通信模块跟这个无关了,其他的外接通信模块比如是i2C接口或者是UART串口,或者SPI接口,只要跟对应的接口相接就行。这个不会要求你太多,只要满足接口的协议就行了。比如你用我们430单片机,把主频设置到1MHz都可以正常外接这些模块的。如果你不会使用硬件的通信接口,你还可以按照时序用IO模拟这个通信协议。