This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GXL launchpad做鼠标、游戏手柄的相关问题



现在手上有一块TM4C123GXL  launchpad,想做一个模拟USB鼠标,参考了TivaWare中提供的 “usb_dev_gamepad” 例程还是没有头绪,想问下各位大神几个问题:

1.用开发板做一个模拟USB鼠标需要了解什么知识?

2.下面usblib.h代码分别是什么模式?在什么时候使用?

typedef enum
{
    //
    //! Operate in USB device mode with active monitoring of VBUS and the
    //! ID pin must be pulled to a logic high value.
    //
    eUSBModeDevice = 0,

    //
    //! Operate in USB host mode with active monitoring of VBUS and the ID pin
    //! must be pulled to a logic low value.
    //
    eUSBModeHost,

    //
    //! Operate as an On-The-Go device which requires both VBUS and ID to be
    //! connected directly to the USB controller from the USB connector.
    //
    eUSBModeOTG,

    //
    //! A marker indicating that no USB mode has yet been set by the
    //! application.
    //
    eUSBModeNone,

    //
    //! Force host mode so that the VBUS and ID pins are not used or monitored
    //! by the USB controller.
    //
    eUSBModeForceHost,

    //
    //! Forcing device mode so that the VBUS and ID pins are not used or
    //! monitored by the USB controller.
    //
    eUSBModeForceDevice,
}
tUSBMode;

3.在usblib.h文件中有:

extern void USBStackModeSet(uint32_t ui32Index, tUSBMode iUSBMode, tUSBModeCallback pfnCallback);

想问下这个函数的三个参数分别代表什么?如何使用?

4.自己按例程改的代码如下,在main中运行到USBStackModeSet(0, eUSBModeForceDevice, 0);时会跳入错误函数,想了解这块怎么写?(main.c 82行)

以下为代码,其他用的都是官方代码就不贴了

main.c

#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "inc/hw_sysctl.h"
#include "driverlib/adc.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "usblib/usblib.h"
#include "usblib/usbhid.h"
#include "usblib/device/usbdevice.h"
#include "usblib/device/usbdhid.h"
#include "usblib/device/usbdhidmouse.h"
#include "usb_mouse_structs.h"
//#include "drivers/buttons.h"
#include "utils/uartstdio.h"
#include "drivers/rocker.h"

//extern void USBStackModeSet(uint32_t ui32Index, tUSBMode iUSBMode, tUSBModeCallback pfnCallback);
//void *USBDHIDMouseInit(uint32_t ui32Index, tUSBDHIDMouseDevice *psMouseDevice);
//uint32_t USBDHIDMouseStateChange(void *pvMouseDevice, int8_t i8DeltaX, int8_t i8DeltaY, uint8_t ui8Buttons);

void ConfigureUART(void);
uint32_t MouseHandler(void *pvCBData, uint32_t ui32Event, uint32_t ui32MsgData, void *pvMsgData);

volatile enum
{
    //
    // Not yet configured.
    //
    eStateNotConfigured,

    //
    // Connected and not waiting on data to be sent.
    //
    eStateIdle,

    //
    // Suspended.
    //
    eStateSuspend,

    //
    // Connected and waiting on data to be sent out.
    //
    eStateSending
}
g_iGamepadState;

int main(void)
{
	ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);

	//LED_RED
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
	ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2);

	ConfigureUART();
	
	// Not configured initially.
	g_iGamepadState = eStateNotConfigured;

	//
	// Enable the GPIO peripheral used for USB, and configure the USB
	// pins.
	//
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
	SysCtlGPIOAHBEnable(SYSCTL_PERIPH_GPIOD);
	ROM_GPIOPinTypeUSBAnalog(GPIO_PORTD_AHB_BASE, GPIO_PIN_4 | GPIO_PIN_5);

//	ButtonsInit();
//	ADCInit();

	UARTprintf("Configuring USB\n");

	USBStackModeSet(0, eUSBModeForceDevice, 0);

	USBDHIDMouseInit(0, &g_sMouseDevice);

	while(1)
		USBDHIDMouseStateChange(&g_sMouseDevice, 1, 1, 1);

	return 0;
}

void
ConfigureUART(void)
{
    //
    // Enable the GPIO Peripheral used by the UART.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    //
    // Enable UART0
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

    //
    // Configure GPIO Pins for UART mode.
    //
    ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
    ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
    ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    //
    // Use the internal 16MHz oscillator as the UART clock source.
    //
    UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);

    //
    // Initialize the UART for console I/O.
    //
    UARTStdioConfig(0, 115200, 16000000);
}

uint32_t MouseHandler(void *pvCBData, uint32_t ui32Event,
                               uint32_t ui32MsgData, void *pvMsgData)
{

}

usb_mouse_structs.c

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "usblib/usblib.h"
#include "usblib/usbhid.h"
#include "usblib/usb-ids.h"
#include "usblib/device/usbdevice.h"
#include "usblib/device/usbdcomp.h"
#include "usblib/device/usbdhid.h"
#include "usblib/device/usbdhidmouse.h"

#include "usb_mouse_structs.h"

//****************************************************************************
//
// The languages supported by this device.
//
//****************************************************************************
const uint8_t g_pui8LangDescriptor[] =
{
    4,
    USB_DTYPE_STRING,
    USBShort(USB_LANG_EN_US)
};

//****************************************************************************
//
// The manufacturer string.
//
//****************************************************************************
const uint8_t g_pui8ManufacturerString[] =
{
    (17 + 1) * 2,
    USB_DTYPE_STRING,
    'T', 0, 'e', 0, 'x', 0, 'a', 0, 's', 0, ' ', 0, 'I', 0, 'n', 0, 's', 0,
    't', 0, 'r', 0, 'u', 0, 'm', 0, 'e', 0, 'n', 0, 't', 0, 's', 0,
};

//****************************************************************************
//
// The product string.
//
//****************************************************************************
const uint8_t g_pui8ProductString[] =
{
    (17 + 1) * 2,
    USB_DTYPE_STRING,
    'E', 0, 'x', 0, 'a', 0, 'm', 0, 'p', 0, 'l', 0, 'e', 0, ' ', 0,
    'G', 0, 'a', 0, 'm', 0, 'e', 0, ' ', 0, 'P', 0, 'a', 0, 'd', 0, ' ', 0,
};

//****************************************************************************
//
// The serial number string.
//
//****************************************************************************
const uint8_t g_pui8SerialNumberString[] =
{
    (8 + 1) * 2,
    USB_DTYPE_STRING,
    '1', 0, '2', 0, '3', 0, '4', 0, '5', 0, '6', 0, '7', 0, '8', 0
};

//*****************************************************************************
//
// The interface description string.
//
//*****************************************************************************
const uint8_t g_pui8HIDInterfaceString[] =
{
    (21 + 1) * 2,
    USB_DTYPE_STRING,
    'H', 0, 'I', 0, 'D', 0, ' ', 0, 'G', 0, 'a', 0, 'm', 0, 'e', 0,
    'p', 0, 'a', 0, 'd', 0, ' ', 0, 'I', 0, 'n', 0, 't', 0, 'e', 0,
    'r', 0, 'f', 0, 'a', 0, 'c', 0, 'e', 0
};

//*****************************************************************************
//
// The configuration description string.
//
//*****************************************************************************
const uint8_t g_pui8ConfigString[] =
{
    (25 + 1) * 2,
    USB_DTYPE_STRING,
    'H', 0, 'I', 0, 'D', 0, ' ', 0, 'G', 0, 'a', 0, 'm', 0, 'e', 0,
    'p', 0, 'a', 0, 'd', 0, ' ', 0, 'C', 0, 'o', 0, 'n', 0, 'f', 0,
    'i', 0, 'g', 0, 'u', 0, 'r', 0, 'a', 0, 't', 0, 'i', 0, 'o', 0,
    'n', 0
};

//*****************************************************************************
//
// The descriptor string table.
//
//*****************************************************************************
const uint8_t * const g_ppui8StringDescriptors[] =
{
    g_pui8LangDescriptor,
    g_pui8ManufacturerString,
    g_pui8ProductString,
    g_pui8SerialNumberString,
    g_pui8HIDInterfaceString,
    g_pui8ConfigString
};

#define NUM_STRING_DESCRIPTORS (sizeof(g_ppui8StringDescriptors) /            \
                                sizeof(uint8_t *))

//*****************************************************************************
//
// The HID game pad device initialization and customization structures.
//
//*****************************************************************************
tUSBDHIDMouseDevice  g_sMouseDevice =
{
    USB_VID_TI_1CBE,
	USB_PID_MOUSE,
    500,
    USB_CONF_ATTR_SELF_PWR | USB_CONF_ATTR_RWAKE,
	USB_PID_MOUSE,
    (void *)&g_sMouseDevice,
    g_ppui8StringDescriptors,
    NUM_STRING_DESCRIPTORS
};

感谢各位工程师、大佬们赐教。

编译环境:win7,CCS6.2