This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123x使用知识点1----某些特殊引脚被lock不能使用需要解锁的处理



以下解决办法均来自于TI的官方。

当TM4C123x的一些引脚比如PC0/PC1/PC2/PC3,PD7,PF0或者PE7被用作JTAG特定功能,NMI特使功能引脚的时候,需要切换这些引脚为其他功能的时候,需要进行解锁并提交的,解锁的示例代码如下。

#include "inc/hw_types.h"

#include "inc/hw_gpio.h"

#include "inc/hw_memmap.h"

TM4C123 Devices Port-C

HWREG(GPIO_PORTC_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY;

HWREG(GPIO_PORTC_BASE+GPIO_O_CR) |= (GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);

TM4C123 Devices Port-D

HWREG(GPIO_PORTD_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY;

HWREG(GPIO_PORTD_BASE+GPIO_O_CR) |= GPIO_PIN_7;

TM4C123 Devices Port-F

HWREG(GPIO_PORTF_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY;

HWREG(GPIO_PORTF_BASE+GPIO_O_CR) |= GPIO_PIN_0;

TM4C129 Devices Port-C

HWREG(GPIO_PORTC_AHB_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY;

HWREG(GPIO_PORTC_AHB_BASE+GPIO_O_CR) |= (GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);

TM4C129 Devices Port-D

HWREG(GPIO_PORTD_AHB_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY;

HWREG(GPIO_PORTD_AHB_BASE+GPIO_O_CR) |= GPIO_PIN_7;

TM4C129 Devices Port-E

HWREG(GPIO_PORTE_AHB_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY;

HWREG(GPIO_PORTE_AHB_BASE+GPIO_O_CR) |= GPIO_PIN_7;