This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,关于TM4C1294控制颜色传感器TCS34725的问题

#include <stdint.h>
#include <stdbool.h>
#include <stdio.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "inc/hw_i2c.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/i2c.h"
#include "utils/uartstdio.h"

#define SLAVE_ADDRESS           0x29
#define AMBIENT_TEMPERATURE     0x05
#define DEVICE_ID_REGISTER          0x12
#define MANUFACTURE_ID_REGISTER     0x07
#define TCS34725_ENABLE           0x00
#define TCS34725_ENABLE_PON       0x01

uint16_t convertTemp(uint8_t, uint8_t);
void ConfigureUART(void);
void I2C_Init(void);
void I2C_Send(void);
uint16_t I2C_readMode(void);
uint16_t I2C_TempRead(void);
void Device_ID(uint8_t device_reg);
void Manufacture_ID(uint8_t manufacture_reg);
void Ambient_Temp(uint8_t ambient_temp_reg);

uint8_t readI2C0(uint16_t device_address, uint16_t device_register)
{
    //specify that we want to communicate to device address with an intended write to bus
    I2CMasterSlaveAddrSet(I2C0_BASE, device_address, false);

    //the register to be read
    I2CMasterDataPut(I2C0_BASE, device_register);

    //send control byte and register address byte to slave device
    I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);

    //wait for MCU to complete send transaction
    while(I2CMasterBusy(I2C0_BASE));

    //read from the specified slave device
    I2CMasterSlaveAddrSet(I2C0_BASE, device_address, true);

    //send control byte and read from the register from the MCU
    I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);

    //wait while checking for MCU to complete the transaction
    while(I2CMasterBusy(I2C0_BASE));

    //Get the data from the MCU register and return to caller
    return( I2CMasterDataGet(I2C0_BASE));
}

void writeI2C0(uint16_t device_address, uint16_t device_register, uint8_t device_data)
{
    //specify that we want to communicate to device address with an intended write to bus
    I2CMasterSlaveAddrSet(I2C0_BASE, device_address, false);

    //register to be read
    I2CMasterDataPut(I2C0_BASE, device_register);

    //send control byte and register address byte to slave device
    I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);

    //wait for MCU to finish transaction
    while(I2CMasterBusy(I2C0_BASE));

    I2CMasterSlaveAddrSet(I2C0_BASE, device_address, true);

    //specify data to be written to the above mentioned device_register
    I2CMasterDataPut(I2C0_BASE, device_data);

    //wait while checking for MCU to complete the transaction
    I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);

    //wait for MCU & device to complete transaction
    while(I2CMasterBusy(I2C0_BASE));
}




int main(void)
{
    FPULazyStackingEnable();
    uint8_t Device_id = 0;
    uint16_t Manufacture_id = 0;

    // Set the clocking to run directly from the crystal
    //SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);

    // Enable the GPIO Port that is used for the on-board LEDs
    //SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    // Enable the GPIO Pins for the LEDs (PF1, PF2, PF3);
    //GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);

    // Initialize the UART
    ConfigureUART();
    SysCtlDelay(10000000);
    UARTprintf("Program Starting....\n\n");
    SysCtlDelay(50000000);
    UARTprintf("UART Initialized\n");
    SysCtlDelay(50000000);

    I2C_Init();
    SysCtlDelay(50000000);

    writeI2C0(SLAVE_ADDRESS,TCS34725_ENABLE,TCS34725_ENABLE_PON);
    UARTprintf("POWER ON!\n");
    SysCtlDelay(10000000);
    // I2C Send data to Slave Address - Device ID register - See MCP9808 datasheet
    //I2C_Send();
    //Device_ID(DEVICE_ID_REGISTER);
    //while(I2CMasterBusy(I2C0_BASE))
    //{
    //}
    Device_id = readI2C0(SLAVE_ADDRESS,DEVICE_ID_REGISTER);
    UARTprintf("Received Device ID from Slave: 0x%x\n\r", Device_id);
    SysCtlDelay(50000000);


}

void ConfigureUART(void)
{
  // Enable the GPIO Peripheral used by the UART
  SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

  SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

  // Configure the GPIO Pins for UART mode
  GPIOPinConfigure(GPIO_PA0_U0RX);
  GPIOPinConfigure(GPIO_PA1_U0TX);
  GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

  // Use the internal 16MHz oscillator as the UART Clock source
  UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);

  // Initialize the UART for console I/O.
  UARTStdioConfig(0, 9600, 16000000);
}

void I2C_Init()
{
    // Enable I2C1 peripheral
  SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
  SysCtlPeripheralReset(SYSCTL_PERIPH_I2C0);

  // Enable GPIO Port B to be used for I2C0
  SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

  GPIOPinConfigure(GPIO_PB2_I2C0SCL);
  GPIOPinConfigure(GPIO_PB3_I2C0SDA);

  // Configure the pin muxing for I2C1 functions on Port B2 and B3
  GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
  GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);

  I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
  // Set write mode
  UARTprintf("I2C Master init communication with Slave Address\n");
  SysCtlDelay(10000);
  UARTprintf("I2C Init complete!\n");
  SysCtlDelay(50000000);
}

void I2C_Send()
{
  // Specify Slave device address to write to
  I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, false);
  UARTprintf("Master transmit to Slave address\n\n");
}

void Device_ID(uint8_t device_reg)
{
  // Send Register address on Slave device
  I2CMasterDataPut(I2C0_BASE, device_reg);
  UARTprintf("Writing to device id register on Slave address\n");

  // Initiate send of register address from Master to Slave
  I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
  UARTprintf("Device ID register sent to Slave address\n");
}



uint16_t I2C_readMode()
{
  uint8_t UpperByte = 0;
  uint8_t LowerByte = 0;
  uint16_t data = 0;
  // Set read mode
  I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, true);

  // Get first byte from slave and ack for more
  I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
  while(I2CMasterBusy(I2C0_BASE));

  UpperByte = I2CMasterDataGet(I2C0_BASE);

  // Get second byte from slave and nack for complete
  I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
  while(I2CMasterBusy(I2C0_BASE));
  LowerByte = I2CMasterDataGet(I2C0_BASE);

  // See MCP9808 Data Sheet for each of the register information requested for
  data = UpperByte<<8|LowerByte;
  return data;
}
代码如上,按照我的预期,他应该可以读到设备的ID号0x44才对,可是他总是返回0x0.是我哪里没写对吗,还是?求指教,谢谢!
TCS34725的数据手册也上传了,寄存器地址什么的可以看数据手册,感觉寄存器地址也可能出问题?因为我DEBUG的时候那个SLAVEADRESS的值也不是我预期的
。。。。求赐教

TCS34725.pdf