This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我准备用msp432的driver例程中pwmled的例程编写一个马达控制程序,再修改测试过程中发现无法使用Timer_A0这个硬件资源,我在board.h,msp432p401r.h,msp432p401r.c中做了相应的修改,但依然无法打开Timer_A0。Timer_A1-A3都可以用。程序如下。
“Board.h”
#define Board_TIMER0 MSP_EXP432P401R_TIMER_T32_0
#define Board_TIMER1 MSP_EXP432P401R_TIMER_T32_1
#define Board_TIMER2 MSP_EXP432P401R_TIMER_TA_0
#define Board_TIMER3 MSP_EXP432P401R_TIMER_TA_1
#define Board_TIMER4 MSP_EXP432P401R_TIMER_TA_2
#define Board_TIMER5 MSP_EXP432P401R_TIMER_TA_3
“msp432p401r.h”
/*!
* @def MSP_EXP432P401R_TimerName
* @brief Enum of Timer names on the MSP_EXP432P401R dev board
*/
typedef enum MSP_EXP432P401R_TimerName {
MSP_EXP432P401R_TIMER_T32_0 = 0,
MSP_EXP432P401R_TIMER_T32_1,
MSP_EXP432P401R_TIMER_TA_0,
MSP_EXP432P401R_TIMER_TA_1,
MSP_EXP432P401R_TIMER_TA_2,
MSP_EXP432P401R_TIMER_TA_3,
MSP_EXP432P401R_TIMERCOUNT
} MSP_EXP432P401R_TimerName;
“msp432p401r.c”
/*
* =============================== Timer ===============================
*/
#include <ti/drivers/Timer.h>
#include <ti/drivers/timer/TimerMSP432.h>
TimerMSP432_Object timerMSP432Objects[MSP_EXP432P401R_TIMERCOUNT];
const TimerMSP432_HWAttrs timerMSP432HWAttrs[MSP_EXP432P401R_TIMERCOUNT] = {
/* Timer32_0 */
{
.timerBaseAddress = TIMER32_0_BASE,
.clockSource = TIMER_A_CLOCKSOURCE_SMCLK,
.intNum = INT_T32_INT1,
.intPriority = ~0
},
{
.timerBaseAddress = TIMER32_1_BASE,
.clockSource = TIMER_A_CLOCKSOURCE_SMCLK,
.intNum = INT_T32_INT2,
.intPriority = ~0
},
/* Timer_A0 */
{
.timerBaseAddress = TIMER_A0_BASE,
.clockSource = TIMER_A_CLOCKSOURCE_ACLK,
.intNum = INT_TA0_N,
.intPriority = ~0
},
/* Timer_A1 */
{
.timerBaseAddress = TIMER_A1_BASE,
.clockSource = TIMER_A_CLOCKSOURCE_ACLK,
.intNum = INT_TA1_0,
.intPriority = ~0
},
/* Timer_A2 */
{
.timerBaseAddress = TIMER_A2_BASE,
.clockSource = TIMER_A_CLOCKSOURCE_ACLK,
.intNum = INT_TA2_0,
.intPriority = ~0
},
/* Timer_A3 */
{
.timerBaseAddress = TIMER_A3_BASE,
.clockSource = TIMER_A_CLOCKSOURCE_ACLK,
.intNum = INT_TA3_0,
.intPriority = ~0
}
};
const Timer_Config Timer_config[MSP_EXP432P401R_TIMERCOUNT] = {
{
.fxnTablePtr = &TimerMSP432_Timer32_fxnTable,
.object = &timerMSP432Objects[MSP_EXP432P401R_TIMER_T32_0],
.hwAttrs = &timerMSP432HWAttrs[MSP_EXP432P401R_TIMER_T32_0]
},
{
.fxnTablePtr = &TimerMSP432_Timer32_fxnTable,
.object = &timerMSP432Objects[MSP_EXP432P401R_TIMER_T32_1],
.hwAttrs = &timerMSP432HWAttrs[MSP_EXP432P401R_TIMER_T32_1]
},
{
.fxnTablePtr = &TimerMSP432_Timer_A_fxnTable,
.object = &timerMSP432Objects[MSP_EXP432P401R_TIMER_TA_0],
.hwAttrs = &timerMSP432HWAttrs[MSP_EXP432P401R_TIMER_TA_0]
},
{
.fxnTablePtr = &TimerMSP432_Timer_A_fxnTable,
.object = &timerMSP432Objects[MSP_EXP432P401R_TIMER_TA_1],
.hwAttrs = &timerMSP432HWAttrs[MSP_EXP432P401R_TIMER_TA_1]
},
{
.fxnTablePtr = &TimerMSP432_Timer_A_fxnTable,
.object = &timerMSP432Objects[MSP_EXP432P401R_TIMER_TA_2],
.hwAttrs = &timerMSP432HWAttrs[MSP_EXP432P401R_TIMER_TA_2]
},
{
.fxnTablePtr = &TimerMSP432_Timer_A_fxnTable,
.object = &timerMSP432Objects[MSP_EXP432P401R_TIMER_TA_3],
.hwAttrs = &timerMSP432HWAttrs[MSP_EXP432P401R_TIMER_TA_3]
}
};
"pwmled.c"
/*
* ======== pwmled.c ========
*/
/* For usleep() */
#include <unistd.h>
#include <stddef.h>
#include <stdbool.h>
/* Driver Header files */
#include <ti/drivers/PWM.h>
#include <ti/drivers/Timer.h>
/* Example/Board Header files */
#include "Board.h"
PWM_Handle pwm1 = NULL;
PWM_Handle pwm2 = NULL;
PWM_Handle pwm3 = NULL;
PWM_Handle pwm4 = NULL;
/* Period and duty in microseconds */
uint32_t pwmPeriod = 5000;
uint32_t duty = 3000;
/* N steps */
uint32_t n = 4096;
/* motor start/stop flag */
bool motorflag = true;
/*******************************************************************************
* LOCAL FUNCTIONS
******************************************************************************/
static void motor_forward(uint32_t value);
static void motor_reversal(uint32_t value);
static void timer0Callback(Timer_Handle myHandle);
/*
* ======== mainThread ========
* Task periodically increments the PWM duty for the on board LED.
*/
void *mainThread(void *arg0)
{
PWM_Params params;
Timer_Params timeparams;
Timer_Handle timer0;
/* Call driver init functions. */
PWM_init();
Timer_init();
PWM_Params_init(¶ms);
params.dutyUnits = PWM_DUTY_US;
params.dutyValue = 0;
params.periodUnits = PWM_PERIOD_US;
params.periodValue = pwmPeriod;
pwm1 = PWM_open(Board_PWM0, ¶ms);
pwm2 = PWM_open(Board_PWM1, ¶ms);
pwm3 = PWM_open(Board_PWM2, ¶ms);
pwm4 = PWM_open(Board_PWM3, ¶ms);
if (pwm1 == NULL) {
/* Board_PWM0 did not open */
while (1);
}
if (pwm2 == NULL) {
/* Board_PWM0 did not open */
while (1);
}
if (pwm3 == NULL) {
/* Board_PWM0 did not open */
while (1);
}
if (pwm4 == NULL) {
/* Board_PWM0 did not open */
while (1);
}
PWM_start(pwm1);
PWM_start(pwm2);
PWM_start(pwm3);
PWM_start(pwm4);
Timer_Params_init(&timeparams);
timeparams.period = 5000000;
timeparams.periodUnits = Timer_PERIOD_US;
timeparams.timerMode = Timer_ONESHOT_CALLBACK;
timeparams.timerCallback = timer0Callback;
timer0 = Timer_open(Board_TIMER2, &timeparams);
if (timer0 == NULL) {
/* Failed to initialized timer */
while (1); 程序会在这里进入死循环,因为Board_TIMER2(Timer_A0)没有打开.
}
Timer_start(timer0);
motor_forward(n);
sleep(1);
motor_reversal(n);
sleep(1);
return NULL;
}
/*Motor forward*/
static void motor_forward(uint32_t value)
{
uint32_t i;
uint8_t j;
uint8_t step;
for(i=value;i>8;i=i-8)
{
if(motorflag == false)
{
i = 0;
break;
}
for(step=0;step<8;step++)
{
if(motorflag == false)
{
break;
}
switch(step)
{
case 0:
/*A*/
PWM_setDuty(pwm1, duty);
usleep(pwmPeriod);
break;
case 1:
/*AB*/
PWM_setDuty(pwm2, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm1, 0);
break;
case 2:
/*B*/
usleep(pwmPeriod);
break;
case 3:
/*BC*/
PWM_setDuty(pwm3, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm2, 0);
break;
case 4:
/*C*/
usleep(pwmPeriod);
break;
case 5:
/*CD*/
PWM_setDuty(pwm4, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm3, 0);
break;
case 6:
/*D*/
usleep(pwmPeriod);
break;
case 7:
/*DA*/
PWM_setDuty(pwm1, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm4, 0);
PWM_setDuty(pwm1, 0);
break;
default:
break;
}
}
}
for(j=0;j<i;j++)
{
if(motorflag == false)
{
break;
}
switch(j)
{
case 0:
/*A*/
PWM_setDuty(pwm1, duty);
usleep(pwmPeriod);
break;
case 1:
/*AB*/
PWM_setDuty(pwm2, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm1, 0);
break;
case 2:
/*B*/
usleep(pwmPeriod);
break;
case 3:
/*BC*/
PWM_setDuty(pwm3, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm2, 0);
break;
case 4:
/*C*/
usleep(pwmPeriod);
break;
case 5:
/*CD*/
PWM_setDuty(pwm4, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm3, 0);
break;
case 6:
/*D*/
usleep(pwmPeriod);
break;
case 7:
/*DA*/
PWM_setDuty(pwm1, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm4, 0);
PWM_setDuty(pwm1, 0);
break;
default:
break;
}
}
PWM_setDuty(pwm1, 0);
PWM_setDuty(pwm2, 0);
PWM_setDuty(pwm3, 0);
PWM_setDuty(pwm4, 0);
}
/*Motor reversal*/
static void motor_reversal(uint32_t value)
{
uint32_t i;
uint8_t j;
uint8_t step;
for(i=value;i>8;i=i-8)
{
if(motorflag == false)
{
i = 0;
break;
}
for(step=0;step<8;step++)
{
if(motorflag == false)
{
break;
}
switch(step)
{
case 0:
/*D*/
PWM_setDuty(pwm4, duty);
usleep(pwmPeriod);
break;
case 1:
/*DC*/
PWM_setDuty(pwm3, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm4, 0);
break;
case 2:
/*C*/
usleep(pwmPeriod);
break;
case 3:
/*CB*/
PWM_setDuty(pwm2, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm3, 0);
break;
case 4:
/*B*/
usleep(pwmPeriod);
break;
case 5:
/*BA*/
PWM_setDuty(pwm1, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm2, 0);
break;
case 6:
/*A*/
usleep(pwmPeriod);
break;
case 7:
/*AD*/
PWM_setDuty(pwm4, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm1, 0);
PWM_setDuty(pwm4, 0);
break;
default:
break;
}
}
}
for(j=0;j<i;j++)
{
if(motorflag == false)
{
break;
}
switch(j)
{
case 0:
/*D*/
PWM_setDuty(pwm4, duty);
usleep(pwmPeriod);
break;
case 1:
/*DC*/
PWM_setDuty(pwm3, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm4, 0);
break;
case 2:
/*C*/
usleep(pwmPeriod);
break;
case 3:
/*CB*/
PWM_setDuty(pwm2, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm3, 0);
break;
case 4:
/*B*/
usleep(pwmPeriod);
break;
case 5:
/*BA*/
PWM_setDuty(pwm1, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm2, 0);
break;
case 6:
/*A*/
usleep(pwmPeriod);
break;
case 7:
/*AD*/
PWM_setDuty(pwm4, duty);
usleep(pwmPeriod);
PWM_setDuty(pwm1, 0);
PWM_setDuty(pwm4, 0);
break;
default:
break;
}
}
PWM_setDuty(pwm1, 0);
PWM_setDuty(pwm2, 0);
PWM_setDuty(pwm3, 0);
PWM_setDuty(pwm4, 0);
}
static void timer0Callback(Timer_Handle myHandle)
{
motorflag = false;
}