//*****************************************************************************
//
// bitband.c - Bit-band manipulation example.
//
// Copyright (c) 2012-2017 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.4.178 of the EK-TM4C123GXL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/fpu.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/rom.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Bit-Banding (bitband)</h1>
//!
//! This example application demonstrates the use of the bit-banding
//! capabilities of the Cortex-M4F microprocessor. All of SRAM and all of the
//! peripherals reside within bit-band regions, meaning that bit-banding
//! operations can be applied to any of them. In this example, a variable in
//! SRAM is set to a particular value one bit at a time using bit-banding
//! operations (it would be more efficient to do a single non-bit-banded write;
//! this simply demonstrates the operation of bit-banding).
//
//*****************************************************************************
//*****************************************************************************
//
// The value that is to be modified via bit-banding.
//
//*****************************************************************************
static volatile uint32_t g_ui32Value;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
while(1)
{
//
// Hang on runtime error.
//
}
}
#endif
//*****************************************************************************
//
// Configure the UART and its pins. This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
// Enable GPIOC
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
while(!(SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOB)));
//
// Enable UART1
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
while(!(SysCtlPeripheralReady(SYSCTL_PERIPH_UART1)));
//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PB0_U1RX);
ROM_GPIOPinConfigure(GPIO_PB1_U1TX);
ROM_GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART1_BASE, UART_CLOCK_PIOSC);
UARTConfigSetExpClk(UART1_BASE,16000000,115200,UART_CONFIG_PAR_NONE|UART_CONFIG_STOP_ONE|UART_CONFIG_WLEN_8);
UARTEnable(UART1_BASE);
}
//*****************************************************************************
//
// This example demonstrates the use of bit-banding to set individual bits
// within a word of SRAM.
//
//*****************************************************************************
int
main(void)
{
//
// Set the clocking to run directly from the crystal.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// Initialize the UART interface.
//
ConfigureUART();
//
// Loop forever.
//
while(1)
{
UARTCharPut(UART1_BASE,0xAA);
}
}