This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GH6PM-UART2



EK-TM4C123GH6PM 設置UART 2 輸出, 無任何輸出,

是那裡設置有錯?

void ConfigureUART(void)
{
// Enable GPIOD
HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTD_BASE + GPIO_O_CR) = 0xFF;

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
while(!(SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOD)));
//
// Enable UART2
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART2);
while(!(SysCtlPeripheralReady(SYSCTL_PERIPH_UART2)));

//
// Configure GPIO Pins for UART mode.
//
GPIOPinConfigure(GPIO_PD6_U2RX);
GPIOPinConfigure(GPIO_PD7_U2TX);
GPIOPinTypeUART(GPIO_PORTD_BASE, GPIO_PIN_6 | GPIO_PIN_7);

//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART2_BASE, UART_CLOCK_PIOSC);
UARTConfigSetExpClk(UART2_BASE,16000000,115200,UART_CONFIG_PAR_NONE|UART_CONFIG_STOP_ONE|UART_CONFIG_WLEN_8);
UARTConfigSetExpClk(UART2_BASE, SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));

UARTEnable(UART2_BASE);
}

//*****************************************************************************
int main(void)
{

ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);

ConfigureUART();

while(1)
{
UARTCharPut(UART2_BASE,0xAA);
}
}