您好:
请问为什么我在使用串口dma接收数据的过程中,定义了4K的一个缓冲区,分为a和b两个区域作为ping-pong区,但是每次都发现dma从a+1024和b+1024的地址开始存数据,而且每1024个字节就进一次中断。谢谢。程序代码如下:
static void usart1_rx_dma_cfg(uint8_t *ping, uint8_t *pong, uint32_t size)
{
ROM_UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);
//enable the uDMA interface for RX channels.
ROM_UARTDMAEnable(UART1_BASE, UART_DMA_RX);
// Put the attributes in a known state for the uDMA UART1RX channel. These
// should already be disabled by default.
ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1RX,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
ping, size);
// Set up the transfer parameters for the UART RX alternate control
// structure. The mode is set to ping-pong, the transfer source is the
// UART data register, and the destination is the receive "B" buffer. The
// transfer size is set to match the size of the buffer.
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
pong, size);
// Now the uDMA UART RX channels are primed to start a
// transfer. As soon as the channels are enabled, the peripheral will
// issue a transfer request and the data transfers will begin.
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1RX);
// Enable the UART DMA RX interrupts.
ROM_UARTIntEnable(UART1_BASE, UART_INT_DMARX);
}
中断函数如下:
uDMAmode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT);
if(uDMAmode == UDMA_MODE_STOP)
{
g_app.dma.buffHalf = 1;
recv_app_code_time_clear();
g_recvState = RECV_CODE;
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
g_app.dma.buff, APP_MDA_BUF_HALF_SIZE);
}
uDMAmode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT);
if(uDMAmode == UDMA_MODE_STOP)
{
g_app.dma.buffFull = 1;
recv_app_code_time_clear();
g_recvState = RECV_CODE;
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
&g_app.dma.buff[APP_MDA_BUF_HALF_SIZE], APP_MDA_BUF_HALF_SIZE);
}
以上程序定义的这个g_app.dma.buff[APP_MDA_BUF_SIZE]是4k的一个缓冲区,
程序里面APP_MDA_BUF_HALF_SIZE = APP_MDA_BUF_SIZE/2即将一个连续的4K缓冲区分为两个2k做ping-pong区。
现出现以下问题:
每次接收数据DMA往缓冲区里面存都是从g_app.dma.buff+1024的地址处和g_app.dma.buff[APP_MDA_BUF_HALF_SIZE+1024]地址处开存1K;
MDA只在以上描述的这两个地址处开始版数据,即MDA每次都是从ping区首地址+1024的内存处开始放数据。pong区也是从首地址+1024的地址开始放数据。且没有数据丢失。
请问这是什么原因造成的。为什么MDA把两个缓冲区的前面1k内存不用。