This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C 串口UDMA中断条件疑问。

//*****************************************************************************
//
// Initializes the UART1 peripheral and sets up the TX and RX uDMA channels.
// The UART is configured for loopback mode so that any data sent on TX will be
// received on RX.  The uDMA channels are configured so that the TX channel
// will copy data from a buffer to the UART TX output.  And the uDMA RX channel
// will receive any incoming data into a pair of buffers in ping-pong mode.
//
//*****************************************************************************
void
InitUART1Transfer(void)
{
    uint_fast16_t ui16Idx;

    //
    // Fill the TX buffer with a simple data pattern.
    //
    for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
    {
        g_ui8TxBuf[ui16Idx] = ui16Idx;
    }

    //
    // Enable the UART peripheral, and configure it to operate even if the CPU
    // is in sleep.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART1);

    //
    // Configure the UART communication parameters.
    //
    ROM_UARTConfigSetExpClk(UART1_BASE, g_ui32SysClock, 115200,
                            UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
                            UART_CONFIG_PAR_NONE);

    //
    // Set both the TX and RX trigger thresholds to 4.  This will be used by
    // the uDMA controller to signal when more data should be transferred.  The
    // uDMA TX and RX channels will be configured so that it can transfer 4
    // bytes in a burst when the UART is ready to transfer more data.
    //
    ROM_UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);

    //
    // Enable the UART for operation, and enable the uDMA interface for both TX
    // and RX channels.
    //
    ROM_UARTEnable(UART1_BASE);
    ROM_UARTDMAEnable(UART1_BASE, UART_DMA_RX | UART_DMA_TX);

    //
    // This register write will set the UART to operate in loopback mode.  Any
    // data sent on the TX output will be received on the RX input.
    //
    HWREG(UART1_BASE + UART_O_CTL) |= UART_CTL_LBE;

    //
    // Put the attributes in a known state for the uDMA UART1RX channel.  These
    // should already be disabled by default.
    //
    ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1RX,
                                    UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    //
    // Configure the control parameters for the primary control structure for
    // the UART RX channel.  The primary contol structure is used for the "A"
    // part of the ping-pong receive.  The transfer data size is 8 bits, the
    // source address does not increment since it will be reading from a
    // register.  The destination address increment is byte 8-bit bytes.  The
    // arbitration size is set to 4 to match the RX FIFO trigger threshold.
    // The uDMA controller will use a 4 byte burst transfer if possible.  This
    // will be somewhat more effecient that single byte transfers.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                              UDMA_ARB_4);

    //
    // Configure the control parameters for the alternate control structure for
    // the UART RX channel.  The alternate contol structure is used for the "B"
    // part of the ping-pong receive.  The configuration is identical to the
    // primary/A control structure.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                              UDMA_ARB_4);

    //
    // Set up the transfer parameters for the UART RX primary control
    // structure.  The mode is set to ping-pong, the transfer source is the
    // UART data register, and the destination is the receive "A" buffer.  The
    // transfer size is set to match the size of the buffer.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
                               UDMA_MODE_PINGPONG,
                               (void *)(UART1_BASE + UART_O_DR),
                               g_ui8RxBufA, sizeof(g_ui8RxBufA));

    //
    // Set up the transfer parameters for the UART RX alternate control
    // structure.  The mode is set to ping-pong, the transfer source is the
    // UART data register, and the destination is the receive "B" buffer.  The
    // transfer size is set to match the size of the buffer.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
                               UDMA_MODE_PINGPONG,
                               (void *)(UART1_BASE + UART_O_DR),
                               g_ui8RxBufB, sizeof(g_ui8RxBufB));

    //
    // Put the attributes in a known state for the uDMA UART1TX channel.  These
    // should already be disabled by default.
    //
    ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1TX,
                                    UDMA_ATTR_ALTSELECT |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    //
    // Set the USEBURST attribute for the uDMA UART TX channel.  This will
    // force the controller to always use a burst when transferring data from
    // the TX buffer to the UART.  This is somewhat more effecient bus usage
    // than the default which allows single or burst transfers.
    //
    ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_UART1TX, UDMA_ATTR_USEBURST);

    //
    // Configure the control parameters for the UART TX.  The uDMA UART TX
    // channel is used to transfer a block of data from a buffer to the UART.
    // The data size is 8 bits.  The source address increment is 8-bit bytes
    // since the data is coming from a buffer.  The destination increment is
    // none since the data is to be written to the UART data register.  The
    // arbitration size is set to 4, which matches the UART TX FIFO trigger
    // threshold.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_8 |
                              UDMA_DST_INC_NONE |
                              UDMA_ARB_4);

    //
    // Set up the transfer parameters for the uDMA UART TX channel.  This will
    // configure the transfer source and destination and the transfer size.
    // Basic mode is used because the peripheral is making the uDMA transfer
    // request.  The source is the TX buffer and the destination is the UART
    // data register.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
                               UDMA_MODE_BASIC, g_ui8TxBuf,
                               (void *)(UART1_BASE + UART_O_DR),
                               sizeof(g_ui8TxBuf));

    //
    // Now both the uDMA UART TX and RX channels are primed to start a
    // transfer.  As soon as the channels are enabled, the peripheral will
    // issue a transfer request and the data transfers will begin.
    //
    ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1RX);
    ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1TX);

    //
    // Enable the UART DMA TX/RX interrupts.
    //
    ROM_UARTIntEnable(UART1_BASE, UART_INT_DMATX | UART_INT_DMATX);

    //
    // Enable the UART peripheral interrupts.
    //
    ROM_IntEnable(INT_UART1);
}

上述代码是TM4C1294芯片官方例程中的代码,例程中使用了串口DMA通信方式。。其中有三个函数的设置涉及到了数据大小,一是ROM_UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);这个函数中设置了UART_FIFO_RX4_8,UART_FIFO_TX4_8,我的理解为当数据量到达串口FIFO的8分之四大小时就会触发中断;二是

ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);这里设置了UDMA_ARB_4,我理解为数据量达到4个字节触发中断;三是

ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
g_ui8RxBufB, sizeof(g_ui8RxBufB));这里利用缓冲区数组大小设置数据量的大小,例程中缓冲区大小为256。

那么这三个函数到底之间有什么关系呢?哪个函数才是真正设置DMA中断触发的条件呢?如果我想接收到13个字节的数据就触发中断,请问这三个函数的参数该如何设置?