MSP432 软件方法怎么实现16位AD
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
给你提供一个参考,你下载后可以看到很多个ADC操作的示例
/*
* -------------------------------------------
* MSP432 DriverLib - v3_21_00_05
* -------------------------------------------
*
* --COPYRIGHT--,BSD,BSD
* Copyright (c) 2016, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
/*******************************************************************************
* MSP432 ADC14 - Single Channel with External Reference
*
* Description: This very simple code example shows the use of an external
* reference for use in the ADC14 module. A single channel sample/conversion
* is setup on input A0 (P5.5) and the sample timer is used to continuously
* store the result in a local variable. The value coming in VREF+ (P5.6) is
* treated as the max value of the ADC and the value coming in VREF- (P5.7) is
* treated as the minimum value.
*
* MSP432P401
* ------------------
* /|\| |
* | | |
* --|RST P5.5 |<---- A0 In
* | P5.6 |<---- VREF+
* | P5.7 |<---- VREF-
* | |
*
* Author: Timothy Logan
******************************************************************************/
/* DriverLib Includes */
#include "driverlib.h"
/* Standard Includes */
#include <stdint.h>
#include <string.h>
volatile uint16_t adcResult;
int main(void)
{
/* Halting WDT */
WDT_A_holdTimer();
Interrupt_enableSleepOnIsrExit();
/* Initializing ADC (MCLK/1/1) */
ADC14_enableModule();
ADC14_initModule(ADC_CLOCKSOURCE_MCLK, ADC_PREDIVIDER_1, ADC_DIVIDER_1,
0);
/* Configuring ADC Memory (ADC_MEM0 A0/A1) in repeat mode
* with use of external references */
ADC14_configureSingleSampleMode(ADC_MEM0, true);
ADC14_configureConversionMemory(ADC_MEM0, ADC_VREFPOS_EXTPOS_VREFNEG_EXTNEG,
ADC_INPUT_A0, false);
/* Setting up GPIO pins as analog inputs (and references) */
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P5,
GPIO_PIN7 | GPIO_PIN6 | GPIO_PIN5 | GPIO_PIN4, GPIO_TERTIARY_MODULE_FUNCTION);
/* Enabling sample timer in auto iteration mode and interrupts*/
ADC14_enableSampleTimer(ADC_AUTOMATIC_ITERATION);
ADC14_enableInterrupt(ADC_INT0);
/* Enabling Interrupts */
Interrupt_enableInterrupt(INT_ADC14);
Interrupt_enableMaster();
/* Triggering the start of the sample */
ADC14_enableConversion();
ADC14_toggleConversionTrigger();
/* Going to sleep */
while (1)
{
PCM_gotoLPM0();
}
}
/* This interrupt happens whenever a conversion has been completed and placed
* into ADC_MEM0. */
void ADC14_IRQHandler(void)
{
uint64_t status;
status = ADC14_getEnabledInterruptStatus();
ADC14_clearInterruptFlag(status);
if(status & ADC_INT0)
{
adcResult = ADC14_getResult(ADC_MEM0);
}
}
建议您看一下相关的APP NOTE: Precision ADC With 16-Bit Performance

给出了相关的测试代码。