请问MSP-GANG如何使用命令控制,我想实现通过命令去控制烧录器烧录,读取烧录成功/失败状态
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您可以看一下

的第3章
The MSP-GANG can be controlled by firmware commands received through USB or its RS-232 serial port.
我看了第三章的介绍,目前我用“Hello”指令是可以访问MSP-GANG的,以及我会如何使用检验码,但是我最主要的控制烧录器烧录指令用不了,文档介绍:不要使用此命令。此命令在固件或信息内存更新期间使用。如果需要使用msp-gang可执行图形用户界面软件来更新固件或信息内存更新。请告诉我怎么样才能使用这个命令呢
3.5.2.7 Load Firmware Command
Tx -> 3E 3A ... ... ... CKL CKH
Rx -> 0x90 (ACK)
Do not use this command. This command is used during firmware or information memory update. Use the MSP-GANG executable GUI software for updating firmware or information memory update if required.
建议您看一下 
您所使用的Load Firmware Command属于3.5.2 Commands Supported by the BOOT Loader。而BOOT Loader的命令主要是用于操作 MSP-GANG 本身的固件firmware的
建议您使用 3.5.3 Commands Supported by Application Firmware
1. Synchronization Sequence (see MSP-GANG User's Guide section 3.3)
TX: 0D
RX: 90 (ACK)
2. Select Image 0 (see MSP-GANG User's Guide section 3.5.3.1) - byte 4 sets the index in the MSP-GANG for the desired image, in this case 0 (the first image in memory)
TX: 3E 50 04 04 00 00 00 00 C5 AB
RX: 90 (ACK)
3. Main Process (see MSP-GANG User's Guide section 3.5.3.2)
TX: 3E 31 04 04 00 00 00 00 C5 CA
RX: B0 (In Progress)
4. Get Progress Status (see MSP-GANG User's Guide section 3.5.2.10)
Poll Get Progress Status command (TX: A5) until byte 6 of the response stops being B0 (In Progress) and becomes 90 (ACK).