近期想在TM4C129上UART3采用dma方式间断性发送数据,对官方例程进行修改后却只能连续发,望各位大佬指教一二
贴上代码
//*****************************************************************************
//
// udma_demo.c - uDMA example.
//
// Copyright (c) 2013-2017 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.4.178 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "driverlib/udma.h"
#include "utils/cpu_usage.h"
#include "utils/uartstdio.h"
#include "utils/ustdlib.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>uDMA (udma_demo)</h1>
//!
//! This example application demonstrates the use of the uDMA controller to
//! transfer data between memory buffers, and to transfer data to and from a
//! UART. The test runs for 10 seconds before exiting.
//!
//! UART0, connected to the ICDI virtual COM port and running at 115,200,
//! 8-N-1, is used to display messages from this application.
//
//*****************************************************************************
//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;
//*****************************************************************************
//
// The number of SysTick ticks per second used for the SysTick interrupt.
//
//*****************************************************************************
#define SYSTICKS_PER_SECOND 100
//*****************************************************************************
//
// The size of the memory transfer source and destination buffers (in words).
//
//*****************************************************************************
#define MEM_BUFFER_SIZE 1024
//*****************************************************************************
//
// The size of the UART transmit and receive buffers. They do not need to be
// the same size.
//
//*****************************************************************************
#define UART_TXBUF_SIZE 10
#define UART_RXBUF_SIZE 10
//*****************************************************************************
//
// The source and destination buffers used for memory transfers.
//
//*****************************************************************************
static uint32_t g_ui32SrcBuf[MEM_BUFFER_SIZE];
static uint32_t g_ui32DstBuf[MEM_BUFFER_SIZE];
//*****************************************************************************
//
// The transmit and receive buffers used for the UART transfers. There is one
// transmit buffer and a pair of recieve ping-pong buffers.
//
//*****************************************************************************
static uint8_t g_ui8TxBuf[UART_TXBUF_SIZE];
static uint8_t g_ui8RxBufA[UART_RXBUF_SIZE];
static uint8_t g_ui8RxBufB[UART_RXBUF_SIZE];
//*****************************************************************************
//
// The count of uDMA errors. This value is incremented by the uDMA error
// handler.
//
//*****************************************************************************
static uint32_t g_ui32uDMAErrCount = 0;
//*****************************************************************************
//
// The count of times the uDMA interrupt occurred but the uDMA transfer was not
// complete. This should remain 0.
//
//*****************************************************************************
static uint32_t g_ui32BadISR = 0;
//*****************************************************************************
//
// The count of UART buffers filled, one for each ping-pong buffer.
//
//*****************************************************************************
static uint32_t g_ui32RxBufACount = 0;
static uint32_t g_ui32RxBufBCount = 0;
//*****************************************************************************
//
// The count of memory uDMA transfer blocks. This value is incremented by the
// uDMA interrupt handler whenever a memory block transfer is completed.
//
//*****************************************************************************
static uint32_t g_ui32MemXferCount = 0;
//*****************************************************************************
//
// The number of seconds elapsed since the start of the program. This value is
// maintained by the SysTick interrupt handler.
//
//*****************************************************************************
static uint32_t g_ui32Seconds = 0;
//*****************************************************************************
//
// The control table used by the uDMA controller. This table must be aligned
// to a 1024 byte boundary.
//
//*****************************************************************************
#if defined(ewarm)
#pragma data_alignment=1024
uint8_t pui8ControlTable[1024];
#elif defined(ccs)
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
#else
uint8_t pui8ControlTable[1024] __attribute__ ((aligned(1024)));
#endif
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// The interrupt handler for the SysTick timer. This handler will increment a
// seconds counter whenever the appropriate number of ticks has occurred. It
// will also call the CPU usage tick function to find the CPU usage percent.
//
//*****************************************************************************
void
SysTickHandler(void)
{
static uint32_t ui32TickCount = 0;
//
// Increment the tick counter.
//
ui32TickCount++;
//
// If the number of ticks per second has occurred, then increment the
// seconds counter.
//
// if(!(ui32TickCount % SYSTICKS_PER_SECOND))
// {
// g_ui32Seconds++;
// }
}
//*****************************************************************************
//
// The interrupt handler for uDMA errors. This interrupt will occur if the
// uDMA encounters a bus error while trying to perform a transfer. This
// handler just increments a counter if an error occurs.
//
//*****************************************************************************
void
uDMAErrorHandler(void)
{
uint32_t ui32Status;
//
// Check for uDMA error bit
//
ui32Status = ROM_uDMAErrorStatusGet();
//
// If there is a uDMA error, then clear the error and increment
// the error counter.
//
if(ui32Status)
{
ROM_uDMAErrorStatusClear();
g_ui32uDMAErrCount++;
}
}
//*****************************************************************************
//
// The interrupt handler for uDMA interrupts from the memory channel. This
// interrupt will increment a counter, and then restart another memory
// transfer.
//
//*****************************************************************************
void
uDMAIntHandler(void)
{
uint32_t ui32Mode,status;
//
// Check for the primary control structure to indicate complete.
//
status = ROM_uDMAIntStatus();
uDMAIntClear(status);
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_SW);
if(ui32Mode == UDMA_MODE_STOP)
{
//
// Configure it for another transfer.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SW, UDMA_MODE_AUTO,
g_ui32SrcBuf, g_ui32DstBuf,
MEM_BUFFER_SIZE);
//
// Initiate another transfer.
//
ROM_uDMAChannelEnable(UDMA_CHANNEL_SW);
ROM_uDMAChannelRequest(UDMA_CHANNEL_SW);
}
}
//*****************************************************************************
//
// The interrupt handler for UART1. This interrupt will occur when a DMA
// transfer is complete using the UART1 uDMA channel. It will also be
// triggered if the peripheral signals an error. This interrupt handler will
// switch between receive ping-pong buffers A and B. It will also restart a TX
// uDMA transfer if the prior transfer is complete. This will keep the UART
// running continuously (looping TX data back to RX).
//
//*****************************************************************************
void
UART3IntHandler(void)
{
uint32_t ui32Status;
uint32_t ui32Mode;
ui32Status = ROM_UARTIntStatus(UART3_BASE, 1);
ROM_UARTIntClear(UART3_BASE, ui32Status);
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CH16_UART3RX | UDMA_PRI_SELECT);
if(ui32Mode == UDMA_MODE_STOP)
{
ROM_uDMAChannelTransferSet(UDMA_CH16_UART3RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART3_BASE + UART_O_DR),
g_ui8RxBufA, sizeof(g_ui8RxBufA));
}
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CH16_UART3RX | UDMA_ALT_SELECT);
if(ui32Mode == UDMA_MODE_STOP)
{
//
// Set up the next transfer for the "B" buffer, using the alternate
// control structure. When the ongoing receive into the "A" buffer is
// done, the uDMA controller will switch back to this one. This
// example re-uses buffer B, but a more sophisticated application could
// use a rotating set of buffers to increase the amount of time that
// the main thread has to process the data in the buffer before it is
// reused.
//
ROM_uDMAChannelTransferSet(UDMA_CH16_UART3RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART3_BASE + UART_O_DR),
g_ui8RxBufA, sizeof(g_ui8RxBufB));////!!!!!!!!!!!!!!!!!!!!!!!
}
ui32Status = ROM_UARTIntStatus(UART3_BASE, 1);
ROM_UARTIntClear(UART3_BASE, ui32Status);
// ROM_UARTIntClear(UART3_BASE, UART_INT_DMATX );
if(!ROM_uDMAChannelIsEnabled(UDMA_CH17_UART3TX))
// if(ROM_UARTIntStatus(UART3_BASE, UART_INT_DMATX))
{
ROM_uDMAChannelTransferSet(UDMA_CH17_UART3TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ui8TxBuf,
(void *)(UART3_BASE + UART_O_DR),
sizeof(g_ui8TxBuf));
ROM_uDMAChannelEnable(UDMA_CH17_UART3TX);
// ui32Status = ROM_UARTIntStatus(UART3_BASE, 1);
// ROM_UARTIntClear(UART3_BASE, ui32Status);
//// ROM_UARTIntClear(UART3_BASE, UART_INT_DMATX );
}
}
void UART3Init(){
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART3);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART3);
GPIOPinConfigure(GPIO_PJ0_U3RX);
GPIOPinConfigure(GPIO_PJ1_U3TX);
ROM_GPIOPinTypeUART(GPIO_PORTJ_BASE,GPIO_PIN_0|GPIO_PIN_1);
ROM_UARTConfigSetExpClk(UART3_BASE, g_ui32SysClock, 115200,
UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE);
ROM_UARTFIFOLevelSet(UART3_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);
ROM_UARTEnable(UART3_BASE);
ROM_UARTDMAEnable(UART3_BASE, UART_DMA_RX | UART_DMA_TX);
// HWREG(UART3_BASE + UART_O_CTL) |= UART_CTL_LBE;
ROM_uDMAChannelAssign(UDMA_CH16_UART3RX);
ROM_uDMAChannelAssign(UDMA_CH17_UART3TX);
//
// Enable the UART DMA TX/RX interrupts.
//
ROM_UARTIntEnable(UART3_BASE, UART_INT_DMATX | UART_INT_DMARX);
//
// Enable the UART peripheral interrupts.
//
ROM_IntEnable(INT_UART3);
}
void uDMA_U3Rx(){
//
// Put the attributes in a known state for the uDMA UART1RX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CH16_UART3RX,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
//
// Configure the control parameters for the primary control structure for
// the UART RX channel. The primary contol structure is used for the "A"
// part of the ping-pong receive. The transfer data size is 8 bits, the
// source address does not increment since it will be reading from a
// register. The destination address increment is byte 8-bit bytes. The
// arbitration size is set to 4 to match the RX FIFO trigger threshold.
// The uDMA controller will use a 4 byte burst transfer if possible. This
// will be somewhat more effecient that single byte transfers.
//
ROM_uDMAChannelControlSet(UDMA_CH16_UART3RX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
//
// Configure the control parameters for the alternate control structure for
// the UART RX channel. The alternate contol structure is used for the "B"
// part of the ping-pong receive. The configuration is identical to the
// primary/A control structure.
//
ROM_uDMAChannelControlSet(UDMA_CH16_UART3RX | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
//
// Set up the transfer parameters for the UART RX primary control
// structure. The mode is set to ping-pong, the transfer source is the
// UART data register, and the destination is the receive "A" buffer. The
// transfer size is set to match the size of the buffer.
//
ROM_uDMAChannelTransferSet(UDMA_CH16_UART3RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,//UDMA_MODE_PINGPONG,UDMA_MODE_BASIC
(void *)(UART3_BASE + UART_O_DR),
g_ui8RxBufA, sizeof(g_ui8RxBufA));
//
// Set up the transfer parameters for the UART RX alternate control
// structure. The mode is set to ping-pong, the transfer source is the
// UART data register, and the destination is the receive "B" buffer. The
// transfer size is set to match the size of the buffer.
//
ROM_uDMAChannelTransferSet(UDMA_CH16_UART3RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART3_BASE + UART_O_DR),
g_ui8RxBufA, sizeof(g_ui8RxBufA));//!!!!!!!!!!!!!!!!!!!
ROM_uDMAChannelEnable(UDMA_CH16_UART3RX);
}
void uDMA_U4Tx(uint32_t size, uint8_t *data){
//
// Put the attributes in a known state for the uDMA UART1TX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CH17_UART3TX,
UDMA_ATTR_ALTSELECT |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
//
// Set the USEBURST attribute for the uDMA UART TX channel. This will
// force the controller to always use a burst when transferring data from
// the TX buffer to the UART. This is somewhat more effecient bus usage
// than the default which allows single or burst transfers.
//
ROM_uDMAChannelAttributeEnable(UDMA_CH17_UART3TX, UDMA_ATTR_USEBURST);
//
// Configure the control parameters for the UART TX. The uDMA UART TX
// channel is used to transfer a block of data from a buffer to the UART.
// The data size is 8 bits. The source address increment is 8-bit bytes
// since the data is coming from a buffer. The destination increment is
// none since the data is to be written to the UART data register. The
// arbitration size is set to 4, which matches the UART TX FIFO trigger
// threshold.
//
ROM_uDMAChannelControlSet(UDMA_CH17_UART3TX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 |
UDMA_DST_INC_NONE |
UDMA_ARB_4);
//
// Set up the transfer parameters for the uDMA UART TX channel. This will
// configure the transfer source and destination and the transfer size.
// Basic mode is used because the peripheral is making the uDMA transfer
// request. The source is the TX buffer and the destination is the UART
// data register.
//
ROM_uDMAChannelTransferSet(UDMA_CH17_UART3TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, data,
(void *)(UART3_BASE + UART_O_DR),
size);
//
// Now both the uDMA UART TX and RX channels are primed to start a
// transfer. As soon as the channels are enabled, the peripheral will
// issue a transfer request and the data transfers will begin.
//
ROM_uDMAChannelEnable(UDMA_CH17_UART3TX);
}
//*****************************************************************************
//
// Initializes the UART1 peripheral and sets up the TX and RX uDMA channels.
// The UART is configured for loopback mode so that any data sent on TX will be
// received on RX. The uDMA channels are configured so that the TX channel
// will copy data from a buffer to the UART TX output. And the uDMA RX channel
// will receive any incoming data into a pair of buffers in ping-pong mode.
//
//*****************************************************************************
void
InitUART4Transfer(void)
{
UART3Init();
uDMA_U3Rx();
uDMA_U4Tx(sizeof(g_ui8TxBuf),g_ui8TxBuf);
}
//*****************************************************************************
//
// Initializes the uDMA software channel to perform a memory to memory uDMA
// transfer.
//
//*****************************************************************************
void
InitSWTransfer(void)
{
// uint_fast16_t ui16Idx;
//
// Enable interrupts from the uDMA software channel.
//
ROM_IntEnable(INT_UDMA);
//
// Put the attributes in a known state for the uDMA software channel.
// These should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_SW,
UDMA_ATTR_USEBURST | UDMA_ATTR_ALTSELECT |
(UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK));
//
// Configure the control parameters for the SW channel. The SW channel
// will be used to transfer between two memory buffers, 32 bits at a time.
// Therefore the data size is 32 bits, and the address increment is 32 bits
// for both source and destination. The arbitration size will be set to 8,
// which causes the uDMA controller to rearbitrate after 8 items are
// transferred. This keeps this channel from hogging the uDMA controller
// once the transfer is started, and allows other channels cycles if they
// are higher priority.
//
ROM_uDMAChannelControlSet(UDMA_CHANNEL_SW | UDMA_PRI_SELECT,
UDMA_SIZE_32 | UDMA_SRC_INC_32 | UDMA_DST_INC_32 |
UDMA_ARB_8);
//
// Set up the transfer parameters for the software channel. This will
// configure the transfer buffers and the transfer size. Auto mode must be
// used for software transfers.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SW | UDMA_PRI_SELECT,
UDMA_MODE_AUTO, g_ui32SrcBuf, g_ui32DstBuf,
MEM_BUFFER_SIZE);
//
// Now the software channel is primed to start a transfer. The channel
// must be enabled. For software based transfers, a request must be
// issued. After this, the uDMA memory transfer begins.
//
ROM_uDMAChannelEnable(UDMA_CHANNEL_SW);
ROM_uDMAChannelRequest(UDMA_CHANNEL_SW);
}
void uDMA_Init(){
//
// Enable the uDMA controller at the system level. Enable it to continue
// to run while the processor is in sleep.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
//
// Enable the uDMA controller error interrupt. This interrupt will occur
// if there is a bus error during a transfer.
//
ROM_IntEnable(INT_UDMAERR);
//
// Enable the uDMA controller.
//
ROM_uDMAEnable();
//
// Point at the control table to use for channel control structures.
//
ROM_uDMAControlBaseSet(pui8ControlTable);
}
void delay_s(int s) {
ROM_SysCtlDelay((g_ui32SysClock / (3 )) * s); // more accurate
}
//*****************************************************************************
//
// This example demonstrates how to use the uDMA controller to transfer data
// between memory buffers and to and from a peripheral, in this case a UART.
// The uDMA controller is configured to repeatedly transfer a block of data
// from one memory buffer to another. It is also set up to repeatedly copy a
// block of data from a buffer to the UART output. The UART data is looped
// back so the same data is received, and the uDMA controlled is configured to
// continuously receive the UART data using ping-pong buffers.
//
// The processor is put to sleep when it is not doing anything, and this allows
// collection of CPU usage data to see how much CPU is being used while the
// data transfers are ongoing.
//
//*****************************************************************************
int
main(void)
{
//
// Set the clocking to run directly from the crystal at 120MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
uDMA_Init();
//
// Initialize the uDMA memory to memory transfers.
//
InitSWTransfer();
//
// Initialize the uDMA UART transfers.
//
// InitUART4Transfer();
UART3Init();
uDMA_U3Rx();
uDMA_U4Tx(sizeof(g_ui8TxBuf),g_ui8TxBuf);
//
// Loop until the button is pressed. The processor is put to sleep
// in this loop so that CPU utilization can be measured.
//
while(1)
{
uint_fast16_t ui16Idx;
//
// Fill the TX buffer with a simple data pattern.
//
for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
{
g_ui8TxBuf[ui16Idx] = ui16Idx;
}
delay_s(10);
for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
{
g_ui8TxBuf[ui16Idx] = 0x70;
}
delay_s(10);
for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
{
g_ui8TxBuf[ui16Idx] = 0x71;
}
delay_s(10);
}
}