Other Parts Discussed in Thread: CONTROLSUITE
dsp28335使用EPWM1触发ADC采集数据,请问还需要对EPWM1单独配置吗,只是像图片中配置是不是就行了?不需要再单独配置EPWM吧?请各位帮帮忙,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE
dsp28335使用EPWM1触发ADC采集数据,请问还需要对EPWM1单独配置吗,只是像图片中配置是不是就行了?不需要再单独配置EPWM吧?请各位帮帮忙,谢谢
您可以参考一下例程内的配置
C:\ti\controlSUITE\device_support\f2833x\v142\DSP2823x_examples_ccsv5
如下
//########################################################################### // Description: //! \addtogroup f2823x_example_list //! <h1>ePWM Action Qualifier Module using Upcount mode (epwm_up_aq)</h1> //! //! This example configures ePWM1, ePWM2, ePWM3 to produce a waveform with //! independent modulation on EPWMxA and EPWMxB. The compare values CMPA //! and CMPB are modified within the ePWM's ISR. The TB counter is in upmode. //! //! Monitor the ePWM1 - ePWM3 pins on an oscilloscope. //! //! \b External \b Connections \n //! - EPWM1A is on GPIO0 //! - EPWM1B is on GPIO1 //! - EPWM2A is on GPIO2 //! - EPWM2B is on GPIO3 //! - EPWM3A is on GPIO4 //! - EPWM3B is on GPIO5 // //########################################################################### // $TI Release: F2833x/F2823x Header Files and Peripheral Examples V142 $ // $Release Date: November 1, 2016 $ // $Copyright: Copyright (C) 2007-2016 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File typedef struct { volatile struct EPWM_REGS *EPwmRegHandle; Uint16 EPwm_CMPA_Direction; Uint16 EPwm_CMPB_Direction; Uint16 EPwmTimerIntCount; Uint16 EPwmMaxCMPA; Uint16 EPwmMinCMPA; Uint16 EPwmMaxCMPB; Uint16 EPwmMinCMPB; }EPWM_INFO; // Prototype statements for functions found within this file. void InitEPwm1Example(void); void InitEPwm2Example(void); void InitEPwm3Example(void); __interrupt void epwm1_isr(void); __interrupt void epwm2_isr(void); __interrupt void epwm3_isr(void); void update_compare(EPWM_INFO*); // Global variables used in this example EPWM_INFO epwm1_info; EPWM_INFO epwm2_info; EPWM_INFO epwm3_info; // Configure the period for each timer #define EPWM1_TIMER_TBPRD 2000 // Period register #define EPWM1_MAX_CMPA 1950 #define EPWM1_MIN_CMPA 50 #define EPWM1_MAX_CMPB 1950 #define EPWM1_MIN_CMPB 50 #define EPWM2_TIMER_TBPRD 2000 // Period register #define EPWM2_MAX_CMPA 1950 #define EPWM2_MIN_CMPA 50 #define EPWM2_MAX_CMPB 1950 #define EPWM2_MIN_CMPB 50 #define EPWM3_TIMER_TBPRD 2000 // Period register #define EPWM3_MAX_CMPA 950 #define EPWM3_MIN_CMPA 50 #define EPWM3_MAX_CMPB 1950 #define EPWM3_MIN_CMPB 1050 // To keep track of which way the compare value is moving #define EPWM_CMP_UP 1 #define EPWM_CMP_DOWN 0 void main(void) { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initialize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // For this case just init GPIO pins for ePWM1, ePWM2, ePWM3 // These functions are in the DSP2833x_EPwm.c file InitEPwm1Gpio(); InitEPwm2Gpio(); InitEPwm3Gpio(); // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.EPWM1_INT = &epwm1_isr; PieVectTable.EPWM2_INT = &epwm2_isr; PieVectTable.EPWM3_INT = &epwm3_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); // Not required for this example // For this example, only initialize the ePWM EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; InitEPwm1Example(); InitEPwm2Example(); InitEPwm3Example(); EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; EDIS; // Step 5. User specific code, enable interrupts: // Enable CPU INT3 which is connected to EPWM1-3 INT: IER |= M_INT3; // Enable EPWM INTn in the PIE: Group 3 interrupt 1-3 PieCtrlRegs.PIEIER3.bit.INTx1 = 1; PieCtrlRegs.PIEIER3.bit.INTx2 = 1; PieCtrlRegs.PIEIER3.bit.INTx3 = 1; // Enable global Interrupts and higher priority real-time debug events: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // Step 6. IDLE loop. Just sit and loop forever (optional): for(;;) { __asm(" NOP"); } } __interrupt void epwm1_isr(void) { // Update the CMPA and CMPB values update_compare(&epwm1_info); // Clear INT flag for this timer EPwm1Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } __interrupt void epwm2_isr(void) { // Update the CMPA and CMPB values update_compare(&epwm2_info); // Clear INT flag for this timer EPwm2Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } __interrupt void epwm3_isr(void) { // Update the CMPA and CMPB values update_compare(&epwm3_info); // Clear INT flag for this timer EPwm3Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } void InitEPwm1Example() { // Setup TBCLK EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm1Regs.TBPRD = EPWM1_TIMER_TBPRD; // Set timer period EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0 EPwm1Regs.TBCTR = 0x0000; // Clear counter EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV2; // Clock ratio to SYSCLKOUT EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV2; // Setup shadow register load on ZERO EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Set Compare values EPwm1Regs.CMPA.half.CMPA = EPWM1_MIN_CMPA; // Set compare A value EPwm1Regs.CMPB = EPWM1_MIN_CMPB; // Set Compare B value // Set actions EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // Set PWM1A on Zero EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Clear PWM1A on event A, up count EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET; // Set PWM1B on Zero EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Clear PWM1B on event B, up count // Interrupt where we will change the Compare Values EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable INT EPwm1Regs.ETPS.bit.INTPRD = ET_3RD; // Generate INT on 3rd event // Information this example uses to keep track // of the direction the CMPA/CMPB values are // moving, the min and max allowed values and // a pointer to the correct ePWM registers epwm1_info.EPwm_CMPA_Direction = EPWM_CMP_UP; // Start by increasing CMPA & CMPB epwm1_info.EPwm_CMPB_Direction = EPWM_CMP_UP; epwm1_info.EPwmTimerIntCount = 0; // Zero the interrupt counter epwm1_info.EPwmRegHandle = &EPwm1Regs; // Set the pointer to the ePWM module epwm1_info.EPwmMaxCMPA = EPWM1_MAX_CMPA; // Setup min/max CMPA/CMPB values epwm1_info.EPwmMinCMPA = EPWM1_MIN_CMPA; epwm1_info.EPwmMaxCMPB = EPWM1_MAX_CMPB; epwm1_info.EPwmMinCMPB = EPWM1_MIN_CMPB; } void InitEPwm2Example() { // Setup TBCLK EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm2Regs.TBPRD = EPWM2_TIMER_TBPRD; // Set timer period EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading EPwm2Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0 EPwm2Regs.TBCTR = 0x0000; // Clear counter EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV2; // Clock ratio to SYSCLKOUT EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV2; // Setup shadow register load on ZERO EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Set Compare values EPwm2Regs.CMPA.half.CMPA = EPWM2_MIN_CMPA; // Set compare A value EPwm2Regs.CMPB = EPWM2_MAX_CMPB; // Set Compare B value // Set actions EPwm2Regs.AQCTLA.bit.PRD = AQ_CLEAR; // Clear PWM2A on Period EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM2A on event A, up count EPwm2Regs.AQCTLB.bit.PRD = AQ_CLEAR; // Clear PWM2B on Period EPwm2Regs.AQCTLB.bit.CBU = AQ_SET; // Set PWM2B on event B, up count // Interrupt where we will change the Compare Values EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event EPwm2Regs.ETSEL.bit.INTEN = 1; // Enable INT EPwm2Regs.ETPS.bit.INTPRD = ET_3RD; // Generate INT on 3rd event // Information this example uses to keep track // of the direction the CMPA/CMPB values are // moving, the min and max allowed values and // a pointer to the correct ePWM registers epwm2_info.EPwm_CMPA_Direction = EPWM_CMP_UP; // Start by increasing CMPA epwm2_info.EPwm_CMPB_Direction = EPWM_CMP_DOWN; // and decreasing CMPB epwm2_info.EPwmTimerIntCount = 0; // Zero the interrupt counter epwm2_info.EPwmRegHandle = &EPwm2Regs; // Set the pointer to the ePWM module epwm2_info.EPwmMaxCMPA = EPWM2_MAX_CMPA; // Setup min/max CMPA/CMPB values epwm2_info.EPwmMinCMPA = EPWM2_MIN_CMPA; epwm2_info.EPwmMaxCMPB = EPWM2_MAX_CMPB; epwm2_info.EPwmMinCMPB = EPWM2_MIN_CMPB; } void InitEPwm3Example(void) { // Setup TBCLK EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm3Regs.TBPRD = EPWM3_TIMER_TBPRD; // Set timer period EPwm3Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading EPwm3Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0 EPwm3Regs.TBCTR = 0x0000; // Clear counter EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1; // Setup shadow register load on ZERO EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Set Compare values EPwm3Regs.CMPA.half.CMPA = EPWM3_MIN_CMPA; // Set compare A value EPwm3Regs.CMPB = EPWM3_MAX_CMPB; // Set Compare B value // Set Actions EPwm3Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM3A on event B, up count EPwm3Regs.AQCTLA.bit.CBU = AQ_CLEAR; // Clear PWM3A on event B, up count EPwm3Regs.AQCTLB.bit.ZRO = AQ_TOGGLE; // Toggle EPWM3B on Zero // Interrupt where we will change the Compare Values EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event EPwm3Regs.ETSEL.bit.INTEN = 1; // Enable INT EPwm3Regs.ETPS.bit.INTPRD = ET_3RD; // Generate INT on 3rd event // Start by increasing the compare A and decreasing compare B epwm3_info.EPwm_CMPA_Direction = EPWM_CMP_UP; epwm3_info.EPwm_CMPB_Direction = EPWM_CMP_DOWN; // Start the count at 0 epwm3_info.EPwmTimerIntCount = 0; epwm3_info.EPwmRegHandle = &EPwm3Regs; epwm3_info.EPwmMaxCMPA = EPWM3_MAX_CMPA; epwm3_info.EPwmMinCMPA = EPWM3_MIN_CMPA; epwm3_info.EPwmMaxCMPB = EPWM3_MAX_CMPB; epwm3_info.EPwmMinCMPB = EPWM3_MIN_CMPB; } void update_compare(EPWM_INFO *epwm_info) { // Every 10'th interrupt, change the CMPA/CMPB values if(epwm_info->EPwmTimerIntCount == 10) { epwm_info->EPwmTimerIntCount = 0; // If we were increasing CMPA, check to see if // we reached the max value. If not, increase CMPA // else, change directions and decrease CMPA if(epwm_info->EPwm_CMPA_Direction == EPWM_CMP_UP) { if(epwm_info->EPwmRegHandle->CMPA.half.CMPA < epwm_info->EPwmMaxCMPA) { epwm_info->EPwmRegHandle->CMPA.half.CMPA++; } else { epwm_info->EPwm_CMPA_Direction = EPWM_CMP_DOWN; epwm_info->EPwmRegHandle->CMPA.half.CMPA--; } } // If we were decreasing CMPA, check to see if // we reached the min value. If not, decrease CMPA // else, change directions and increase CMPA else { if(epwm_info->EPwmRegHandle->CMPA.half.CMPA == epwm_info->EPwmMinCMPA) { epwm_info->EPwm_CMPA_Direction = EPWM_CMP_UP; epwm_info->EPwmRegHandle->CMPA.half.CMPA++; } else { epwm_info->EPwmRegHandle->CMPA.half.CMPA--; } } // If we were increasing CMPB, check to see if // we reached the max value. If not, increase CMPB // else, change directions and decrease CMPB if(epwm_info->EPwm_CMPB_Direction == EPWM_CMP_UP) { if(epwm_info->EPwmRegHandle->CMPB < epwm_info->EPwmMaxCMPB) { epwm_info->EPwmRegHandle->CMPB++; } else { epwm_info->EPwm_CMPB_Direction = EPWM_CMP_DOWN; epwm_info->EPwmRegHandle->CMPB--; } } // If we were decreasing CMPB, check to see if // we reached the min value. If not, decrease CMPB // else, change directions and increase CMPB else { if(epwm_info->EPwmRegHandle->CMPB == epwm_info->EPwmMinCMPB) { epwm_info->EPwm_CMPB_Direction = EPWM_CMP_UP; epwm_info->EPwmRegHandle->CMPB++; } else { epwm_info->EPwmRegHandle->CMPB--; } } } else { epwm_info->EPwmTimerIntCount++; } return; } //=========================================================================== // No more. //===========================================================================