This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问想驱动蜂鸣器发出声音,通过DAC这么写可不可以呢?



#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_ssi.h"
#include "inc/hw_types.h"
#include "driverlib/ssi.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"

#define NUM_SSI_DATA 8
const uint8_t pui8DataTx[NUM_SSI_DATA] =
{0xFF, 0xF8, 0xF8, 0x88, 0x01, 0x1F, 0x1F, 0x01};
int main(void)
{
    uint32_t ui32Index;
    uint32_t ui32Data;
        SysCtlClockSet(SYSCTL_SYSDIV_4|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
        GPIOPinConfigure(GPIO_PD3_SSI1TX);
        GPIOPinConfigure(GPIO_PD0_SSI1CLK);
        //复用为外设引脚;
        GPIOPinTypeSSI(GPIO_PORTD_BASE,GPIO_PIN_3);
        GPIOPinTypeSSI(GPIO_PORTD_BASE,GPIO_PIN_0);
        //设置为SSI功能
        SSIConfigSetExpClk(SSI1_BASE,SysCtlClockGet(),SSI_FRF_MOTO_MODE_1,SSI_MODE_MASTER,1000000,16);
        //配置SSI1
        SSIEnable(SSI1_BASE);
        GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1,0);
        SSIDataPut(SSI1_BASE,0xFFF);
        while(SSIBusy(SSI1_BASE))
        {
            for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
                   {
                       ui32Data = pui8DataTx[ui32Index];
                       SSIDataPut(SSI0_BASE, ui32Data);
                       while(SSIBusy(SSI0_BASE))
                       {
                       }
                       SysCtlDelay(40000000);
                   }
        }
}