This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

想通过I2C读取温度传感器的值,并显示在LCD上,温度传感器是TMP75,不知道是哪里的问题

Other Parts Discussed in Thread: TMP100

/*
 * main.c
 */
#include <stdbool.h>
#include <stdint.h>
#include <string.h>
#include "driverlib/i2c.h"
#include "inc/hw_memmap.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/ssi.h"
#include "lcddriver/uc1701.h"
#define TMP_I2C_ADDR 0b1001000
#define TMP_TEMP_REG 0x01
#define TMP_PIN_I2C_PORT I2C1_BASE
uint16_t TMP100DataRead(void);
int main(void)
{
    SysCtlClockSet(SYSCTL_SYSDIV_1|SYSCTL_USE_OSC|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C1);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    //
    GPIOPinConfigure(GPIO_PA6_I2C1SCL);
    GPIOPinConfigure(GPIO_PA7_I2C1SDA);
    //
    GPIOPinTypeGPIOOutputOD(GPIO_PORTA_BASE,GPIO_PIN_6|GPIO_PIN_7);
    GPIOPinTypeI2C(GPIO_PORTA_BASE,GPIO_PIN_6|GPIO_PIN_7);
    UC1701Init(60000);
    UC1701Clear();
    UC1701CharDispaly(0, 0, "the temp is:");
    UC1701DisplayN(1,0,TMP100DataRead());
    SysCtlDelay(1000000);
    while(1)
    {
    }
}
/读这部分是/实验指导书上的程序
uint16_t TMP100DataRead(void)
{
    uint8_t i2cWriteBuffer;
    uint32_t i2cReadBuffer[2];
    uint16_t temp_value;
    // send to tmp100:
    i2cWriteBuffer = TMP_TEMP_REG;
    i2cWriteBuffer &= 0x03; // 2 bit valid
    // frame 1:
    I2CMasterSlaveAddrSet(TMP_PIN_I2C_PORT, TMP_I2C_ADDR, false);
    // frame 2:
    I2CMasterDataPut(TMP_PIN_I2C_PORT, i2cWriteBuffer);
    I2CMasterControl(TMP_PIN_I2C_PORT, I2C_MASTER_CMD_SINGLE_SEND);
    // wait finish
    while(I2CMasterBusBusy(TMP_PIN_I2C_PORT))
        ;
    // read from tmp100:
    // frame 3:
    I2CMasterSlaveAddrSet(TMP_PIN_I2C_PORT, TMP_I2C_ADDR, true);
    //I2CMasterControl(TMP_PIN_I2C_PORT, I2C_MASTER_CMD_SINGLE_RECEIVE);
    I2CMasterControl(TMP_PIN_I2C_PORT, I2C_MASTER_CMD_BURST_RECEIVE_START);
    // get temperature int value
    // frame 4:
    i2cReadBuffer[0] = I2CMasterDataGet(TMP_PIN_I2C_PORT);
    int a = 500;
    while (a--)
        ;
    I2CMasterControl(TMP_PIN_I2C_PORT, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
    // get the decimal value
    // frame 5:
    i2cReadBuffer[1] = I2CMasterDataGet(TMP_PIN_I2C_PORT);
    // while(I2CMasterBusBusy(TMP_PIN_I2C_PORT))
    // ;
    I2CMasterControl(TMP_PIN_I2C_PORT, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
    temp_value = i2cReadBuffer[0] | (i2cReadBuffer[1] << 8);
    return temp_value;
}