This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB连接无法识别



把USB虚拟串口的官方例程烧进TM4C123的开发板里没有问题 但是烧进我自己做的板子里就无法识别

自己做的板子供电和晶振工作都正常 引脚连接也正确 SWD也能识别 但插上USB就是无法识别

硬件连接就是PD4接DM PD5接DP吧 我给DP加1.5K上拉电阻也没用

microUSB的接头封装也肯定是对的 以前用CH340做TTL转USB也没有问题

想请教一下工程师们可能出现什么情况

  • //*****************************************************************************
    //
    // Note:
    //
    // This example is intended to run on Tiva C Series evaluation kit hardware
    // where the UARTs are wired solely for TX and RX, and do not have GPIOs
    // connected to act as handshake signals.  As a result, this example mimics
    // the case where communication is always possible.  It reports DSR, DCD
    // and CTS as high to ensure that the USB host recognizes that data can be
    // sent and merely ignores the host's requested DTR and RTS states.  "TODO"
    // comments in the code indicate where code would be required to add support
    // for real handshakes.
    //
    //*****************************************************************************

    这个示例就是写给官方开发板的,UART仅为TX和RX连接,没有GPIO连接以充当握手信号。

    "TODO"
    // comments in the code indicate where code would be required to add support
    // for real handshakes.
  • 你烧的是哪个历程呢?
  • 官方的usb_dev_serial
  • 我是用USB做虚拟串口 连线都跟开发板一样 开发板例程也没有GPIO握手信号