Other Parts Discussed in Thread: TM4C123GH6PM
用TM4C123GH6PM对MPU9150进行控制和数据读取,用官方给的例程和sensorlib库,所用软件为CCS 8.3.0 。程序运行正常,数据读取正常,数据输出结果正常。
但在mpu9150.c文件中增加断点都是无效的。具体程序分两个部分贴出:
一、main.c中部分程序,对MPU9150进行设置
void MPU9150CFG(void) { // Initialize the MPU9150 Driver. MPU9150Init(&g_sMPU9150Inst, &g_sI2CInst, MPU9150_I2C_ADDRESS, I2C3Callback, &g_sMPU9150Inst); I2C3Wait(__FILE__, __LINE__); // Write application specifice sensor configuration such as filter settings // and sensor range settings. g_sMPU9150Inst.pui8Data[0] = MPU9150_CONFIG_DLPF_CFG_94_98; g_sMPU9150Inst.pui8Data[1] = MPU9150_GYRO_CONFIG_FS_SEL_250; g_sMPU9150Inst.pui8Data[2] = (MPU9150_ACCEL_CONFIG_ACCEL_HPF_5HZ | MPU9150_ACCEL_CONFIG_AFS_SEL_2G); MPU9150Write(&g_sMPU9150Inst, MPU9150_O_CONFIG, g_sMPU9150Inst.pui8Data, 3, I2C3Callback, &g_sMPU9150Inst); I2C3Wait(__FILE__, __LINE__); // Configure the data ready interrupt pin output of the MPU9150. g_sMPU9150Inst.pui8Data[0] = MPU9150_INT_PIN_CFG_INT_LEVEL | MPU9150_INT_PIN_CFG_INT_RD_CLEAR | MPU9150_INT_PIN_CFG_LATCH_INT_EN; g_sMPU9150Inst.pui8Data[1] = MPU9150_INT_ENABLE_DATA_RDY_EN; MPU9150Write(&g_sMPU9150Inst, MPU9150_O_INT_PIN_CFG, g_sMPU9150Inst.pui8Data, 2, I2C3Callback, &g_sMPU9150Inst); // Wait for transaction to complete I2C3Wait(__FILE__, __LINE__); // Initialize the DCM system. 50 hz sample rate. // accel weight = .2, gyro weight = .8, mag weight = .2 }
二、mpu9150.c中部分程序,主要对MPU9150进行初始化,MPU9150的初始化函数为 MPU9150Init()
//*****************************************************************************
//
//! Initializes the MPU9150 driver.
//!
//! \param psInst is a pointer to the MPU9150 instance data.
//! \param psI2CInst is a pointer to the I2C master driver instance data.
//! \param ui8I2CAddr is the I2C address of the MPU9150 device.
//! \param pfnCallback is the function to be called when the initialization has
//! completed (can be \b NULL if a callback is not required).
//! \param pvCallbackData is a pointer that is passed to the callback function.
//!
//! This function initializes the MPU9150 driver, preparing it for operation.
//!
//! \return Returns 1 if the MPU9150 driver was successfully initialized and 0
//! if it was not.
//
//*****************************************************************************
uint_fast8_t
MPU9150Init(tMPU9150 *psInst, tI2CMInstance *psI2CInst,
uint_fast8_t ui8I2CAddr, tSensorCallback *pfnCallback,
void *pvCallbackData)
{
//
// Initialize the MPU9150 instance structure.
//
psInst->psI2CInst = psI2CInst;
psInst->ui8Addr = ui8I2CAddr;
//
// Save the callback information.
//
psInst->pfnCallback = pfnCallback;
psInst->pvCallbackData = pvCallbackData;
//
// Default range setting is +/- 2 g
//
psInst->ui8AccelAfsSel = (MPU9150_ACCEL_CONFIG_AFS_SEL_2G >>
MPU9150_ACCEL_CONFIG_AFS_SEL_S);
psInst->ui8NewAccelAfsSel = (MPU9150_ACCEL_CONFIG_AFS_SEL_2G >>
MPU9150_ACCEL_CONFIG_AFS_SEL_S);
//
// Default range setting is +/- 250 degrees/s
//
psInst->ui8GyroFsSel = (MPU9150_GYRO_CONFIG_FS_SEL_250 >>
MPU9150_GYRO_CONFIG_FS_SEL_S);
psInst->ui8NewGyroFsSel = (MPU9150_GYRO_CONFIG_FS_SEL_250 >>
MPU9150_GYRO_CONFIG_FS_SEL_S);
//
// Set the state to show we are initiating a reset.
//
psInst->ui8State = MPU9150_STATE_INIT_RESET;
//
// Load the buffer with command to perform device reset
//
psInst->uCommand.pui8Buffer[0] = MPU9150_O_PWR_MGMT_1;
psInst->uCommand.pui8Buffer[1] = MPU9150_PWR_MGMT_1_DEVICE_RESET;
if(I2CMWrite(psInst->psI2CInst, psInst->ui8Addr,
psInst->uCommand.pui8Buffer, 2, MPU9150Callback, psInst) == 0)
{
psInst->ui8State = MPU9150_STATE_IDLE;
return(0);
}
//
// Success
//
return(1);
}
程序在进入MPU9150CFG函数,首先对MPU9150进行初始化,因此程序会跳入mpu9150.c 文件中执行 MPU9150Init()。但我在 MPU9150Init()中设置断点的时候,断点都是无效的,断点显示为灰色,且有感叹号,并且会出现以下字符:“[ S/W BP - disabled ]” 请问这是为什么,这问题已经卡了一周了,请帮帮我。