This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tm4c123gh6pm的Uart例程中UARTLoopbackEnable请问在哪里呢?

  • 1.在.lib库中有的

    2.C:\ti\TivaWare_C_Series-2.1.4.178\driverlib下的uart.c中也是有原型的,原型函数如下所示:

    //*****************************************************************************
    //
    //! Enables internal loopback mode for a UART port
    //!
    //! \param ui32Base is the base address of the UART port.
    //!
    //! This function configures a UART port in internal loopback mode to help with
    //! diagnostics and debug.  In this mode, the transmit and receive terminals of
    //! the same UART port are internally connected.  Hence, the data transmitted
    //! on the UnTx output is received on the UxRx input, without having to go
    //! through I/O's.  UARTCharPut(), UARTCharGet() functions can be used along 
    //! with this function.
    //!
    //! \return None.
    //
    //*****************************************************************************
    void UARTLoopbackEnable(uint32_t ui32Base)
    {
        //
        // Check the arguments.
        //
        ASSERT(_UARTBaseValid(ui32Base));
    
        //
        // Write the Loopback Enable bit to register.
        //
        HWREG(ui32Base + UART_O_CTL) |= UART_CTL_LBE;
    }
    

    3.楼主你的图片挂了,图片需要以附件方式上传,不能直接粘贴的。

  • 谢谢楼上的回答

    另外您也可以在 TI Resource Explorer 内查看

    http://dev.ti.com/tirex/explore/node?node=AG7Ca9JTFbbddKCFBzVSOQ__mic1X5.__LATEST