This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
很荣幸在21IC论坛活动中获得一块MSP432P401R LanchPad。拿到开发板后,先搭建开发环境,MSP432P401R可在CCS、KEIL、IAR 3个IDE平台都可开发,这里选择了比较熟悉的KEIL。并对MSP432P401R的SDK进行熟悉。
刚好手头有一块带6轴LSM6DSO传感器的板子和一块0.96寸的OLED屏,两个都可通过I2C进行通讯。LSM6DSO传感器自带计步功能,既通过中断通知计步事件,也可以通过读取对应的寄存器获得。那就做一个计步功能,来测试MSP432P401R的I2C功能。
下图是I2C的框架图
MSP432P401R的I2C模块包括下列功能:
7位和10位设备寻址模式
启动、重启和停止
多主发射机/接收机模式
从接收机/发射机模式
支持高达100 Kbps的标准模式、高达400 Kbps的快速模式和高达1 Mbps的快速模式
主模式下可编程UCXCLK频率
专为低功耗设计
具有中断能力和自动停止断言的8位字节计数器
多达四个硬件从地址,每个都有自己的中断和DMA触发器
从机地址和地址接收中断的屏蔽寄存器
时钟低超时中断,以避免总线暂停
I2C模块的功能非常丰富。此次评测只使用I2C的基本功能。
硬件连接为SCL -- P1.7,SDA -- P1.6,gpio中断 -- P5.0。
/* DriverLib Includes */ #include <ti/devices/msp432p4xx/driverlib/driverlib.h> /* Standard Includes */ #include <stdint.h> #include <stdbool.h> #include "i2c_driver.h" #include "oled_i2c.h" #include "Lsm6dso.h" #define system_jump_time 1000 // 1/system_jump_time = 1ms /* Slave Address for I2C Slave */ #define SLAVE_ADDRESS_1 0x48 #define SLAVE_ADDRESS_2 0x49 #define NUM_OF_REC_BYTES 10 #define I2C_DELAY 50 uint32_t i, j; uint32_t pedometerCnt, pedometerCntOld = 0xffffffff; static uint8_t index, indexOld = 0xff; //一次滴答中断的tick数 uint32_t System_tick_num; static uint32_t delayCnt = 0xffffffff, delayTarget = 0; static uint8_t delayFinFlag = 0; static volatile uint8_t Lsm6dsoEventDetected = 0; uint8_t pedoFlag = 0; // void pedometerShow(void); void MCU_Init() { // Set P1.0 to output direction GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0); /* Configuring P1.1 as an input and enabling interrupts */ MAP_GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN1); MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, GPIO_PIN1); MAP_GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN1); MAP_Interrupt_enableInterrupt(INT_PORT1); /* Configuring P1.1 as an input and enabling interrupts */ MAP_GPIO_setAsInputPinWithPullDownResistor(GPIO_PORT_P5, GPIO_PIN0); MAP_GPIO_clearInterruptFlag(GPIO_PORT_P5, GPIO_PIN0); MAP_GPIO_enableInterrupt(GPIO_PORT_P5, GPIO_PIN0); MAP_Interrupt_enableInterrupt(INT_PORT5); /* Enabling SRAM Bank Retention */ MAP_SysCtl_enableSRAMBankRetention(SYSCTL_SRAM_BANK1); /* Enabling MASTER interrupts */ MAP_Interrupt_enableMaster(); } void SysTick_Init(void) { /* Setup SysTick Timer for 10ms interrupts */ System_tick_num = SystemCoreClock / system_jump_time; if (SysTick_Config(System_tick_num)) { // OLED_ShowStr(1, 3, "SysTick err", 2); // OLED_ON();//OLED唤醒 while (1); } } void delayMS(uint32_t num) { delayTarget = num; delayCnt = 0; delayFinFlag = 0; while(!delayFinFlag); } int main(void) { /* Disabling the Watchdog */ MAP_WDT_A_holdTimer(); MCU_Init(); SysTick_Init(); BSP_I2C_Init(); for(i = 0; i < 4; i++) { // Toggle P1.0 output GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0); delayMS(250); } OLED_Init(); if(0 == Lsm6dso_Init()) { OLED_ShowStr(0, 1, "PEDOMETER :", 1); } else { OLED_ShowStr(1, 3, "Lsm6dso err", 2); OLED_ON();//OLED唤醒 while(1); } pedometerCnt = 0; while(1) { if(Lsm6dsoEventDetected) { Lsm6dsoEventDetected = 0; if(RET_OK == Get_Lsm6dso_Event(&pedoFlag)) { pedoFlag = 0; pedometerCnt++; } } pedometerShow(); } } void SysTick_Handler(void) { if(delayCnt < delayTarget) { delayCnt++; if(delayCnt >= delayTarget) { delayFinFlag = 1; } } } void pedometerShow() { stOledShow currRow; uint32_t pedometerCntShow; if(pedometerCntOld == pedometerCnt) { return; } pedometerCntOld = pedometerCnt; pedometerCntShow = pedometerCnt; index = 0; currRow.str[MAX_ROW_STR_NUM] = 0x0; while(pedometerCntShow > 9) { index++; currRow.str[MAX_ROW_STR_NUM - index] = (pedometerCntShow % 10) + 0x30; pedometerCntShow /= 10; } index++; if(index > MAX_PEDOMETER_INDEX) { index = 1; currRow.str[MAX_ROW_STR_NUM - index] = 0x21; index++; currRow.str[MAX_ROW_STR_NUM - index] = 0x4c; index++; currRow.str[MAX_ROW_STR_NUM - index] = 0x6e; index++; currRow.str[MAX_ROW_STR_NUM - index] = 0x6e; index++; currRow.str[MAX_ROW_STR_NUM - index] = 0x41; } else { currRow.str[MAX_ROW_STR_NUM - index] = (pedometerCntShow % 10) + 0x30; } if(indexOld != index) { indexOld = index; currRow.x = 0; currRow.y = 2; OLED_Fill_Line(currRow.y, 0x0); OLED_Fill_Line(currRow.y+1, 0x0); OLED_Fill_Line(currRow.y+2, 0x0); OLED_Fill_Line(currRow.y+3, 0x0); } currRow.y = 3; currRow.TextSize = 4; currRow.x = (ROW_PIXEL - 16 * index) / 2; OLED_ShowStr(currRow.x, currRow.y, &currRow.str[MAX_ROW_STR_NUM - index], currRow.TextSize); } /* GPIO ISR */ void PORT1_IRQHandler(void) { uint32_t status; status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P1); MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, status); /* Toggling the output on the LED */ if(status & GPIO_PIN1) { // MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0); pedometerCnt = 0; } } /* GPIO ISR */ void PORT5_IRQHandler(void) { uint32_t status; status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P5); MAP_GPIO_clearInterruptFlag(GPIO_PORT_P5, status); /* Toggling the output on the LED */ if(status & GPIO_PIN0) { // if(GPIO_INPUT_PIN_HIGH == GPIO_getInputPinValue(GPIO_PORT_P5, GPIO_PIN0)) { Lsm6dsoEventDetected = 1; } } }
I2C调试期间遇到了很多问题,也参考了E2E上帖子解决了问题(具体的网页一时找不到了)。这里把驱动文件上传上来,可供大家参考。
//***************************************************************************** // // Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // //**************************************************************************** //************************MODIFICATON INFORMATION***************************** //Modified from original source located at: // https://e2e.ti.com/support/microcontrollers/msp430/f/166/p/472504/1701554#1701554 // //Modifed by Reid Kersey, CEO, Sniffer GPS - 7/19/2017 // sniffergps.com // reid@sniffergps.com // 678-209-2215 // //Updates: //6/7/2017 //Changed EUSCI_Bx_MODULE to EUSCI_Bx_BASE //Changed from using B1 to allowing use of any Bx Module //Added funciton description comments //7/19/2017 //removed slow speed bug on B2 and B3 //Feel free to contact me about modifications to this code or questions about usage, //however I am not the original author. Credit goes to DavidL https://e2e.ti.com/members/2005340 #include "msp432.h" #include "i2c_driver.h" //#include "driverlib.h" #include <ti/devices/msp432p4xx/driverlib/driverlib.h> //***************************************************************************** // // Definitions // //***************************************************************************** //***************************************************************************** // // Global Data // //***************************************************************************** volatile eUSCI_status ui8Status; uint8_t *pData; uint8_t ui8DummyRead; uint32_t g_ui32ByteCount; bool burstMode = false; //B0-3 configurations /* I2C Master Configuration Parameter */ //volatile eUSCI_I2C_MasterConfig i2cConfig_B0 = eUSCI_I2C_MasterConfig i2cConfig_B0 = { EUSCI_B_I2C_CLOCKSOURCE_SMCLK, // SMCLK Clock Source 0, EUSCI_B_I2C_SET_DATA_RATE_100KBPS, // Desired I2C Clock of 400khz 0, // No byte counter threshold EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD // Autostop }; //volatile eUSCI_I2C_MasterConfig i2cConfig_B1 = eUSCI_I2C_MasterConfig i2cConfig_B1 = { EUSCI_B_I2C_CLOCKSOURCE_SMCLK, // SMCLK Clock Source 0, EUSCI_B_I2C_SET_DATA_RATE_100KBPS, // Desired I2C Clock of 400khz 0, // No byte counter threshold EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD // Autostop }; //volatile eUSCI_I2C_MasterConfig i2cConfig_B2 = eUSCI_I2C_MasterConfig i2cConfig_B2 = { EUSCI_B_I2C_CLOCKSOURCE_SMCLK, // SMCLK Clock Source 0, EUSCI_B_I2C_SET_DATA_RATE_100KBPS, // Desired I2C Clock of 400khz 0, // No byte counter threshold EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD // Autostop }; //volatile eUSCI_I2C_MasterConfig i2cConfig_B3 = eUSCI_I2C_MasterConfig i2cConfig_B3 = { EUSCI_B_I2C_CLOCKSOURCE_SMCLK, // SMCLK Clock Source 0, EUSCI_B_I2C_SET_DATA_RATE_100KBPS, // Desired I2C Clock of 400khz 0, // No byte counter threshold EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD // Autostop }; //***************************************************************************** // // Imported Data // //***************************************************************************** //***************************************************************************** // // Constants // //***************************************************************************** //***************************************************************************** // // Function Prototypes // //***************************************************************************** /*********************************************************** Function: You MUST call this before doing any read or writes @param module the EUSCI module to use ex: EUSCI_B0_BASE */ void initI2C(int module) { /* I2C Clock Soruce Speed */ if(module == EUSCI_B0_BASE){ i2cConfig_B0.i2cClk = MAP_CS_getSMCLK(); GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P1, GPIO_PIN6 | GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION); /* Initializing I2C Master to SMCLK at 100kbs with autostop */ MAP_I2C_initMaster(EUSCI_B0_BASE, &i2cConfig_B0); }else if(module == EUSCI_B1_BASE){ i2cConfig_B1.i2cClk = MAP_CS_getSMCLK(); GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P6, GPIO_PIN5 | GPIO_PIN4, GPIO_PRIMARY_MODULE_FUNCTION); /* Initializing I2C Master to SMCLK at 100kbs with autostop */ MAP_I2C_initMaster(EUSCI_B1_BASE, &i2cConfig_B1); }else if(module == EUSCI_B2_BASE){ i2cConfig_B2.i2cClk = MAP_CS_getSMCLK(); GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P3, GPIO_PIN6 | GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION); /* Initializing I2C Master to SMCLK at 100kbs with autostop */ MAP_I2C_initMaster(EUSCI_B2_BASE, &i2cConfig_B2); }else if(module == EUSCI_B3_BASE){ i2cConfig_B3.i2cClk = MAP_CS_getSMCLK(); GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P6, GPIO_PIN6 | GPIO_PIN7, GPIO_SECONDARY_MODULE_FUNCTION); /* Initializing I2C Master to SMCLK at 100kbs with autostop */ MAP_I2C_initMaster(EUSCI_B3_BASE, &i2cConfig_B3); } } /*********************************************************** Function: @param module the EUSCI module to use ex: EUSCI_B0_BASE @param ui8Addr the 7 bit address of the module @param ui8Reg the register to write to @param Data a pointer to where the data to be written is stored @param ui32ByteCount the number of bytes to write @returns true if successful, false otherwise */ bool writeI2C(int module, uint8_t ui8Addr, uint8_t ui8Reg, uint8_t *Data, uint8_t ui8ByteCount) { /* Wait until ready to write */ while (MAP_I2C_isBusBusy(module)); /* Assign Data to local Pointer */ pData = Data; /* Disable I2C module to make changes */ MAP_I2C_disableModule(module); /* Setup the number of bytes to transmit + 1 to account for the register byte */ if(module == EUSCI_B0_BASE){ i2cConfig_B0.byteCounterThreshold = ui8ByteCount + 1; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B0); }else if(module == EUSCI_B1_BASE){ i2cConfig_B1.byteCounterThreshold = ui8ByteCount + 1; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B1); }else if(module == EUSCI_B2_BASE){ i2cConfig_B2.byteCounterThreshold = ui8ByteCount + 1; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B2); }else if(module == EUSCI_B3_BASE){ i2cConfig_B3.byteCounterThreshold = ui8ByteCount + 1; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B3); }else{ return false; } /* Load device slave address */ MAP_I2C_setSlaveAddress(module, ui8Addr); /* Enable I2C Module to start operations */ MAP_I2C_enableModule(module); /* Enable master STOP, TX and NACK interrupts */ MAP_I2C_enableInterrupt(module, EUSCI_B_I2C_STOP_INTERRUPT + EUSCI_B_I2C_NAK_INTERRUPT + EUSCI_B_I2C_TRANSMIT_INTERRUPT0); /* Set our local state to Busy */ ui8Status = eUSCI_BUSY; /* Send start bit and register */ MAP_I2C_masterSendMultiByteStart(module,ui8Reg); /* Enable master interrupt for the remaining data */ if(module == EUSCI_B0_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB0); }else if(module == EUSCI_B1_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB1); }else if(module == EUSCI_B2_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB2); }else if(module == EUSCI_B3_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB3); }else{ return false; } // NOW WAIT FOR DATA BYTES TO BE SENT while(ui8Status == eUSCI_BUSY) { #ifdef USE_LPM MAP_PCM_gotoLPM0(); #else __no_operation(); #endif } /* Disable interrupts */ MAP_I2C_disableInterrupt(module, EUSCI_B_I2C_STOP_INTERRUPT + EUSCI_B_I2C_NAK_INTERRUPT + EUSCI_B_I2C_TRANSMIT_INTERRUPT0); if(module == EUSCI_B0_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB0); }else if(module == EUSCI_B1_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB1); }else if(module == EUSCI_B2_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB2); }else if(module == EUSCI_B3_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB3); }else{ return false; } if(ui8Status == eUSCI_NACK) { return(false); } else { return(true); } } /*********************************************************** Function: @param module the EUSCI module to use ex: EUSCI_B0_BASE @param ui8Addr the 7 bit address of the module @param ui8Reg the register to read from @param Data a pointer to where to put the data @param ui32ByteCount the number of bytes to read @returns true if successful, false otherwise */ bool readI2C(int module, uint8_t ui8Addr, uint8_t ui8Reg, uint8_t *Data, uint8_t ui8ByteCount) { /* Todo: Put a delay */ //todo reset if busy for long enough time /* Wait until ready */ while (MAP_I2C_isBusBusy(module)); /* Assign Data to local Pointer */ pData = Data; /* Disable I2C module to make changes */ MAP_I2C_disableModule(module); /* Setup the number of bytes to receive */ if(module == EUSCI_B0_BASE){ i2cConfig_B0.byteCounterThreshold = ui8ByteCount; i2cConfig_B0.autoSTOPGeneration = EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B0); // i2cConfig_B0.byteCounterThreshold = ui8ByteCount; // i2cConfig_B0.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP;//EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD;// // g_ui32ByteCount = ui8ByteCount; // burstMode = true; }else if(module == EUSCI_B1_BASE){ i2cConfig_B1.byteCounterThreshold = ui8ByteCount; i2cConfig_B1.autoSTOPGeneration = EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B1); }else if(module == EUSCI_B2_BASE){ i2cConfig_B2.byteCounterThreshold = ui8ByteCount; i2cConfig_B2.autoSTOPGeneration = EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B2); }else if(module == EUSCI_B3_BASE){ i2cConfig_B3.byteCounterThreshold = ui8ByteCount; i2cConfig_B3.autoSTOPGeneration = EUSCI_B_I2C_SEND_STOP_AUTOMATICALLY_ON_BYTECOUNT_THRESHOLD; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B3); }else{ return false; } /* Load device slave address */ MAP_I2C_setSlaveAddress(module, ui8Addr); /* Enable I2C Module to start operations */ MAP_I2C_enableModule(module); /* Enable master STOP and NACK interrupts */ MAP_I2C_enableInterrupt(module, EUSCI_B_I2C_STOP_INTERRUPT + EUSCI_B_I2C_NAK_INTERRUPT); /* Set our local state to Busy */ ui8Status = eUSCI_BUSY; /* Send start bit and register */ MAP_I2C_masterSendMultiByteStart(module,ui8Reg); /* Enable master interrupt for the remaining data */ if(module == EUSCI_B0_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB0); }else if(module == EUSCI_B1_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB1); }else if(module == EUSCI_B2_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB2); }else if(module == EUSCI_B3_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB3); }else{ return false; } /* NOTE: If the number of bytes to receive = 1, then as target register is being shifted * out during the write phase, UCBxTBCNT will be counted and will trigger STOP bit prematurely * If count is > 1, wait for the next TXBUF empty interrupt (just after reg value has been * shifted out * * If your code is getting stuck here, you probably called this function from an interrupt * DON'T DO THAT! */ while(ui8Status == eUSCI_BUSY) { if(MAP_I2C_getInterruptStatus(module, EUSCI_B_I2C_TRANSMIT_INTERRUPT0)) { ui8Status = eUSCI_IDLE; } } ui8Status = eUSCI_BUSY; /* Turn off TX and generate RE-Start */ MAP_I2C_masterReceiveStart(module); /* Enable RX interrupt */ MAP_I2C_enableInterrupt(module, EUSCI_B_I2C_RECEIVE_INTERRUPT0); /* Wait for all data be received */ while(ui8Status == eUSCI_BUSY) { #ifdef USE_LPM MAP_PCM_gotoLPM0(); #else __no_operation(); #endif } /* Disable interrupts */ MAP_I2C_disableInterrupt(module, EUSCI_B_I2C_STOP_INTERRUPT + EUSCI_B_I2C_NAK_INTERRUPT + EUSCI_B_I2C_RECEIVE_INTERRUPT0); if(module == EUSCI_B0_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB0); }else if(module == EUSCI_B1_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB1); }else if(module == EUSCI_B2_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB2); }else if(module == EUSCI_B3_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB3); }else{ return false; } if(ui8Status == eUSCI_NACK) { return(false); } else { return(true); } } /*********************************************************** Function: @param module the EUSCI module to use ex: EUSCI_B0_BASE @param ui8Addr the 7 bit address of the module @param ui8Reg the register to read from @param Data a pointer to where to put the data @param ui32ByteCount the number of bytes to read @returns true if successful, false otherwise */ bool readBurstI2C(int module, uint8_t ui8Addr, uint8_t ui8Reg, uint8_t *Data, uint32_t ui32ByteCount) { /* Todo: Put a delay */ /* Wait until ready */ while (MAP_I2C_isBusBusy(module)); /* Assign Data to local Pointer */ pData = Data; /* Disable I2C module to make changes */ MAP_I2C_disableModule(module); /* Setup the number of bytes to receive */ if(module == EUSCI_B0_BASE){ i2cConfig_B0.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP; g_ui32ByteCount = ui32ByteCount; burstMode = true; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B0); }else if(module == EUSCI_B1_BASE){ i2cConfig_B0.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP; g_ui32ByteCount = ui32ByteCount; burstMode = true; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B1); }else if(module == EUSCI_B2_BASE){ i2cConfig_B0.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP; g_ui32ByteCount = ui32ByteCount; burstMode = true; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B2); }else if(module == EUSCI_B3_BASE){ i2cConfig_B0.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP; g_ui32ByteCount = ui32ByteCount; burstMode = true; MAP_I2C_initMaster(module, (const eUSCI_I2C_MasterConfig *)&i2cConfig_B3); }else{ return false; } /* Load device slave address */ MAP_I2C_setSlaveAddress(module, ui8Addr); /* Enable I2C Module to start operations */ MAP_I2C_enableModule(module); /* Enable master STOP and NACK interrupts */ MAP_I2C_enableInterrupt(module, EUSCI_B_I2C_STOP_INTERRUPT + EUSCI_B_I2C_NAK_INTERRUPT); /* Set our local state to Busy */ ui8Status = eUSCI_BUSY; /* Send start bit and register */ MAP_I2C_masterSendMultiByteStart(module,ui8Reg); /* Enable master interrupt for the remaining data */ if(module == EUSCI_B0_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB0); }else if(module == EUSCI_B1_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB1); }else if(module == EUSCI_B2_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB2); }else if(module == EUSCI_B3_BASE){ MAP_Interrupt_enableInterrupt(INT_EUSCIB3); }else{ return false; } /* NOTE: If the number of bytes to receive = 1, then as target register is being shifted * out during the write phase, UCBxTBCNT will be counted and will trigger STOP bit prematurely * If count is > 1, wait for the next TXBUF empty interrupt (just after reg value has been * shifted out * * If your code is getting stuck here, you probably called this function from an interrupt * DON'T DO THAT! */ while(ui8Status == eUSCI_BUSY) { if(MAP_I2C_getInterruptStatus(module, EUSCI_B_I2C_TRANSMIT_INTERRUPT0)) { ui8Status = eUSCI_IDLE; } } ui8Status = eUSCI_BUSY; /* Turn off TX and generate RE-Start */ MAP_I2C_masterReceiveStart(module); /* Enable RX interrupt */ MAP_I2C_enableInterrupt(module, EUSCI_B_I2C_RECEIVE_INTERRUPT0); /* Wait for all data be received */ while(ui8Status == eUSCI_BUSY) { #ifdef USE_LPM MAP_PCM_gotoLPM0(); #else __no_operation(); #endif } /* Disable interrupts */ MAP_I2C_disableInterrupt(module, EUSCI_B_I2C_STOP_INTERRUPT + EUSCI_B_I2C_NAK_INTERRUPT + EUSCI_B_I2C_RECEIVE_INTERRUPT0); if(module == EUSCI_B0_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB0); }else if(module == EUSCI_B1_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB1); }else if(module == EUSCI_B2_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB2); }else if(module == EUSCI_B3_BASE){ MAP_Interrupt_disableInterrupt(INT_EUSCIB3); }else{ return false; } if(ui8Status == eUSCI_NACK) { return(false); } else { return(true); } } /*********************************************************** Function: euscib0IntHandler */ void EUSCIB0_IRQHandler(void) { uint_fast16_t status; status = MAP_I2C_getEnabledInterruptStatus(EUSCI_B0_BASE); MAP_I2C_clearInterruptFlag(EUSCI_B0_BASE, status); if (status & EUSCI_B_I2C_NAK_INTERRUPT) { /* Generate STOP when slave NACKS */ MAP_I2C_masterSendMultiByteStop(EUSCI_B0_BASE); /* Clear any pending TX interrupts */ MAP_I2C_clearInterruptFlag(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0); /* Set our local state to NACK received */ ui8Status = eUSCI_NACK; } if (status & EUSCI_B_I2C_START_INTERRUPT) { /* Change our local state */ ui8Status = eUSCI_START; } if (status & EUSCI_B_I2C_STOP_INTERRUPT) { /* Change our local state */ ui8Status = eUSCI_STOP; } if (status & EUSCI_B_I2C_RECEIVE_INTERRUPT0) { /* RX data */ *pData++ = MAP_I2C_masterReceiveMultiByteNext(EUSCI_B0_BASE); ui8DummyRead= MAP_I2C_masterReceiveMultiByteNext(EUSCI_B0_BASE); if (burstMode) { g_ui32ByteCount--; if (g_ui32ByteCount == 1) { burstMode = false; /* Generate STOP */ MAP_I2C_masterSendMultiByteStop(EUSCI_B0_BASE); } } } if (status & EUSCI_B_I2C_TRANSMIT_INTERRUPT0) { /* Send the next data */ MAP_I2C_masterSendMultiByteNext(EUSCI_B0_BASE, *pData++); } #ifdef USE_LPM MAP_Interrupt_disableSleepOnIsrExit(); #endif } void EUSCIB1_IRQHandler(void) { uint_fast16_t status; status = MAP_I2C_getEnabledInterruptStatus(EUSCI_B1_BASE); MAP_I2C_clearInterruptFlag(EUSCI_B1_BASE, status); if (status & EUSCI_B_I2C_NAK_INTERRUPT) { /* Generate STOP when slave NACKS */ MAP_I2C_masterSendMultiByteStop(EUSCI_B1_BASE); /* Clear any pending TX interrupts */ MAP_I2C_clearInterruptFlag(EUSCI_B1_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0); /* Set our local state to NACK received */ ui8Status = eUSCI_NACK; } if (status & EUSCI_B_I2C_START_INTERRUPT) { /* Change our local state */ ui8Status = eUSCI_START; } if (status & EUSCI_B_I2C_STOP_INTERRUPT) { /* Change our local state */ ui8Status = eUSCI_STOP; } if (status & EUSCI_B_I2C_RECEIVE_INTERRUPT0) { /* RX data */ *pData++ = MAP_I2C_masterReceiveMultiByteNext(EUSCI_B1_BASE); ui8DummyRead= MAP_I2C_masterReceiveMultiByteNext(EUSCI_B1_BASE); if (burstMode) { g_ui32ByteCount--; if (g_ui32ByteCount == 1) { burstMode = false; /* Generate STOP */ MAP_I2C_masterSendMultiByteStop(EUSCI_B1_BASE); } } } if (status & EUSCI_B_I2C_TRANSMIT_INTERRUPT0) { /* Send the next data */ MAP_I2C_masterSendMultiByteNext(EUSCI_B1_BASE, *pData++); } #ifdef USE_LPM MAP_Interrupt_disableSleepOnIsrExit(); #endif } void EUSCIB2_IRQHandler(void) { uint_fast16_t status; status = MAP_I2C_getEnabledInterruptStatus(EUSCI_B2_BASE); MAP_I2C_clearInterruptFlag(EUSCI_B2_BASE, status); if (status & EUSCI_B_I2C_NAK_INTERRUPT) { /* Generate STOP when slave NACKS */ MAP_I2C_masterSendMultiByteStop(EUSCI_B2_BASE); /* Clear any pending TX interrupts */ MAP_I2C_clearInterruptFlag(EUSCI_B2_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0); /* Set our local state to NACK received */ ui8Status = eUSCI_NACK; } if (status & EUSCI_B_I2C_START_INTERRUPT) { /* Change our local state */ ui8Status = eUSCI_START; } if (status & EUSCI_B_I2C_STOP_INTERRUPT) { /* Change our local state */ ui8Status = eUSCI_STOP; } if (status & EUSCI_B_I2C_RECEIVE_INTERRUPT0) { /* RX data */ *pData++ = MAP_I2C_masterReceiveMultiByteNext(EUSCI_B2_BASE); ui8DummyRead= MAP_I2C_masterReceiveMultiByteNext(EUSCI_B2_BASE); if (burstMode) { g_ui32ByteCount--; if (g_ui32ByteCount == 1) { burstMode = false; /* Generate STOP */ MAP_I2C_masterSendMultiByteStop(EUSCI_B2_BASE); } } } if (status & EUSCI_B_I2C_TRANSMIT_INTERRUPT0) { /* Send the next data */ MAP_I2C_masterSendMultiByteNext(EUSCI_B2_BASE, *pData++); } #ifdef USE_LPM MAP_Interrupt_disableSleepOnIsrExit(); #endif } void EUSCIB3_IRQHandler(void) { uint_fast16_t status; status = MAP_I2C_getEnabledInterruptStatus(EUSCI_B3_BASE); MAP_I2C_clearInterruptFlag(EUSCI_B3_BASE, status); if (status & EUSCI_B_I2C_NAK_INTERRUPT) { /* Generate STOP when slave NACKS */ MAP_I2C_masterSendMultiByteStop(EUSCI_B3_BASE); /* Clear any pending TX interrupts */ MAP_I2C_clearInterruptFlag(EUSCI_B3_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0); /* Set our local state to NACK received */ ui8Status = eUSCI_NACK; } if (status & EUSCI_B_I2C_START_INTERRUPT) { /* Change our local state */ ui8Status = eUSCI_START; } if (status & EUSCI_B_I2C_STOP_INTERRUPT) { /* Change our local state */ ui8Status = eUSCI_STOP; } if (status & EUSCI_B_I2C_RECEIVE_INTERRUPT0) { /* RX data */ *pData++ = MAP_I2C_masterReceiveMultiByteNext(EUSCI_B3_BASE); ui8DummyRead= MAP_I2C_masterReceiveMultiByteNext(EUSCI_B3_BASE); if (burstMode) { g_ui32ByteCount--; if (g_ui32ByteCount == 1) { burstMode = false; /* Generate STOP */ MAP_I2C_masterSendMultiByteStop(EUSCI_B3_BASE); } } } if (status & EUSCI_B_I2C_TRANSMIT_INTERRUPT0) { /* Send the next data */ MAP_I2C_masterSendMultiByteNext(EUSCI_B3_BASE, *pData++); } #ifdef USE_LPM MAP_Interrupt_disableSleepOnIsrExit(); #endif } void BSP_I2C_Init() { initI2C(EUSCI_B0_BASE); } bool BSP_I2C1_WriteReg(uint16_t DevAddr, uint16_t Reg, uint8_t *pData, uint16_t Length) { if(writeI2C(EUSCI_B0_BASE, (DevAddr & 0xff), (Reg & 0xff), pData, (Length & 0xff))) { return 0; } return 1; } bool BSP_I2C1_ReadReg(uint16_t DevAddr, uint16_t Reg, uint8_t *pData, uint16_t Length) { if(readI2C(EUSCI_B0_BASE, (DevAddr & 0xff), (Reg & 0xff), pData, (Length & 0xff))) { return 0; } return 1; }
思路不错,但是没有把过程中碰到什么问题,如何解决的写出来就略显文章差一点了,对初学网友解决问题帮助就差了点。
这篇分享结合使用了作者自己 传感器+显示模块,主要使用I2C功能驱动,具体也给了驱动代码,代码调理也比较清晰,并结合了资料分析,这个很值得初学的小伙伴参考;
缺点就是代码少了些注释,需要有一定代码功底的人才能看懂,还有就是如果有调试过程的还有出现的问题及解决过程总结等的分享就更好了。
虽如此但还是作者感谢分享!